DOCA0194EN-00

Introduction

PowerLogic Master Range

PowerLogic smooths the power supply, protects the network, the installation and the operator by improving the power factor and hence the quality of the power. It also allows for remote control of equipment and the monitoring of its performance and condition in real time.

Overview

The PowerTag system can be adapted to design a basic electrical distribution panel with only one gateway or large installation with a high number of power data units, gateways, and wireless devices.

The PowerTag system consists of:

  • Gateways

  • Wired Acti 9 devices

  • Wireless PowerTag devices

For more information on the system components, refer to Related Documents.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.