DOCA0194EN-00

Wireless Channel Assignment Prerequisite

Before assigning the wireless channels, make sure that the following conditions are met:

  • The total number of PowerTag systems for the architecture is defined.

  • The panels are pre-designed in accordance with the enclosure implementation rules (refer to Enclosure Implementation Rules). Therefore, the number of gateways and the number of wireless devices per PowerTag system for each type of panel is defined.

  • The physical position of each panel in the architecture is defined.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?