DOCA0194EN-00

PowerTag System Engineering Workflow

The PowerTag System engineering workflow consists of the following design phases:

Graphic Rules

The following legends are used to qualify the architecture and implementation:

Icon

Description

Architecture or implementation forbidden

Architecture or implementation possible

Architecture or implementation recommended

Remarks

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?