DOCA0194EN-00

Wireless Parameters in PowerTag System

The parameters dedicated to wireless communication are defined in a gateway. These parameters are set through the webpage during the gateway commissioning:

  • Wireless channel selection mode (automatic or manual)

  • Wireless channel (only if wireless channel selection mode is set on manual)

  • Wireless communication periods for energy monitoring, control sensors, and HeatTag sensor (future features)

For more details on wireless parameters, refer to the below user guides, as applicable:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?