DOCA0127EN-03

Motor Protection Functions

Overview

This chapter describes the motor protection functions provided by the LTMR controller.

Motor Protection Functions Introduction

Overview

This section introduces you to the motor protection functions provided by the LTMR controller, including protection parameters and characteristics.

Definitions

Defined Functions and Data

The LTMR controller monitors current, ground-current and motor temperature sensor parameters. When the LTMR controller is connected to an expansion module, it also monitors voltage and power parameters. The LTMR controller uses these parameters in protection functions to detect trip and alarm conditions. The LTMR controller’s response to trip and alarm conditions is fixed for the predefined operating modes. Logic output O.4 activates on a trip, and logic output O.3 activates on an alarm. For more information about predefined operating modes, refer to Operating Modes.

You can configure these motor protection functions to detect the existence of undesirable operating conditions that, if not resolved, can cause motor and equipment damage.

All motor protection functions include trip detection, and most protection functions also include alarm detection.

Customized Functions and Data

In addition to using the protection functions and parameters included in a predefined operating mode, you can use the Custom Logic Editor in the TeSys T DTM to create a new, customized operating mode. To create a custom operating mode, select any predefined operating mode, then edit its code to meet the needs of your application.

Using the Custom Logic Editor, you can create a customized operating mode by:

  • Modifying the LTMR controller’s responses to protection trips or alarms

  • Adding new functions, based on either predefined or newly created parameters

Trips

A trip is a serious undesirable operating condition. Trip-related parameters can be configured for most protection functions.

The response of the LTMR controller to a trip include the following:

  • Output O.4 contacts:

    • Contact 95-96 is open

    • Contact 97-98 is closed

  • On LTMR Ethernet controllers: Alarm/MS LED is On

    • Minor trip if blinking red once per second (EtherNet/IP only)

    • Minor trip if steady red (Modbus/TCP only)

    • Major trip if steady red

  • On other LTMR controllers: Alarm LED is On (steady red)

  • Trip status bits are set in a trip parameter

  • A text message is displayed in an HMI screen (if an HMI is attached)

  • A trip status indicator is displayed in the TeSys T DTM, if connected

The LTMR controller counts and records the number of trips for each protection function.

After a trip has occurred, merely resolving the underlying condition does not clear the trip. To clear the trip, the LTMR controller must be reset. For more information, refer to Trip Management - Introduction.

Alarms

An alarm is a less-serious, though still undesirable, operating condition. An alarm indicates corrective action may be required to address the undesirable condition. If left unresolved, an alarm may lead to a trip condition. Alarm-related parameters can be configured for most protection functions.

The response of the LTMR controller to an alarm include the following:

  • Output O.3 is closed

  • On LTMR Ethernet controllers: Alarm/MS LED flashes (Modbus/TCP only)

  • On other LTMR controllers: Alarm LED flashes red twice per second

  • Alarm status bits are set in an alarm parameter

  • A text message is displayed in an HMI screen (if attached)

  • An alarm status indicator is displayed in the TeSys T DTM

NOTE: For some protection functions, alarm detection shares the same threshold as a trip. For other protection functions, alarm has a separate threshold.

The LTMR controller clears the alarm whenever the measured value no longer exceeds the alarm threshold-plus or minus a 5% hysteresis band.

Motor Protection Characteristics

Operation

The following diagram describes the operation of a typical motor protection function. This diagram, and the following diagrams, are expressed in terms of current. However, the same principles apply to voltage.

I Measurement of the monitored parameter

Is1 Alarm threshold setting

Is2 Trip threshold setting

T Trip timeout setting

Inst Instantaneous alarm/trip detection

Settings

Some protection functions include configurable settings, including:

  • Trip threshold: A limit setting for the monitored parameter that triggers a protection function trip.

  • Alarm threshold: A limit setting for the monitored parameter that triggers a protection function alarm.

  • Trip timeout: A time delay that must expire before the protection function trip is triggered. The behavior of a timeout depends on its trip current characteristic profile.

  • Trip curve characteristic (TCC): The LTMR controller includes a definite trip characteristic for all protection functions, except the Thermal Overload Inverse Thermal protection function, which has both an inverse trip and definite trip curve characteristic, as described in the following diagram.

Definite TCC: The duration of the trip timeout remains a constant regardless of changes in the value of the measured quantity (current), as described in the following diagram:

Inverse TCC: The duration of the time delay varies inversely with the value of the measured quantity (here, thermal capacity). As the measured quantity increases, the potential for harm also increases, thereby causing the duration of the time delay to decrease, as described in the following diagram:

Hysteresis

To improve stability, motor protection functions apply a hysteresis value that is added to or subtracted from limit threshold settings before a trip or alarm response is reset. The hysteresis value is calculated as a percentage, typically 5%, of the limit threshold and is

  • Subtracted from the threshold value for upper limit thresholds,

  • Added to the threshold value for lower limit thresholds.

The following diagram describes the logic result of measurement processing (Inst) when hysteresis is applied to an upper limit threshold:

d Hysteresis percentage

Thermal Motor Protection Functions

Overview

This section describes the thermal motor protection functions of the LTMR controller.

Thermal Overload

Overview

The LTMR controller can be configured to provide thermal protection, by selecting one of the following settings:

Each setting represents a Trip Curve Characteristic. The LTMR controller stores the selected setting in its Thermal Overload Mode parameter. Only one setting can be activated at a time. See the topics that immediately follow, for information on the operation and configuration of each setting.

Parameter Settings

The Thermal Overload function has the following configurable parameter settings, which apply to every trip current characteristic:

Parameters

Setting Range

Factory Setting

Mode

  • Inverse thermal

  • Definite time

Inverse thermal

Trip enable

Enable/Disable

Enable

Alarm enable

Enable/Disable

Enable

Motor auxiliary fan cooled

Enable/Disable

Disable

Thermal Overload - Inverse Thermal

Description

When you set the Thermal Overload Mode parameter to Inverse Thermal and select a motor trip class, the LTMR controller monitors the motor’s utilized thermal capacity and signals

  • An alarm when utilized thermal capacity exceeds a configured alarm threshold,

  • A trip when utilized thermal capacity is greater than 100%.

CAUTION
RISK OF MOTOR OVERHEATING
The Motor Trip Class parameter must be set to the thermal heating characteristics of the motor. Refer to the motor manufacturer’s instructions before setting this parameter.
Failure to follow these instructions can result in injury or equipment damage.

There is no time delay for the thermal overload alarm.

The LTMR controller calculates the Thermal Capacity Level in all operating states. When power to the LTMR controller is lost, the LTMR controller retains the last measurements of the motor’s thermal state for 30 minutes, allowing it to estimate the motor’s thermal state when power is reapplied.

Trip and alarm monitoring can be separately enabled and disabled.

  • The thermal overload alarm is cleared by the LTMR controller when the utilized thermal capacity falls 5% below the alarm threshold.

  • The thermal overload trip can be reset when the utilized thermal capacity falls below the trip reset threshold and after the trip reset timeout is elapsed.

Reset for Emergency Restart

You can use the Clear Thermal Capacity Level Command, issued from the PLC or an HMI, to restart an overloaded motor in an emergency situation. This command resets the thermal capacity utilization value to 0 and bypasses the cooling period required by the thermal model before the motor can be restarted.

This command also resets the Rapid Cycle Lockout Timeout to allow an immediate restart without lock.

The Clear All Command does not perform a Clear Thermal Capacity Level.

WARNING
LOSS OF MOTOR PROTECTION
Clearing the thermal capacity level inhibits thermal protection and can cause equipment overheating and fire. Continued operation with inhibited thermal protection should be limited to applications where immediate restart is vital.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The Clear Thermal Capacity Level Command will not reset the trip response. Instead

  • Only an action external to the LTMR controller (for example, a reduction in the motor load) can clear the trip condition,

  • Only a reset command, from the valid reset means configured in the Trip Reset Mode parameter, will reset the trip response.

WARNING
UNINTENDED EQUIPMENT OPERATION
  • A reset command may restart the motor if the LTMR controller is used in a 2-wire control circuit.
  • Equipment operation must conform to local and national safety regulations and codes.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Operation

The thermal overload inverse thermal protection function is based on a thermal model of the motor that combines two thermal images:

  • A copper-based image representing the thermal state of the stator and rotor windings, and

  • An iron-based image representing the thermal state of the motor frame.

Using measured current and the input motor trip class setting, the LTMR controller considers only the highest thermal state, iron, or copper, when calculating thermal capacity utilized by the motor, as described in the following diagram:

θ Thermal value

θfe Iron tripping threshold

θcu Copper tripping threshold

t Time

When inverse thermal trip mode is selected, the Thermal Capacity Level parameter, indicating utilized thermal capacity due to load current, is incremented during both start and run states. When the LTMR controller detects that the thermal capacity level (θ) exceeds the trip threshold (θ s), it triggers a thermal overload trip, as described in the following diagram:

Functional Characteristics

The Thermal Overload inverse thermal functions include the following features:

  • One motor trip class setting:

    • Motor Trip Class

  • Four configurable thresholds:

    • Motor Full Load Current Ratio (FLC1)

    • Motor High-Speed Full Load Current Ratio (FLC2)

    • Thermal Overload Alarm Threshold

    • Thermal Overload Trip Reset Threshold

  • One time delay:

    • Trip Reset Timeout

  • Two function outputs:

    • Thermal Overload Trip

    • Thermal Overload Trip

  • Two counting statistics:

    • Thermal Overload Trips Count

    • Thermal Overload Alarms Count

  • One setting for an external auxiliary motor cooling fan:

    • Motor Aux Fan Cooled

  • One measure of utilized thermal capacity:

    • Thermal Capacity Level

NOTE: For LTMR controllers configured for 2-speed predefined operating mode, 2 trip thresholds are used: FLC1 and FLC2.

Block Diagram

Imax Maximum current

θmax Thermal capacity level

θs1 Thermal overload alarm threshold

Parameter Settings

The thermal overload inverse thermal functions have the following configurable parameter settings:

Parameters

Setting Range

Factory Setting

FLC1, FLC2

  • 0.4...8.0 A in increments of 0.08 A for LTMR08

  • 1.35...27.0 A in increments of 0.27 A for LTMR27

  • 5...100 A in increments of 1 A for LTMR100

  • 0.4 A for LTMR08

  • 1.35 A for LTMR27

  • 5 A for LTMR100

Alarm threshold

10...100 % of thermal capacity

85 % of thermal capacity

Motor trip class

5...30 in increments of 5

5

Trip reset timeout

50...9999 in 1 s increments

480 s

Trip reset threshold

35...95 % of thermal capacity

75% of thermal capacity

The thermal overload inverse thermal functions have the following non-configurable parameter settings:

Parameter

Fixed Setting

Thermal overload trip threshold

100% of thermal capacity

Technical Characteristics

The thermal overload inverse thermal functions have the following characteristics:

Characteristics

Value

Hysteresis

–5 % of thermal overload alarm threshold

Trip time accuracy

+/– 0.1 s

Thermal Overload - Definite Time

Description

When you set the Thermal Overload Mode parameter to Definite Time, the LTMR controller signals:

  • An alarm when measured maximum phase current exceeds a configurable threshold (OC1 or OC2).

  • A trip when the maximum phase current continuously exceeds the same threshold (OC1 or OC2) for a set time delay.

The thermal overload definite time trip includes a time delay of constant magnitude, following a start command, before the protection is active and a trip timeout duration, as described in the following diagram:

IsTrip and alarm threshold (OC1 or OC2)

T1 Start command

T2 Elapsed time delay

There is no time delay for the thermal overload definite time alarm.

Trip and alarm monitoring can be separately enabled and disabled.

The definite time protection function is disabled following a start by a delay defined by the Long Start Trip Timeout setting. The LTMR controller, when configured for overload predefined operating mode, uses the change in state from off to on level current to begin the Start state. This delay allows the motor to draw current on startup required to overcome the inertia of the motor at rest.

NOTE: Configuration of this protection function requires configuration of the Long Start protection function, including the Long Start Trip Timeout parameter.

Functional Characteristics

The thermal overload definite time function includes the following features:

  • Two configurable threshold settings; one setting (OC1) is used for single speed motors, both settings are required for two-speed motors:

    • OC1(Motor Full Load Current Ratio) or

    • OC2 (Motor High-Speed Full Load Current Ratio)

  • One time delay:

    • Overcurrent Time (O-Time, set by the Thermal Overload Trip Definite Timeout parameter)

  • Two function outputs:

    • Thermal Overload Alarm

    • Thermal Overload Trip

  • Two counting statistics:

    • Thermal Overload Trips Count

    • Thermal Overload Alarms Count

Block Diagram

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Is Trip and alarm threshold (OC1 or OC2)

T Trip timeout

Parameter Settings

The definite time thermal overload function has the following configurable parameter settings:

Parameters

Setting Range

Factory Setting

Trip threshold:

  • Motor full load current ratio (OC1)

    - or -

  • Motor high-speed full load current ratio (OC2)

5...100% of FLCmax, in 1% increments.

Note: OC1 and OC2 settings can be set directly (in Amperes) in the Settings menu of an HMI, or in the Parameters tab of the TeSys T DTM.

5% FLCmax

Thermal overload trip definite timeout (O-time or over-current time)

1...300 s in 1 s increments

10 s

Thermal overload alarm threshold

20...800% of OC in 1% increments

80% of OC

Long start trip timeout* (D-time)

1...200 s in 1 s increments

10 s

Technical Characteristics

The definite time thermal overload function has the following characteristics:

Characteristics

Value

Hysteresis

–5% of alarm and trip thresholds

Trip time accuracy

+/– 0.1 s

Example

The following diagram describes a definite time thermal overload trip:

OC Trip threshold (OC1 or OC2)

Motor Temperature Sensor

Overview

The LTMR controller has two terminals, T1 and T2 that can be connected to a motor temperature sensing element to provide protection for motor windings by detecting high temperature conditions that could lead to damage or degradation.

These protections are activated when the Motor Temp Sensor Type parameter is set to one of the following settings:

Only one of these motor protection sensing elements can be enabled at a time.

NOTE: Motor temperature sensor protection is based in ohms. PTC Binary protection thresholds are pre-set to IEC standards and are non-configurable. PTC Analog and NTC Analog protection functions may require that you scale the resistance value to the corresponding threshold level in degrees, based on the properties of the selected sensing element.

When a sensor type is changed, the LTMR controller’s motor temperature sensing configuration settings revert to their factory settings. If a sensor type is replaced with another sensor of the same type, the setting values are retained.

Parameter Settings

The motor temperature sensor function has the following configurable parameter settings, which apply to the selected motor temp sensor type:

Parameters

Setting Range

Factory Setting

Sensor type

  • None

  • PTC Binary

  • PT100

  • PTC Analog

  • NTC Analog

None

Trip enable

Enable/Disable

Disable

Alarm enable

Enable/Disable

Disable

Motor Temperature Sensor - PTC Binary

Description

The PTC Binary motor temperature sensing function is enabled when the Motor Temp Sensor Type parameter is set to PTC Binary and the LTMR controller is connected to a binary positive temperature coefficient thermistor embedded in the motor.

The LTMR controller monitors the state of the temperature sensing element and signals:

  • A motor temperature sensor alarm when the measured resistance exceeds a fixed threshold.

  • A motor temperature sensor trip when the measured resistance exceeds the same fixed threshold.

The trip and alarm conditions continue until measured resistance falls below a separate fixed motor temperature sensor reclosing threshold.

Motor temperature sensing trip thresholds are factory pre-set and are not configurable. Trip monitoring can be enabled or disabled.

The function is available for all operating states.

Functional Characteristics

The PTC Binary motor temperature sensor function includes the following features:

  • Two function output:

    • Motor Temp Sensor Alarm

    • Motor Temp Sensor Trip

  • One counting statistic:

    • Motor Temp Sensor Trips Count

Block Diagram

θ Temperature sensing element resistance

Parameter Settings

The PTC binary motor temperature sensor function has the following non-configurable parameter settings:

Parameter

Fixed settings

Accuracy

Trip/Alarm threshold

2900 Ω

+/– 2%

Trip/Alarm reclosing threshold

1575 Ω

+/– 2%

Technical Characteristics

The PTC binary motor temperature sensor function has the following characteristics:

Characteristic

Value

Detection time

0.5...0.6 s

Detection time accuracy

+/– 0.1 s

Example

The following diagram describes the occurrence of a PTC binary motor temp sensor trip with an automatic reset:

2900 Ω Trip threshold

1575 Ω Trip reclosing threshold

Reset This marks the time after which a reset can be executed. A start command is required before run state can be resumed. In this example, auto-reset has been enabled.

Motor Temperature Sensor - PT100

Description

The PT100 motor temperature sensing function is enabled when the Motor Temperature Sensor Type parameter is set to PT100 and the LTMR controller is connected to a PT100 sensor embedded in the motor.

The LTMR controller monitors the state of the temperature sensing element and signals:

  • A motor temperature sensor alarm when the measured temperature exceeds a configurable alarm threshold.

  • A motor temperature sensor trip when the measured temperature exceeds a separately set trip threshold.

The LTMR directly measures the temperature with a PT100 sensor. The temperature measured by the PT100 sensor, either in °C (factory setting) or in °F, is displayed on the HMI or the TeSys T DTM, according to the Motor Temperature Sensor Display Degree CF parameter:

The trip or alarm condition continues until the measured temperature falls below 95% of the trip or alarm threshold.

There is a fixed detection time of 0.5 s to 0.6 s to the motor temperature sensor trip or alarm.

Trip and alarm monitoring can be separately enabled and disabled.

The function is available for all operating states.

NOTE:

The temperature is derived from the following equation: T = 2.6042 * R - 260.42,

Where R = resistance Ω).

NOTE: To connect a 3-wire PT100 sensor to an LTMR controller, simply do not wire the compensation pin of the 3-wire PT100 sensor.

Functional Characteristics

The PT100 motor temperature sensor function includes the following features:

  • Two configurable thresholds:

    • Motor Temperature Sensor Alarm Threshold Degree

    • Motor Temperature Sensor Trip Threshold Degree

  • Two function outputs:

    • Motor Temperature Sensor Alarm

    • Motor Temperature Sensor Trip

  • One counting statistic:

    • Motor Temperature Sensor Trips Count

  • One display configuration:

    • Motor Temperature Sensor Display Degree CF

Block Diagram

θ Temperature measured by the PT100 sensor

θs1 Motor temperature sensor alarm threshold

θs2 Motor temperature sensor trip threshold

Parameter Settings

The PT100 motor temperature sensor function has the following configurable parameter settings:

Parameters

Setting Range

Factory Setting

Trip threshold degree

0...200 °C in 1 °C increments

0 °C

Alarm threshold degree

0...200 °C in 1 °C increments

0 °C

Motor temperature sensor display degree CF

°C (0)

°F (1)

°C

Technical Characteristics

The PT100 motor temperature sensor function has the following characteristics:

Characteristic

Value

Hysteresis

–5% of Alarm threshold and Trip threshold

Detection time

0.5...0.6 s

Trip time accuracy

+/– 0.1 s

Example

The following diagram describes a Motor temperature sensor PT100 trip with automatic reset and an active Run command:

θs2 Trip threshold

θs3 Trip reclosing threshold (95% of trip threshold)

Motor Temperature Sensor - PTC Analog

Description

The PTC Analog motor temperature sensing function is enabled when the Motor Temp Sensor Type parameter is set to PTC Analog and the LTMR controller is connected to an analog PTC thermistor embedded in the motor.

The LTMR controller monitors the state of the temperature sensing element and signals:

  • A motor temperature sensor alarm when the measured resistance exceeds a configurable alarm threshold.

  • A motor temperature sensor trip when the measured resistance exceeds a separately set trip threshold.

The trip or alarm condition continues until the measured resistance falls below 95% of the trip or alarm threshold.

Trip and alarm monitoring can be separately enabled and disabled.

The function is available for all operating states.

Functional Characteristics

The PTC Analog motor temperature sensor function includes the following features:

  • Two configurable thresholds:

    • Motor Temp Sensor Alarm Threshold

    • Motor Temp Sensor Trip Threshold

  • Two function outputs:

    • Motor Temp Sensor Alarm

    • Motor Temp Sensor Trip

  • One counting statistic:

    • Motor Temp Sensor Trips Count

Block Diagram

θ Temperature sensing element resistance

θs1 Motor temperature sensor alarm threshold

θs2 Motor temperature sensor trip threshold

Parameter Settings

The PTC analog motor temperature sensor function has the following configurable parameter settings:

Parameters

Setting Range

Factory Setting

Trip threshold

20...6500 Ω in 0.1 Ω increments

20 Ω

Alarm threshold

20...6500 Ω in 0.1 Ω increments

20 Ω

Technical Characteristics

The PTC analog motor temperature sensor function has the following characteristics:

Characteristic

Value

Hysteresis

– 5% of Alarm threshold and Trip threshold

Detection time

0.5...0.6 s

Detection time accuracy

+/– 0.1 s

Example

The following diagram describes a Motor temperature sensor PTC analog trip with automatic reset and an active Run command:

θs2 Trip threshold

θs3 Trip reclosing threshold (95% of trip threshold)

Motor Temperature Sensor - NTC Analog

Description

The NTC Analog motor temperature sensing function is enabled when the Motor Temp Sensor Type parameter is set to NTC Analog and the LTMR controller is connected to an analog NTC thermistor embedded in the motor.

The LTMR controller monitors the state of the temperature sensing element and signals:

  • A motor temperature sensor alarm when the measured resistance falls below a configurable alarm threshold.

  • A motor temperature sensor trip when the measured resistance falls below a separately set trip threshold.

The trip or alarm condition continues until the measured resistance exceeds 105% of the trip or alarm threshold.

Trip and alarm monitoring can be separately enabled and disabled.

The function is available for all operating states.

Functional Characteristics

The NTC Analog motor temperature sensor function includes the following features:

  • Two configurable thresholds:

    • Alarm Threshold

    • Trip Threshold

  • Two function outputs:

    • Motor Temp Sensor Alarm

    • Motor Temp Sensor Trip

  • One counting statistic:

    • Motor Temp Sensor Trips Count

Block Diagram

θ Temperature sensing element resistance

θs1 Motor temperature sensor alarm threshold

θs2 Motor temperature sensor trip threshold

Parameter Settings

The NTC analog motor temperature sensor function has the following configurable parameter settings:

Parameters

Setting Range

Factory Setting

Trip threshold

20...6500 Ω in 0.1 Ω increments

20 Ω

Alarm threshold

20...6500 Ω in 0.1 Ω increments

20 Ω

Technical Characteristics

The NTC analog motor temperature sensor function has the following characteristics:

Characteristics

Value

Hysteresis

+ 5% of Alarm threshold and Trip thresholds

Detection time

0.5...0.6 s

Detection time accuracy

+/– 0.1 s

Example

The following diagram describes a Motor temperature sensor NTC analog trip with automatic reset:

θr2 Trip threshold

θr3 Trip reclosing threshold (105% of trip threshold)

Rapid Cycle Lockout

Description

The rapid cycle lockout function prevents potential harm to the motor caused by repetitive, successive inrush currents resulting from too little time between starts.

The rapid cycle lockout function provides a configurable timer, which begins its count when the LTMR controller detects On Level Current–defined as 20% of FLC. At the same time, the Rapid Cycle Lockout bit is set.

If the LTMR controller detects a Run command before the rapid cycle lockout has elapsed, the:

  • Rapid Cycle Lockout bit remains set

  • LTMR controller ignores the Run command. It prevents the motor from restarting

  • HMI device (if attached) displays "WAIT"

  • LTMR controller Alarm LED flashes red 5 times per second, indicating the LTMR controller has disabled motor outputs thereby preventing an undesirable condition caused by starting the motor

  • LTMR controller monitors the wait time-if more than one timer is active, the LTMR controller reports the minimum wait time before the longest timer elapses

On power loss, the LTMR controller stores the state of the lockout timer in non-volatile memory. When the LTMR controller next powers up, the timer restarts its count and again ignores Run commands until the timer completes the timeout.

Setting the Rapid Cycle Lockout Timeout parameter to 0 disables this function.

The Rapid Cycle Lockout Timeout setting can be edited when the LTMR controller is in its normal operating state. If an edit is made while the timer is counting, the edit is effective when the timer finishes counting.

This function has no alarm and no trip.

NOTE: The Rapid Cycle Lockout function is not active when the overload operating mode is selected.

Functional Characteristics

The rapid cycle lockout function includes the following parameters:

  • One time delay:

    • Rapid Cycle Lockout Timeout

  • One status bit:

    • Rapid Cycle Lockout

In addition, the Rapid Cycle Lockout function:

  • Disables motor outputs

  • Causes the LTMR Alarm LED to flash 5 times per second

Parameter Settings

The rapid cycle lockout function has the following parameters:

Parameters

Setting Range

Factory Setting

Rapid cycle lockout timeout

0...9999 s in increments of 1 s

0 s

Technical Characteristics

The rapid cycle lockout function has the following characteristics:

Characteristics

Value

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

Current Motor Protection Functions

Overview

This section describes the current motor protection functions of the LTMR controller.

Current Phase Imbalance

Description

The current phase imbalance function signals:

  • An alarm when the current in any phase differs by more than a set percentage from the average current in all three phases.

  • A trip when the current in any phase differs by more than a separately set percentage from the average current in all three phases for a set period of time.

CAUTION
RISK OF MOTOR OVERHEATING
  • The Current Phase Imbalance Trip Threshold must be properly set to protect the wiring and motor equipment from harm caused by motor overheating.
  • The setting you input must conform to national and local safety regulations and codes.
  • Refer to the motor manufacturer’s instructions before setting this parameter.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use this function to detect and guard against smaller current phase imbalances. For larger imbalances, in excess of 80% of the average current in all three phases, use the current phase loss motor protection function.

This function has two adjustable trip time delays:

  • One applies to current imbalances occurring while the motor is in start state, and

  • One applies to current imbalances occurring after startup while the motor is in run state

Both timers begin if the imbalance is detected in start state.

The function identifies the phase causing a current imbalance. If the maximum deviation from the three-phase current average is the same for two phases, the function identifies both phases.

Trip and alarm monitoring can be separately enabled and disabled.

The function applies only to three-phase motors.

Functional Characteristics

The current phase imbalance function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • Two trip time delays:

    • Trip Timeout Starting

    • Trip Timeout Running

  • Two function outputs:

    • Current Phase Imbalance Alarm

    • Current Phase Imbalance Trip

  • One counting statistic:

    • Current Phase Imbalance Trips Count

  • Three indicators identifying the phase or phases with the highest current imbalance:

    • L1 Current Highest Imbalance

    • L2 Current Highest Imbalance

    • L3 Current Highest Imbalance

Block Diagram

Current phase imbalance alarm and trip:

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Iimb Current imbalance ratio for three-phase

Is1 Alarm threshold

Is2 Trip threshold

T1 Trip timeout starting

T2 Trip timeout running

Parameter Settings

The current phase imbalance function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Enable

Trip timeout starting

0.2...20 s in 0.1 s increments

0.7 s

Trip timeout running

0.2...20 s in 0.1 s increments

5 s

Trip threshold

10...70% of the calculated imbalance in 1% increments

10%

Alarm enable

Enable/Disable

Disable

Alarm threshold

10...70% of the calculated imbalance in 1% increments

10%

NOTE: A time of 0.7 second is added to the Trip timeout starting parameter to avoid nuisance tripping during the start phase.

Technical Characteristics

The current phase imbalance function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of trip or alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the detection of a current phase imbalance occurring during run state.

ΔI Percentage difference between current in any phase and the three-phase current average

Is2 Trip threshold

Current Phase Loss

Description

The current phase loss function signals:

  • An alarm when the current in any phase differs by more than 80% from the average current in all three phases.

  • A trip when the current in any phase differs by more than 80% from the average current in all three phases for a set period of time.

NOTE: Use this function to detect and guard against large current phase imbalances, in excess of 80% of the average current in all three phases. For smaller current imbalances, use the current phase imbalance motor protection function.

This function has a single adjustable trip time delay, which is applied when the motor is in start state or run state.

The function identifies the phase experiencing a current loss. If the maximum deviation from the three-phase current average is the same for two phases, the function identifies both phases.

Trip and alarm monitoring can be separately enabled and disabled.

The function applies only to three-phase motors.

Functional Characteristics

The current phase loss function includes the following features:

  • One fixed trip and alarm threshold equal to 80% of the three-phase average current.

  • One trip time delay:

    • Current Phase Loss Timeout

  • Two function outputs:

    • Current Phase Loss Alarm

    • Current Phase Loss Trip

  • One counting statistic:

    • Current Phase Loss Trips Count

  • Three indicators identifying the phase or phases experiencing the current loss:

    • L1 Current loss

    • L2 Current loss

    • L3 Current loss

Block Diagram

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Ln Line current number or numbers with the greatest deviation from Iavg

Iavg three-phase current average

T Trip timeout

Parameter Settings

The current phase loss function has the following configurable parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Enable

Timeout

0.1...30 s in 0.1 s increments

3 s

Alarm enable

Enable/Disable

Enable

NOTE: A time of 0.7 second is added to the Trip timeout parameter to avoid nuisance tripping during the start phase.

Technical Characteristics

The current phase loss function has the following characteristics:

Characteristics

Value

Hysteresis

75% of the three-phase average current

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of a current phase loss trip of a motor in run state.

Δ%I Percentage difference between current in any phase and the three-phase current average

Current Phase Reversal

Description

The current phase reversal function signals a trip when it detects that the current phases of a three-phase motor are out of sequence with the Motor Phases Sequence parameter, ABC, or ACB.

NOTE: When the LTMR controller is connected to an expansion module, phase reversal protection is based on voltage phase sequence before the motor starts, and on current phase sequence after the motor starts. In case of noisy power systems or loads, it is recommended to use voltage phase reversal protection and disable current phase reversal.

This function:

  • Is active when the motor is in start state or run state

  • Applies only to three-phase motors

  • Has no alarm and no timer.

This function can be enabled or disabled.

Functional Characteristics

The current phase reversal function adds to one counting statistic, Wiring Trips Count.

Parameter Settings

The current phase reversal function has the following configurable parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Phase sequence

  • A-B-C

  • A-C-B

A-B-C

Technical Characteristics

The current phase reversal function has the following characteristics:

Characteristic

Value

Trip time at motor startup

Within 0.2 s of motor startup

Trip time accuracy

+/– 0.1 s or +/– 5%

Long Start

Description

The long start function detects a locked or stalled rotor in start state and signals a trip when current continuously exceeds a separately set threshold for the same period of time.

Each predefined operating mode has its own current profile, representing a successful start cycle for the motor. The LTMR controller detects a long start trip condition whenever the actual current profile, occurring after a start command, varies from the expected profile.

Trip monitoring can be separately enabled and disabled.

This function has no alarm.

Start Cycle

The configurable parameters for the Long Start protection function, Long Start Trip Threshold, and Long Start Trip Timeout, are used by the LTMR controller in defining and detecting the motor’s start cycle. For more information, refer to Start Cycle.

Functional Characteristics

The long start function includes the following features:

  • One threshold:

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • One function outputs:

    • Long Start Trip

  • One counting statistic:

    • Long Start Trips Count

Block Diagram

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Is2 Trip threshold

T Trip timeout

Parameter Settings

The long start function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Enable

Trip timeout

1...200 s in 1 s increments

10 s

Trip threshold

100...800% of FLC

100% of FLC

Technical Characteristics

The long start function has the following characteristics:

Characteristic

Value

Hysteresis

– 5% of Trip threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of a single threshold cross long start trip:

Is2 Long start trip threshold

Jam

Description

The jam function detects a locked rotor during run state and signals:

  • An alarm when current in any phase exceeds a set threshold after the motor has reached run state.

  • A trip when current in any phase continuously exceeds a separately set threshold for a specified period of time after the motor has reached run state.

The jam function is triggered when the motor is jammed during run state and stops, or is suddenly overloaded and draws excessive current.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The jam function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • Jam Alarm

    • Jam Trip

  • One counting statistic:

    • Jam Trips Count

Block Diagram

Jam alarm and trip:

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Is1 Alarm threshold

Is2 Trip threshold

T Trip timeout

Parameter Settings

The jam function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Enable

Trip timeout

1...30 s in 1 s increments

5 s

Trip threshold

100...800% of FLC in 1% increments

200% of FLC

Alarm enable

Enable/Disable

Disable

Alarm threshold

100...800% of FLC in 1% increments

200% of FLC

Technical Characteristics

The jam function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of a jam trip.

Is2 Jam trip threshold

Undercurrent

Description

The undercurrent function signals:

  • An alarm when the three-phase Average Current falls below a set threshold after the motor has reached run state.

  • A trip when the three-phase Average Current falls and remains below a separately set threshold for a set period of time after the motor has reached run state.

The undercurrent function is triggered when the motor current falls below a defined level for the driven load, for example, if a drive belt or shaft has broken, allowing the motor to run free rather than under load. This function has a single trip time delay. Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The undercurrent function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • Undercurrent Alarm

    • Undercurrent Trip

  • One counting statistic:

    • Undercurrent Trips Count

Block Diagram

Undercurrent alarm and trip:

Iavg Average current

Is1 Alarm threshold

Is2 Trip threshold

T Trip timer delay

Parameter Settings

The undercurrent function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

1...200 s in 1 s increments

1 s

Trip threshold

30...100% of FLC in 1% increments

50% of FLC

Alarm enable

Enable/Disable

Disable

Alarm threshold

30...100% of FLC in 1% increments

50% of FLC

Technical Characteristics

The undercurrent function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an undercurrent trip.

Is2 Undercurrent trip threshold

Overcurrent

Description

The overcurrent function signals:

  • An alarm when current in a phase exceeds a set threshold after the motor has reached run state.

  • A trip when current in a phase continuously exceeds a separately set threshold for a set period of time after the motor has reached run state.

The overcurrent function can be triggered when the equipment is overloaded or a process condition is detected causing current to increase beyond the set threshold. This function has a single trip time delay. Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The overcurrent function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • Overcurrent Alarm

    • Overcurrent Trip

  • One counting statistic:

    • Overcurrent Trips Count

Block Diagram

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Is1 Alarm threshold

Is2 Trip threshold

T Trip timeout

Parameter Settings

The overcurrent function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

1...250 s in 1 s increments

10 s

Trip threshold

30...800% of FLC in 1% increments

200% of FLC

Alarm enable

Enable/Disable

Disable

Alarm threshold

30...800% of FLC in 1% increments

200% of FLC

Technical Characteristics

The overcurrent function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an overcurrent trip.

Is2 Overcurrent trip threshold

Ground Current

Overview

The LTMR controller can be configured to detect ground current:

Use the Ground Current Mode parameter to select either internal or external ground current trip protection. Only one of these ground current mode settings can be activated at a time.

Parameter Settings

The ground current protection function has the following configurable parameter settings, which apply to both internal and external ground current protection:

Parameters

Setting Range

Factory Setting

Ground current mode

  • Internal

  • External

Internal

Trip enable

Enable/Disable

Enable

Alarm enable

Enable/Disable

Enable

Ground current trip disabled while starting

Enable/Disable

Enable

Internal Ground Current

Description

The internal ground current function is enabled when the Ground Current Mode parameter is set to Internal and disabled when set to External.

DANGER
IMPROPER TRIP DETECTION
  • Internal ground current function will not protect people from harm caused by ground current.
  • Ground current trip thresholds must be set to protect the motor and related equipment.
  • Ground current trip settings must conform to national and local safety regulations and codes.
Failure to follow these instructions will result in death or serious injury.

The internal ground current function sums the current readings from the secondary of the internal current transformers and signals:

  • An alarm when the summed current exceeds a set threshold.

  • A trip when the summed current continuously exceeds a separately set threshold for a set period of time.

The internal ground current function has a single trip time delay.

The internal ground current function can be enabled when the motor is in ready state, start state, or run state. This function can be configured so that it is disabled during start state, and enabled only during ready state and run state.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The internal ground current function includes the following features:

  • One measure of ground current in amperes:

    • Ground Current

  • One measure of ground current as a % of FLCmin:

    • Ground Current Ratio

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • Internal Ground Current Alarm

    • Internal Ground Current Trip

  • One counting statistic:

    • Ground Current Trips Count

Block Diagram

I1 Phase 1 current

I2 Phase 2 current

I3 Phase 3 current

Summed current

IΣs1 Alarm threshold

IΣs2 Trip threshold

T Trip timeout

Parameter Settings

The internal ground current function has the following parameters:

Parameters

Setting Range

Factory Setting

Internal ground current trip timeout

0.5...25 s in 0.1 s increments

1 s

Internal ground current trip threshold

50...500% of FLCmin in 1% increments

50% of FLCmin

Internal ground current alarm threshold

50...500% of FLCmin in 1% increments

50% of FLCmin

Technical Characteristics

The internal ground current function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an internal ground current trip occurring during run state.

IΣs2 Internal ground current trip threshold

External Ground Current

Description

The external ground current function is enabled when:

  • The Ground Current Mode parameter is set to External, and

  • A current transformation ratio is set.

When Ground Current Mode is set to Internal, the external ground current function is disabled.

DANGER
IMPROPER TRIP DETECTION
  • External ground current function will not protect people from harm caused by ground current.
  • Ground current trip thresholds must be set to protect the motor and related equipment.
  • Ground current trip settings must conform to national and local safety regulations and codes.
Failure to follow these instructions will result in death or serious injury.

The LTMR controller has two terminals-Z1 and Z2-that can be connected to an external ground current sensor. The external ground current function measures ground current delivered by the secondary of the external current transformer and signals:

  • An alarm when the delivered current exceeds a set threshold.

  • A trip when the delivered current continuously exceeds a separately set threshold for a set period of time.

The external ground current function has a single trip time delay.

The external ground current function can be enabled when the motor is in ready state, start state, or run state. This function can be configured so that it is disabled only during start state, and enabled during ready state and run state.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The external ground current function includes the following features:

  • One measure of ground current in amperes:

    • Ground Current

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • External Ground Current Alarm

    • External Ground Current Trip

  • One counting statistic:

    • Ground Current Trips Count

Block Diagram

Igr Ground current from external ground CT

Igr s1 Alarm threshold

Igr s2 Trip threshold

T Trip timeout

Parameter Settings

The external ground current function has the following parameters:

Parameters

Setting Range

Factory Setting

External ground current trip timeout

0.1...25 s in 0.01 s increments

0.5 s

External ground current trip threshold

0.02...20 A in 0.01 A increments

1 A

External ground current alarm threshold

0.02...20 A in 0.01 A increments

1 A

Technical Characteristics

The external ground current function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an external ground current trip occurring during run state.

Igr s2 External ground current trip threshold

Voltage Motor Protection Functions

Overview

This section describes the voltage motor protection functions provided by the LTMR controller.

Voltage Phase Imbalance

Description

The voltage phase imbalance function signals:

  • An alarm when the voltage in any composed phase differs by more than a set percentage from the average voltage in all three phases

  • A trip when the voltage in any composed phase differs by more than a separately set percentage from the average voltage in all three phases for a set period of time

NOTE: A composed phase is the combined measure of two phases: L1 + L2, L2 + L3, or L3 + L1.

This function:

  • Is active when the LTMR controller is connected to an expansion module

  • Is active when the average voltage is between 50% and 120% of the nominal voltage

  • Is available when the motor is in ready state, start state, and run state

  • Applies only to three-phase motors

This function has two adjustable trip time delays:

  • One applies to voltage imbalances occurring while the motor is in start state, and

  • One applies to voltage imbalances occurring while the motor is in run state, or when the long start time duration expires

Both timers begin if the imbalance is detected in start state.

NOTE: Use this function to detect and guard against smaller voltage phase imbalances. For larger imbalances, in excess of 40% of the average voltage in all three phases, use the voltage phase loss motor protection function.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The voltage phase imbalance function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • Two trip time delays:

    • Trip Timeout Starting

    • Trip Timeout Running

  • Two function outputs:

    • Voltage Phase Imbalance Alarm

    • Voltage Phase Imbalance Trip

  • One counting statistic:

    • Voltage Phase Imbalance Trips Count

  • Three indicators identifying the phase with the highest voltage imbalance:

    • L1-L2 Highest Imbalance

    • L2-L3 Highest Imbalance

    • L3-L1 Highest Imbalance

Block Diagram

V1 L1-L2 voltage

V2 L2-L3 voltage

V3 L3-L1 voltage

Ln Line number or numbers with greatest deviation from Vavg

Vs1 Alarm threshold

Vs2 Trip threshold

Vavg Three-phase voltage average

T1 Trip timeout starting

T2 Trip timeout running

Parameter Settings

The voltage phase imbalance function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout starting

0.2...20 s in 0.1 s increments

0.7 s

Trip timeout running

0.2...20 s in 0.1 s increments

2 s

Trip threshold

3...15% of the calculated imbalance in 1% increments

10%

Alarm enable

Enable/Disable

Disable

Alarm threshold

3...15% of the calculated imbalance in 1% increments

10%

Technical Characteristics

The voltage phase imbalance function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of a voltage phase imbalance:

V%Δ Percentage difference between voltage in any phase and the three-phase average voltage

Vs2 Trip threshold

Voltage Phase Loss

Description

The voltage phase loss function is based on the Voltage Phase Imbalance function and signals:

  • An alarm when the voltage in any phase differs by more than 32% from the average voltage in all three phases.

  • A trip when the voltage in any phase differs by more than 32% from the average voltage in all three phases for a set period of time.

This function:

  • Is active when the LTMR controller is connected to an expansion module

  • Is active when the average voltage is between 50% and 120% of the nominal voltage

  • Is available when the motor is in ready state or start state

  • Applies only to three-phase motors

This function has a single adjustable trip time delay.

NOTE: Use this function to detect and guard against large voltage phase imbalances, in excess of 40% of the average voltage in all three phases. For smaller voltage imbalances, use the voltage phase imbalance motor protection function.

The function identifies the phase experiencing a voltage loss. If the maximum deviation from the three-phase voltage average is the same for two phases, the function identifies both phases.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The voltage phase loss function includes the following features:

  • A fixed trip and alarm threshold equal to 32% of the three-phase average voltage.

  • A single, adjustable trip time delay:

    • Voltage Phase Loss Timeout

  • Two function outputs:

    • Voltage Phase Loss Alarm

    • Voltage Phase Loss Trip

  • One counting statistic:

    • Voltage Phase Loss Trips Count

  • Three indicators identifying the phase experiencing the voltage loss:

    • L1-L2 Voltage loss

    • L2-L3 Voltage loss

    • L3-L1 Voltage loss

Block Diagram

V1 L1-L2 voltage

V2 L2-L3 voltage

V3 L3-L1 voltage

Ln Line voltage number or numbers with the greatest deviation from Vavg

Vavg Three-phase average voltage

T Trip timeout

Parameter Settings

The voltage phase loss function has the following configurable parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Enable

Trip timeout

0.1...30 s in 0.1 s increments

3 s

Alarm enable

Enable/Disable

Enable

Technical Characteristics

The voltage phase loss function has the following characteristics:

Characteristics

Value

Hysteresis

45% of the three-phase average voltage

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of a voltage phase loss trip of a motor in start state:

ΔV% Percentage difference between voltage in any phase and the three-phase average voltage

Voltage Phase Reversal

Description

The voltage phase reversal function signals a trip when it detects that the voltage phases of a three-phase motor are out of sequence, usually indicating a detected wiring error. Use the Motor Phases Sequence parameter to configure the direction, ABC or ACB, in which the motor will turn.

This function:

  • Is available when the LTMR controller is connected to an expansion module

  • Is active when the average voltage is between 50% and 120% of the nominal voltage

  • Is available when the motor is in ready state, start state and run state

  • Applies only to three-phase motors

  • Has no alarm and no timer

This function can be enabled or disabled.

Functional Characteristics

The voltage phase reversal function adds one counting statistic, Wiring Trips Count.

Parameter Settings

The voltage phase reversal function has the following configurable parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Motor phases sequence

  • A-B-C

  • A-C-B

A-B-C

Technical Characteristics

The voltage phase reversal function has the following characteristics:

Characteristics

Value

Trip time

Within 0.2 s

Trip time accuracy

+/– 0.1 s

Undervoltage

Description

The undervoltage function signals:

  • An alarm when voltage in a phase falls below a set threshold.

  • A trip when voltage in a phase falls and remains below a separately set threshold for a set period of time.

This function has a single trip time delay. Both the trip and alarm thresholds are defined as a percentage of the Motor Nominal Voltage (Vnom) parameter setting.

The undervoltage function is available only in ready state and run state when the LTMR controller is connected to an expansion module.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The undervoltage function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • Undervoltage Alarm

    • Undervoltage Trip

  • One counting statistic:

    • Undervoltage Trips Count

Block Diagram

V1 L1-L2 voltage

V2 L2-L3 voltage

V3 L3-L1 voltage

Vs1 Alarm threshold

Vs2 Trip threshold

T Trip timeout

Parameter Settings

The undervoltage function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

0.2...25 s in 0.1 s increments

3 s

Trip threshold

70...99% of Motor nominal voltage in 1% increments

85%

Alarm enable

Enable/Disable

Disable

Alarm threshold

70...99% of Motor nominal voltage in 1% increments

85%

Technical Characteristics

The undervoltage function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an undervoltage trip.

Vs2 Undervoltage trip threshold

Overvoltage

Description

The overvoltage function signals:

  • An alarm when voltage in a phase exceeds a set threshold.

  • A trip when voltage in a phase continuously exceeds a separately set threshold for a specified period of time.

This function has a single trip time delay. Both the trip and alarm thresholds are defined as a percentage of the Motor Nominal Voltage (Vnom) parameter setting.

The overvoltage function is available in ready state and run state when the LTMR controller is connected to an expansion module.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The overvoltage function includes the following features:

  • Two thresholds:

    • Alarm Threshold

    • Trip Threshold

  • One trip time delay:

    • Trip Timeout

  • Two function outputs:

    • Overvoltage Alarm

    • Overvoltage Trip

  • One counting statistic:

    • Overvoltage Trips Count

Block Diagram

V1 L1-L2 voltage

V2 L2-L3 voltage

V3 L3-L1 voltage

Vs1 Alarm threshold

Vs2 Trip threshold

T Trip timeout

Parameter Settings

The overvoltage function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

0.2...25 s in 0.1 s increments

3 s

Trip threshold

101...115% of Motor nominal voltage in 1% increments

110%

Alarm enable

Enable/Disable

Disable

Alarm threshold

101...115% of Motor nominal voltage in 1% increments

110%

Technical Characteristics

The overvoltage function has the following characteristics:

Characteristics

Value

Hysteresis

–5% of Trip threshold or Alarm threshold

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an overvoltage trip.

Vs2 Overvoltage trip threshold

Voltage Dip Management

Overview

When a voltage dip is detected, the LTMR can perform two different functions to shed and reconnect automatically the load:

Selection is done via the Voltage dip mode parameter:

If Voltage Dip Mode is...

Then...

0

Nothing happens

1

Load shedding function is enabled

2

Automatic restart function is enabled

Load Shedding and Automatic Restart functions exclude each other.

Load Shedding

Description

The LTMR controller provides load shedding, which you can use to deactivate non-critical loads if voltage level is substantially reduced. For example, use load shedding when power is transferred from a main utility supply to a backup generator system, where the backup generator system can supply power only to a limited number of critical loads.

The LTMR only monitors load shedding when Load Shedding is selected.

With the load shedding function enabled, the LTMR controller monitors the average phase voltage and:

  • Reports a load shedding condition and stops the motor when voltage falls below a configurable Voltage dip threshold and stays below the threshold for the duration of a configurable load shedding timer,

  • Clears the load shedding condition when voltage rises above a configurable Voltage dip restart threshold and remains above the threshold for the duration of a configurable Load shedding restart timer.

When the LTMR controller clears the load shedding condition:

  • In 2-wire (maintained) configuration, it issues a Run command to restart the motor,

  • In 3-wire (impulse) configuration, it does not automatically restart the motor.

In Overload motor operating mode, load shedding conditions do not affect O.1 and O.2 operating states.

In Independent motor operating mode, load shedding conditions do not affect O.2 state.

If your application includes another device that externally provides load shedding, the LTMR controller’s load shedding function should not be enabled.

All voltage dip thresholds and timers can be adjusted when the LTMR controller is in its normal operating state. When a load shedding timer is counting at the time it is adjusted, the new duration time does not become effective until the timer expires.

This function is available only when your application includes an LTME expansion module.

Functional Characteristics

The load shedding function includes the following features:

  • Two thresholds:

    • Voltage Dip Threshold

    • Voltage Dip Restart Threshold

  • Two time delays:

    • Load Shedding Timeout

    • Voltage Dip Restart Timeout

  • One status flag

    • Load Shedding

  • One counting statistic:

    • Load Sheddings Count

In addition, the load shedding function:

  • Disables logic outputs O.1 and O.2

  • Causes the alarm LED to flash 5 times per second

Parameter Settings

The load shedding function has the following parameters:

Parameters

Setting Range

Factory Setting

Voltage dip mode

0 = None

1 = Load shedding

2 = Auto restart

0 = None

Load shedding timeout

1...9999 s in increments of 1 s

10 s

Voltage dip threshold

50...115% of Motor nominal voltage

70%

Voltage dip restart timeout

1...9999 s in increments of 1 s

2 s

Voltage dip restart threshold

65...115% of Motor nominal voltage

90%

Technical Characteristics

The load shedding function has the following characteristics:

Characteristics

Value

Trip time accuracy

+/– 0.1 s or +/– 5%

Timing Sequence

The following diagram is an example of the timing sequence for the load shedding function, for a 2-wire configuration with automatic restart:

1 Motor running

2 Load shed; motor stopped

3 Load shed cleared; motor auto-restart (2-wire operation)

Automatic Restart

Description

The LTMR controller provides automatic restart.

With the automatic restart function enabled, the LTMR controller monitors the instantaneous phase voltage and detects voltage dip conditions. The voltage dip detection shares some parameters with the Load shedding function.

Three restart sequences are managed by the function according to the duration of the voltage dip:

  • Immediate restart: the motor restarts automatically.

  • Delayed restart: the motor restarts automatically after a timeout.

  • Manual restart: the motor restarts manually. A Run command is necessary.

All automatic restart timers can be adjusted when the LTMR controller is in its normal operating state. When an automatic restart timer is counting at the time it is adjusted, the new duration time does not become effective until the timer expires.

This function is available only when your application includes an LTME expansion module.

Functional Characteristics

The automatic restart function includes the following features:

  • Three time delays:

    • Auto Restart Immediate Timeout

    • Auto Restart Delayed Timeout

    • Voltage Dip Restart Timeout

  • Five status flags:

    • Voltage Dip Detection: the LTMR is in a dip condition

    • Voltage Dip Occurred: a dip has been detected in the last 4.5 seconds

    • Auto Restart Immediate Condition

    • Auto Restart Delayed Condition

    • Auto Restart Manual Condition

  • Three counting statistics:

    • Auto Restart Immediate Count

    • Auto Restart Delayed Count

    • Auto Restart Manual Count

Parameter Settings

The automatic restart function has the following parameters:

Parameters

Setting Range

Factory Setting

Voltage dip mode

0 = None

1 = Load shedding

2 = Auto restart

0 = None

Voltage dip threshold

50...115% of Motor nominal voltage

65%

Voltage dip restart threshold

65...115% of Motor nominal voltage

90%

Auto restart immediate timeout

0...0.4 s in increments of 0. 1 s

0.2 s

Auto restart delayed timeout

  • 0...300 s: timeout setting in increments of 1 s

  • 301 s: timeout infinite

4 s

Voltage dip restart timeout

0...9999 s in increments of 1 s

2 s

Technical Characteristics

The automatic restart function has the following characteristics:

Characteristics

Value

Timing accuracy

+/– 0.1 s or +/– 5%

Automatic Restart Behavior

The automatic restart behavior is characterized by the voltage dip duration that is the amount of time passed from the voltage loss until the voltage restoration.

The two possible settings are:

  • Immediate restart timeout,

  • Delayed restart timeout (with delay defined by Restart Delay Time).

The following diagram shows the automatic restart phases:

If the voltage dip duration is less than the immediate restart timeout and if the voltage dip is the second one occurring within 1 second, then the motor will require a delayed restart.

When a delayed restart is active (the delay timer is running):

  • The timer is paused for the duration of the dip if a voltage dip occurs,

  • The delayed restart is canceled if a start or stop command occurs.

Timing Sequence - Immediate Restart

The following diagram is an example of the timing sequence when an immediate restart occurs:

1 Motor running

2 Voltage dip detected, motor stopped

3 Voltage dip cleared, motor automatic restart

Timing Sequence - Delayed Restart

The following diagram is an example of the timing sequence when a delayed restart occurs:

1 Motor running

2 Voltage dip detected, motor stopped

3 Voltage dip cleared, motor automatic restart

Timing Sequence - Manual Restart

The following diagram is an example of the timing sequence when a manual restart occurs:

1 Motor running

2 Voltage dip detected, motor stopped

3 Voltage dip cleared, motor automatic restart

Power Motor Protection Functions

Overview

This section describes the power motor protection functions provided by the LTMR controller.

Underpower

Description

The underpower function signals:

  • An alarm when the value of active power falls below a set threshold.

  • A trip when the value of active power falls and remains below a separately set threshold for a set period of time.

This function has a single trip time delay. Both the trip and alarm thresholds are defined as a percentage of the Motor Nominal Power parameter setting (Pnom).

The underpower function is available only in run state when the LTMR controller is connected to an expansion module.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The underpower function includes the following features:

  • Two thresholds:

    • Underpower Alarm Threshold

    • Underpower Trip Threshold

  • One trip time delay:

    • Underpower Trip Timeout

  • Two function outputs:

    • Underpower Alarm

    • Underpower Trip

  • One counting statistic:

    • Underpower Trips Count

Block Diagram

Vavg Average rms voltage

Iavg Average rms current

P Power

Ps1 Alarm threshold

Ps2 Trip threshold

T Trip timeout

Parameter Settings

The underpower function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

1...100 s in 1 s increments

60 s

Trip threshold

20...800% of Motor nominal power in 1% increments

20%

Alarm enable

Enable/Disable

Disable

Alarm threshold

20...800% of Motor nominal power in 1% increments

30%

Technical Characteristics

The underpower function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Accuracy

+/– 5%

Example

The following diagram describes the occurrence of an underpower trip.

Ps2 Underpower trip threshold

Overpower

Description

The overpower function signals:

  • An alarm when the value of active power exceeds a set threshold.

  • A trip when the value of active power exceeds a separately set threshold and remains above that threshold for a set period of time.

This function has a single trip time delay. Both the trip and alarm thresholds are defined as a percentage of the Motor Nominal Power parameter setting (Pnom).

The overpower function is available only in run state when the LTMR controller is connected to an expansion module.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The overpower function includes the following features:

  • Two thresholds:

    • Overpower Alarm Threshold

    • Overpower Trip Threshold

  • One trip time delay:

    • Overpower Trip Timeout

  • Two function outputs:

    • Overpower Alarm

    • Overpower Trip

  • One counting statistic:

    • Overpower Trips Count

Block Diagram

Vavg Average rms voltage

Iavg Average rms current

P Power

Ps1 Alarm threshold

Ps2 Trip threshold

T Trip timeout

Parameter Settings

The overpower function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

1...100 s in 1 s increments

60 s

Trip threshold

20...800% of Motor nominal power in 1% increments

150%

Alarm enable

Enable/Disable

Disable

Alarm threshold

20...800% of Motor nominal power in 1% increments

150%

Technical Characteristics

The overpower function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Accuracy

+/– 5%

Example

The following diagram describes the occurrence of an overpower trip.

Ps2 Overpower trip threshold

Under Power Factor

Description

The under power factor protection function monitors the value of the power factor and signals:

  • An alarm when the value of the power factor falls below a set threshold.

  • A trip when the value of the power factor falls below a separately set threshold and remains below that threshold for a set period of time.

This function has a single trip time delay.

The under power factor protection function is available only in run state when the LTMR controller is connected to an expansion module.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The under power factor function includes the following features:

  • Two thresholds:

    • Under Power Factor Alarm Threshold

    • Under Power Factor Trip Threshold

  • One trip time delay:

    • Under Power Factor Trip Timeout

  • Two function outputs:

    • Under Power Factor Alarm

    • Under Power Factor Trip

  • One counting statistic:

    • Under Power Factor Trips Count

Block Diagram

cosϕs1 Under power factor alarm threshold

cosϕs2 Under power factor trip threshold

T Under power factor trip timeout

Parameter Settings

The under power factor function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

1...25 s in 0.1 s increments

10 s

Trip threshold

0...1 x Power factor in 0.01 increments

0.60

Alarm enable

Enable/Disable

Disable

Alarm threshold

0...1 x Power factor in 0.01 increments

0.60

Technical Characteristics

The under power factor function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Accuracy

+/– 3° or +/– 10% (for cos ϕ ≥ 0.6)

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an under power factor trip.

cosϕs2 Under power factor trip threshold

Over Power Factor

Description

The over power factor protection function monitors the value of the power factor and signals:

  • An alarm when the value of the power factor exceeds a set threshold.

  • A trip when the value of the power factor exceeds a separately set threshold and remains above that threshold for a set period of time.

This function has a single trip time delay.

The over power factor protection function is available only in run state, when the LTMR controller is connected to an expansion module.

Trip and alarm monitoring can be separately enabled and disabled.

Functional Characteristics

The over power factor function includes the following features:

  • Two thresholds:

    • Over Power Factor Alarm Threshold

    • Over Power Factor Trip Threshold

  • One trip time delay:

    • Over Power Factor Trip Timeout

  • Two function outputs:

    • Over Power Factor Alarm

    • Over Power Factor Trip

  • One counting statistic:

    • Over Power Factor Trips Count

Block Diagram

cosϕs1 Over power factor alarm threshold

cosϕs2 Over power factor trip threshold

T Over power factor trip timeout

Parameter Settings

The over power factor function has the following parameters:

Parameters

Setting Range

Factory Setting

Trip enable

Enable/Disable

Disable

Trip timeout

1...25 s in 0.1 s increments

10 s

Trip threshold

0...1 x Power factor in 0.01 increments

0.90

Alarm enable

Enable/Disable

Disable

Alarm threshold

0...1 x Power factor in 0.01 increments

0.90

Technical Characteristics

The over power factor function has the following characteristics:

Characteristics

Value

Hysteresis

– 5% of Trip threshold or Alarm threshold

Accuracy

+/– 3° or +/– 10% (for cos ϕ ≥ 0.6)

Trip time accuracy

+/– 0.1 s or +/– 5%

Example

The following diagram describes the occurrence of an over power factor trip.

cosϕs2 Over power factor trip threshold

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.