Use
Overview
This chapter describes:
-
The user interface devices and the hardware configurations you can use to operate the LTMR controller
-
How to set parameters with each user interface
-
How to perform monitoring, trip handling, and control functions with each user interface.
Using the LTMR Controller Stand-Alone
Overview
This section describes how to use the LTMR controller, either by itself or connected to an LTME expansion module, in a stand-alone configuration without a user interface device.
Hardware Configurations
Overview
The LTMR controller, either alone or connected to an LTME expansion module, can be operated with or without a user interface device.
In any configuration, the LTMR controller can be configured to perform monitoring, trip management, motor protection and control functions.
Communications
User interface devices and their communications interfaces include:
|
User Interface Device |
Communicates Via the |
|---|---|
|
PC running SoMove with the TeSys T DTM |
HMI port via the local RJ45 connector on the LTMR controller or LTME expansion module. |
|
PLC connected to an Ethernet network |
Network port on the LTMR Ethernet controller via the network RJ45 connector. |
|
PLC connected to a Modbus network |
Network port on the LTMR Modbus controller via the network RJ45 connector or terminal wiring |
|
PLC connected to a PROFIBUS DP network |
Network port on the LTMR PROFIBUS DP controller via the network 9-pin sub-D socket connector or terminal wiring |
|
PLC connected to a CANopen network |
Network port on the LTMR CANopen controller via the network 9-pin sub-D plug connector or terminal wiring |
|
PLC connected to a DeviceNet network |
Network port on the LTMR DeviceNet controller via terminal wiring |
LTMR Ethernet Controller Stand-Alone Configuration
Overview
Before the LTMR controller can operate in a stand-alone configuration, parameters must be set via an HMI device or SoMove software with the TeSys T DTM.
When parameters are set, the device can be detached and you can use the following controls to operate the LTMR controller:
|
Use this Control |
To |
|---|---|
|
Monitor the state of the LTMR controller and LTME expansion module |
|
Self test, manage trips, reset to factory settings |
|
Control the:
|
|
Protect the:
|
Configurations
The stand-alone physical configurations of the LTMR controller (with and without a connected LTME expansion module) are depicted below:
EtherNet/IP LTMR Controller LEDs
Use the 7 LEDs on the face of the EtherNet/IP LTMR controller to monitor its state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
HMI Comm |
Yellow |
Communication activity between LTMR controller and HMI device, PC, or LTME expansion module |
|
|
Power |
Yellow or green |
LTMR controller power or internal trip condition |
|
|
Alarm/MS |
Green or red |
Protection trip or alarm, or internal trip condition |
|
|
|||
|
|||
|
Fallback |
Red |
Indicates communication loss between the LTMR controller and network or HMI control source |
|
|
STS/NS |
Green or red |
Indicates the network status |
|
|
|||
|
|||
|
LK/ACT |
Green or yellow |
Ethernet link status Ethernet communication activity status |
|
Modbus/TCP LTMR Controller LEDs
Use the 7 LEDs on the face of the Modbus/TCP LTMR controller to monitor its state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
HMI Comm |
Yellow |
Communication activity between LTMR controller and LTME expansion module |
|
|
Power |
Green or yellow |
LTMR controller power or internal trip condition |
|
|
Alarm/MS |
Red or green |
Protection trip or alarm, or internal trip condition |
|
|
Fallback |
Red |
Communication connection between LTMR controller and network module |
|
|
STS/NS |
Green or red |
Ethernet link status Ethernet communication activity status |
|
|
LK/ACT |
Green or yellow |
Indicates the connection speed |
|
LTME Expansion Module LEDs
Use the 5 LEDs on the face of the LTME expansion module to monitor its operating and communications state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
Power |
Green or red |
Module power or internal trip condition |
|
|
Logic inputs I.7, I.8, I.9, and I.10 |
Yellow |
State of input |
|
Test/Reset
Use the Test/Reset button to perform the following LTMR controller’s functions:
|
Function |
Description |
Procedure |
|---|---|---|
|
Trip reset |
Resets all trips that can be reset. For more information about resetting trips Trip Management - Introduction. |
Press the button and release within 3 s. |
|
Self test |
Performs a self test if:
|
Press and hold the button for more than 3 s up to and including 15 s. |
|
Local return to factory setting |
Returns the LTMR controller to factory settings if the product is in one of the following states: Ready, Not ready or System configuration. If the product is in Start or Run state, the return to factory setting is ignored. When the reset button is pressed during more than 15 s, the Alarm LED blinks at 2 Hz. If the reset button is released, the product executes a reset to factory setting. |
Press and hold the button down for more than 15 s not exceeding 20 s. |
|
Induce a trip |
Put the LTMR controller into internal trip condition. |
Press and hold the button down for more than 20 s. |
LED Behavior on Power-Up
This table describes the LED sequence behavior on a LTMR controller with EtherNet/IP protocol on power-up.
|
LED Order of Sequence |
Description of Sequence |
|---|---|
|
All LEDs are OFF. |
|
|
Alarm/MS |
MS indicator lights green for 0.25 seconds. |
|
Alarm/MS |
MS indicator changes color to red and lights for 0.25 seconds. |
|
Alarm/MS |
MS indicator remains lights green. |
|
STS/NS |
NS indicator lights up green for 0.25 seconds. |
|
STS/NS |
NS indicator changes color to red for 0.25 seconds. |
|
STS/NS |
NS indicator lights off. |
|
HMI Comm |
HMI indicator lights up yellow for 0.5 seconds. |
|
HMI Comm |
HMI indicator lights off. |
|
Power |
Power indicator lights green for 0.25 seconds. |
|
Power |
Power indicator changes color to yellow and lights up for 0.25 seconds. |
|
Power |
Power indicator lights off. |
|
Fallback |
Fallback indicator lights red for 0.25 seconds. |
|
Fallback |
Fallback indicator lights off. |
LTMR Modbus Controller Stand-Alone Configuration
Overview
Before the LTMR controller can operate in a stand-alone configuration, parameters must be set via an HMI device or SoMove with the TeSys T DTM.
When parameters are set, the device can be detached and you can use the following controls to operate the LTMR controller:
|
Use this Control |
To |
|---|---|
|
Monitor the state of the LTMR controller and LTME expansion module |
|
Self test, manage trips, reset to factory settings |
|
Control the:
|
|
Protect the:
|
Configurations
The stand-alone physical configurations of the LTMR controller (with and without a connected LTME expansion module) are depicted below:
LTMR Controller LEDs
Use the 5 LEDs on the face of the LTMR controller to monitor its state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
HMI Comm |
Yellow |
Communication activity between LTMR controller and LTME expansion module |
|
|
Power |
Green |
LTMR controller power or internal trip condition |
|
|
Alarm/MS |
Red |
Protection trip or alarm, or internal trip condition |
|
|
Fallback |
Red |
Communication connection between LTMR controller and network module |
|
|
PLC Comm |
Yellow |
Communication activity on the network bus |
|
LTME Expansion Module LEDs
Use the 5 LEDs on the face of the LTME expansion module to monitor its operating and communications state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
Power |
Green or red |
Module power or internal trip condition |
|
|
Logic inputs I.7, I.8, I.9, and I.10 |
Yellow |
State of input |
|
Test/Reset
Use the Test/Reset button to perform the following LTMR controller’s functions:
|
Function |
Description |
Procedure |
|---|---|---|
|
Trip reset |
Resets all trips that can be reset. For more information about resetting trips, refer to Trip Management - Introduction. |
Press the button and release within 3 s. |
|
Self test |
Performs a self test if:
|
Press and hold the button for more than 3 s up to and including 15 s. |
|
Local return to factory setting |
Returns the LTMR controller to factory settings if the product is in one of the following states: Ready, Not ready or System configuration. If the product is in Start or Run state, the return to factory setting is ignored. When the reset button is pressed during more than 15 s, the Alarm LED blinks at 2 Hz. If the reset button is released, the product executes a reset to factory setting. |
Press and hold the button down for more than 15 s not exceeding 20 s. |
|
Induce a trip |
Put the LTMR controller into internal trip condition. |
Press and hold the button down for more than 20 s. |
LTMR PROFIBUS DP Controller Stand-Alone Configuration
Overview
Before the LTMR controller can operate in a stand-alone configuration, parameters must be set via an HMI device or SoMove with the TeSys T DTM.
When parameters are set, the device can be detached and you can use the following controls to operate the LTMR controller:
|
Use this Control |
To |
|---|---|
|
Monitor the state of the LTMR controller and LTME expansion module |
|
Self test, manage trips, reset to factory settings |
|
Control the:
|
|
Protect the:
|
Configurations
The stand-alone physical configurations of the LTMR controller (with and without a connected LTME expansion module) are depicted below:
LTMR Controller LEDs
Use the 5 LEDs on the face of the LTMR controller to monitor its state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
HMI Comm |
Yellow |
Communication activity between LTMR controller and LTME expansion module |
|
|
Power |
Green |
LTMR controller power or internal trip condition |
|
|
Alarm/MS |
Red |
Protection trip or alarm, or internal trip condition |
|
|
Fallback |
Red |
Communication connection between LTMR controller and network module |
|
|
BF |
Red |
Communication activity between LTMR controller and network module |
|
LTME Expansion Module LEDs
Use the 5 LEDs on the face of the LTME expansion module to monitor its operating and communications state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
Power |
Green or red |
Module power or internal trip condition |
|
|
Logic inputs I.7, I.8, I.9, and I.10 |
Yellow |
State of input |
|
Test/Reset
Use the Test/Reset button to perform the following LTMR controller’s functions:
|
Function |
Description |
Procedure |
|---|---|---|
|
Trip reset |
Resets all trips that can be reset. For more information about resetting trips, refer to Trip Management - Introduction. |
Press the button and release within 3 s. |
|
Self test |
Performs a self test if:
|
Press and hold the button for more than 3 s up to and including 15 s. |
|
Local return to factory setting |
Returns the LTMR controller to factory settings if the product is in one of the following states: Ready, Not ready or System configuration. If the product is in Start or Run state, the return to factory setting is ignored. When the reset button is pressed during more than 15 s, the Alarm LED blinks at 2 Hz. If the reset button is released, the product executes a reset to factory setting. |
Press and hold the button down for more than 15 s not exceeding 20 s. |
|
Induce a trip |
Put the LTMR controller into internal trip condition. |
Press and hold the button down for more than 20 s. |
LTMR CANopen Controller Stand-Alone Configuration
Overview
Before the LTMR controller can operate in a stand-alone configuration, parameters must be set via an HMI device or SoMove software with the TeSys T DTM.
When parameters are set, the device can be detached and you can use the following controls to operate the LTMR controller:
|
Use this Control |
To |
|---|---|
|
Monitor the state of the LTMR controller and LTME expansion module |
|
Self test, manage trips, reset to factory settings |
|
Control the:
|
|
Protect the:
|
Configurations
The stand-alone physical configurations of the LTMR controller (with and without a connected LTME expansion module) are depicted below:
LTMR Controller LEDs
Use the 5LEDs on the face of the LTMR controller to monitor its state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
HMI Comm |
Yellow |
Communication activity between LTMR controller and LTME expansion module |
|
|
Power |
Green |
LTMR controller power or internal trip condition |
|
|
Alarm/MS |
Red |
Protection trip or alarm, or internal trip condition |
|
|
Fallback |
Red |
Communication connection between LTMR controller and network module |
|
|
Status |
Red/green |
Communication activity between LTMR controller and network module |
|
LTME Expansion Module LEDs
Use the 5 LEDs on the face of the LTME expansion module to monitor its operating and communications state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
Power |
Green or red |
Module power or internal trip condition |
|
|
Logic inputs I.7, I.8, I.9, and I.10 |
Yellow |
State of input |
|
Test/Reset
Use the Test/Reset button to perform the following LTMR controller’s functions:
|
Function |
Description |
Procedure |
|---|---|---|
|
Trip reset |
Resets all trips that can be reset. For more information about resetting trips, refer to Trip Management - Introduction. |
Press the button and release within 3 s. |
|
Self test |
Performs a self test if:
|
Press and hold the button for more than 3 s up to and including 15 s. |
|
Local return to factory setting |
Returns the LTMR controller to factory settings if the product is in one of the following states: Ready, Not ready or System configuration. If the product is in Start or Run state, the return to factory setting is ignored. When the reset button is pressed during more than 15 s, the Alarm LED blinks at 2 Hz. If the reset button is released, the product executes a reset to factory setting. |
Press and hold the button down for more than 15 s not exceeding 20 s. |
|
Induce a trip |
Put the LTMR controller into internal trip condition. |
Press and hold the button down for more than 20 s. |
LTMR DeviceNet Controller Stand-Alone Configuration
Overview
Before the LTMR controller can operate in a stand-alone configuration, parameters must be set via an HMI device or SoMove software with the TeSys T DTM.
When parameters are set, the device can be detached and you can use the following controls to operate the LTMR controller:
|
Use this control |
To |
|---|---|
|
Monitor the state of the LTMR controller and LTME expansion module |
|
Self test, manage trips, reset to factory settings |
|
Control the:
|
|
Protect the:
|
Configurations
The stand-alone physical configurations of the LTMR controller (with and without a connected LTME expansion module) are depicted below:
LTMR Controller LEDs
Use the 5 LEDs on the face of the LTMR controller to monitor its state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
HMI Comm |
Yellow |
Communication activity between LTMR controller and LTME expansion module |
|
|
Power |
Green |
LTMR controller power or internal trip condition |
|
|
Alarm/MS |
Red |
Protection trip or alarm, or internal trip condition |
|
|
Fallback |
Red |
Communication connection between LTMR controller and network module |
|
|
MNS |
Red/green |
Communication activity between LTMR controller and network module |
|
LTME Expansion Module LEDs
Use the 5 LEDs on the face of the LTME expansion module to monitor its operating and communications state, as follows. Note the following definitions:
-
Flashing: when the LED is lit up to 250 ms whatever the time cycle is.
-
Blinking: when the LED is lit 50% of the time in the time cycle.
|
LED |
Color |
Describes |
Indicates |
|---|---|---|---|
|
Power |
Green or red |
Module power or internal trip condition |
|
|
Logic inputs I.7, I.8, I.9, and I.10 |
Yellow |
State of input |
|
Test/Reset
Use the Test/Reset button to perform the following LTMR controller’s functions:
|
Function |
Description |
Procedure |
|---|---|---|
|
Trip reset |
Resets all trips that can be reset. For more information about resetting trips, refer to Trip Management - Introduction. |
Press the button and release within 3 s. |
|
Self test |
Performs a self test if:
|
Press and hold the button for more than 3 s up to and including 15 s. |
|
Local return to factory setting |
Returns the LTMR controller to factory settings if the product is in one of the following states: Ready, Not ready or System configuration. If the product is in Start or Run state, the return to factory setting is ignored. When the reset button is pressed during more than 15 s, the Alarm LED blinks at 2 Hz. If the reset button is released, the product executes a reset to factory setting. |
Press and hold the button down for more than 15 s not exceeding 20 s. |
|
Induce a trip |
Put the LTMR controller into internal trip condition. |
Press and hold the button down for more than 20 s. |
Using the LTMCU Control Operator Unit
Presentation of the LTMCU Control Operator Unit
Aim of the Product
The LTMCU Control Operator Unit is a remote operator terminal that enables the configuration, monitoring and control of the LTMR controller, as part of the TeSys T motor management system. The LTMCU has been specially developed to act as the Human Machine Interface (HMI) of the LTMR controller, and is internally powered by the LTMR controller.
LTMCU Functions
The LTMCU HMI device can be used to:
-
Configure parameters for the LTMR controller,
-
Display information about the LTMR controller configuration and operation,
-
Monitor trips and alarms detected by the controller,
-
Control the motor locally using the local control interface.
LTMCUF Functions
The LTMCUF HMI device is similar to LTMCU HMI device with the FDR (Fast Device Replacement) service and can be used to:
-
Backup or restore the configuration and custom logic of LTMR controller.
-
Facilitate the operator task when replacing a drawer in an environment of high continuity of service without using any computer.
For More Information
Refer to the TeSys T LTMCU Control Operator Unit User’s Manual.
Configuration of the HMI Port
HMI Port
The HMI port is the RJ45 port on the LTMR controller, or on the LTME expansion module used to connect the LTMR controller to an HMI device, such as a Magelis XBT or a TeSys T LTMCU, or to a PC running SoMove with the TeSys T DTM.
Communication Parameters
Use the TeSys T DTM or the HMI to modify the HMI port communication parameters:
-
HMI port address setting
-
HMI port baud rate setting
-
HMI port parity setting
-
HMI port endian setting
HMI Port Address Setting
The HMI port address can be set between 1 and 247.
Factory setting is 1.
HMI Port Baud Rate Setting
Possible transmission rates are:
-
4800 Baud
-
9600 Baud
-
19,200 Baud (Factory setting)
HMI Port Parity Setting
The parity can be selected from:
-
Even (Factory setting)
-
None
Parity and stop bit behavior is linked:
|
If the Parity is... |
Then the Number of Stop Bts is... |
|---|---|
|
Even |
1 |
|
None |
2 |
HMI Port Endian Setting
The HMI port endian setting allows to swap the two words in a double word.
-
0 = least significant word first (little endian)
-
1 = most significant word first (big endian, factory setting)
HMI Port Fallback Setting
Fallback Condition is used to adjust the fallback mode in case of a loss of communication with the PLC.
Configuring the Magelis XBTN410
Overview
The Magelis XBTN410 HMI can be used to operate up to eight LTMR controllers, in a 1 HMI to many LTMR controllers (1-to-many) physical configuration.
The HMI presents a unique user interface, including both LCD display and keypad and requires the use of:
-
A software application file, and
-
A keypad label
This section shows you how to obtain and install a software application in the Magelis XBTN410 for a 1-to-many configuration.
Refer to the XBT-N Instruction Sheet that ships with the Magelis XBTN410 HMI for instructions on selecting and installing the keypad label that is appropriate for your configuration.
After connecting the HMI port, refer to instructions about configuring the HMI port.
Installing Magelis XBTL1000 Programming Software
Overview
The LTMR controller comes with a copy of Magelis XBTL1000 programming software. You need to:
-
Install the Magelis XBTL1000 programming software on your PC, and
-
Use it to transfer a 1-to-many software application to the Magelis XBTN410 HMI.
For instructions on how to download 1-to-many software applications, refer to Download 1-to-many Software Application Files.
For instructions on how to transfer 1-to-many software applications from your PC to the Magelis XBTN410 HM, refer to Transferring Application Software Files to Magelis XBTN410 HMI.
Installation Steps
To install the Magelis XBTL1000 programming software on your PC:
|
Step |
Action |
|---|---|
|
1 |
Place the installation disk into your PC’s disk drive. The installation program should begin. |
|
2 |
If the installation program does not begin, use Microsoft Windows® Explorer to navigate to and click the file Setup.exe. |
|
3 |
If any screens appear that do not require action, click Next. |
|
4 |
In the language screen, select a language and click OK. |
|
5 |
In the name and company screen, type your name and your company name (or accept the factory settings) and click Next. |
|
6 |
If a screen appears alerting you that protocols will be uninstalled, click Yes to continue. |
|
7 |
In the Protocols Choices screen, be sure that Modbus is selected, then click Next. |
|
8 |
In the Select Components screen, make no selections then click Next. |
|
9 |
In the Choose Destination Location screen, either accept proposed path or use the Browse button to navigate to a new one, then click Next. |
|
10 |
In the Start Copying Files screen, review your selections, and then click:
|
|
11 |
In the Finish screen, click Finish. The Magelis XBTL1000 programming software is installed. |
Download 1-to-many Software Application Files
Overview
You must download the software application file required by your installation of the Magelis XBTN410 HMI from the www.se.com website.
From the www.se.com website, you can freely obtain the software application file LTM_1T8_(language)_(version).dop.
For instructions on installing the Magelis XBTL1000 programming software, refer to Installing Magelis XBTL1000 Programming Software.
For instructions on transferring application files from the Magelis XBTL1000 programming software on your PC to the Magelis XBTN410 HMI, refer to Transferring Application Software Files to Magelis XBTN410 HMI.
Transferring Application Software Files to Magelis XBTN410 HMI
Overview
After you have installed the Magelis XBT L1000 programming software on your PC and downloaded the required 1-to-many application software file, you are ready to transfer the application software file to the Magelis XBTN410 HMI.
For instructions on downloading software application files, refer to Download 1-to-many Software Application Files.
Transfer Steps
To transfer a software application file from Magelis XBT L1000 programming software on your PC to the Magelis XBTN410 HMI:
|
Step |
Action |
|---|---|
|
1 |
Supply power to the Magelis XBTN410 HMI. |
|
2 |
Connect the PC 9-PIN Com1 port to the 25-pin data port on the HMI using an XBT Z915 programming cable. The HMI LCD reads: "FIRMWARE VX.X WAITING FOR TRANSFER" |
|
3 |
Start up the Magelis XBT_L1000 programming software. |
|
4 |
Close all child windows in the programming software. |
|
5 |
In the File menu, select Open. The Open dialog is displayed. |
|
6 |
In the Open dialog, navigate to the 1-to-many software application file (with a .dop extension) and click Open. The programming software displays the selected file. |
|
7 |
In the Transfers menu, select Export. |
|
8 |
When notified that the Export command will destroy the existing application, click OK to continue the export. The HMI LCD indicates: "DOWNLOAD IN PROGRESS" and then "DOWNLOAD COMPLETED" |
|
9 |
Click OK when the programming software reports "Transfer accomplished successfully". |
Using the Magelis XBTN410 HMI (1-to-many)
Overview
This section describes how to use the Magelis XBTN410 HMI to operate up to eight LTMR controllers, in a 1 HMI to many LTMR controllers (1-to-many) physical configuration.
The 1-to-many physical configuration presents a unique:
-
User interface (LCD display and keypad)
-
Menu structure
-
An LTMCU control operator unit, or
-
SoMove with the TeSys T DTM.
Physical Description (1-to-many)
1-to-many Interface
1-to-many Keypad
The 1-to-many configuration requires a customized keypad label. Using a blank keypad label, add the names of the six bottom buttons to the label. For instructions on creating and installing a customized keypad label, refer to the XBT-N Instruction Sheet that ships with the Magelis XBTN410 HMI.
In a 1-to-many configuration, the keypad buttons perform the following functions:
|
Keys |
Use this Key to |
|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
1-to-Many LCD
In some cases, the LCD displays only three text lines because one line-containing a trip message or page header-is twice the height of normal text.
Pages
The LCD displays pages of text. There are two types of pages:
|
Page Type |
Contains |
Displayed |
|---|---|---|
|
Menu structure page |
|
By navigating through the HMI menu structure to the specific page |
|
Trip message page |
|
|
Pages often contain more than four lines of text. For instructions on how to navigate within and between pages, refer to Navigating the Menu Structure (1-to-many).
Page Examples
The Home page:
Trip message pages:
Command Lines (1-to-many)
Overview
Use the HMI keypad
and
keys to execute text line
commands. A command line is identified by a:
A command can be executed only when its text line has focus.
A text line has focus when the
or
at either end of the text
line-plus any additional command character-is blinking.
Command Lines
The 1-to-many menu structure presents four different kinds of command lines, depending upon the command character-if any-next to the command-line arrow, as follows:
Navigating the Menu Structure (1-to-many)
Editing Values (1-to-many)
Overview
Use the HMI keypad
,
,
,
,
, and
buttons to edit setting
values. There are three kinds of editable settings:
-
Boolean
-
Numeric
-
Value list
Only settings that are displayed in the LCD can be edited. To display a setting, navigate to the page that contains the setting. With the correct page opened, you may need to scroll down to display the setting.
Boolean Settings
A boolean value setting includes a 0 or a 1 next to the
at the right end of the
text line. The following example shows you how to select and then
edit a boolean value:
1 The Settings page opens with focus at the top line.
2 Click the DOWN button to scroll down to the Local Control setting (HMI). The boolean value (0) and command-line arrow blink, indicating focus.
3 Click the RIGHT arrow to toggle the Local Control setting to Term Strip and the boolean value to 1.
Numeric Settings
Numeric value settings are incremented or decremented, and can be edited in two ways:
-
By selecting the entire setting and then incrementing or decrementing its value
-
By selecting individual characters within the setting and then incrementing or decrementing the value of each digit.
Use the
button to select the value
to be edited, as follows:
1 The Long Start page opens with no setting selected for editing.
2 Click the MOD button once to select the first displayed numerical field for editing.
3 Click the MOD button a second time to select the next displayed numerical field for editing.
Value List Settings
Executing a Value Write Command (1-to-many)
Overview
The Magelis XBTN410 HMI, in 1-to-many configuration provides executable value write commands. A value write command immediately executes a task. The value write command line is identified by either a:
If a value write command is unsuccessful, the HMI displays a detected error message.
Value write commands include:
|
Value Write Command |
Task |
Location |
|---|---|---|
|
Clear Settings |
Clears settings and restores factory settings. |
Reset to Defaults page |
|
Clear Statistics |
Clears statistics and restores factory settings. |
|
|
Self Test |
Performs a self-test. |
Controller page |
|
Reset-Manual |
Enables manual resetting of trips |
Reset page |
|
Reset-Remote |
Enables remote resetting of trips |
|
|
Reset-Automatic |
Enables automatic resetting of trips |
Example
Menu Structure (1-to-many)
Overview
The Magelis XBTN410 HMI 1-to-many menu structure is hierarchical in its design and consists of six levels of individual pages. The upper menu structure levels provide information and commands for the HMI itself and for all LTMR controllers connected to the HMI. The lower menu structure levels provide settings, statistics, and commands for a selected LTMR controller.
Menu Structure Outline
The Magelis XBTN410 HMI 1-to-many menu structure presents the following outline of levels and pages:
|
Level |
Pages |
Description |
|---|---|---|
|
1 |
Home page |
The starting page – navigation to all other pages begins here. Opens on start-up when no trips exist. |
|
2 |
Controller currents page |
|
|
Controller status page |
|
|
|
Trip pages |
Displays a series of pages, each page describing an active trip. Opens automatically when a trip exists. |
|
|
Remote reset page |
Executable commands for the remote reset of each LTMR controller. |
|
|
Reset to defaults page |
Executable commands to reset statistics or settings for each LTMR controller. |
|
|
XBTN reference page |
Describes communication settings, application program file, programming software version, and HMI firmware version. |
|
|
3 |
Controller page |
For a selected LTMR controller:
|
|
4, 5, 6 |
Settings page and sub-pages |
Contains configurable settings for a selected LTMR controller |
|
Statistics page and sub-pages |
Presents statistics for a selected LTMR controller, including trip n-0 and trip n-1 history. |
|
|
Product ID page |
LTMR controller and LTME expansion module part and firmware identification. |
Menu Structure - Home Page (1-to-many)
Overview
The Home Page opens on HMI start-up when the Magelis XBTN410 is connected to 1 or more LTMR controllers-all of which are running without trips or alarms.
The Home page is the only page located in level 1 of the Magelis XBTN410 1-to-many menu structure. It is the starting place for navigation to all other levels and pages in the menu structure.
Home Page
The Home page contains the following menu items:
|
Menu Item |
Description |
|
|---|---|---|
|
Page header with LTMR controller firmware version. |
||
|
IMPORTANT |
Links to a page with the following CAUTION message: ‘Set HMI Port Endianess to LEndian to ensure that all values are correctly displayed’. |
|
|
Controller currents |
Links to a page that displays average current and provides links to data and commands for each LTMR controller. |
|
|
Controller status |
Links to a page that displays status (On, Off, Trip) and provides links to data and commands for each LTMR controller. |
|
|
Trips |
Displays a series of trip messages. |
|
|
Remote Reset |
Links to a page that displays the status of each LTMR controller; and provides a reset command for each LTMR controller. |
|
|
Reset to defaults |
Links to a page with commands that reset to factory settings each LTMR controller’s statistics or settings. |
|
|
XBTN Reference |
Links to a page that describes communication speed and parity, programming software, and LTMR controller firmware. |
|
Menu Structure - All LTMR Controllers and the HMI (1-to-many)
Overview
Pages located in level 2 of the menu structure contain:
-
Information and commands for up to eight connected LTMR controllers, or
-
Trip information for all LTMR controllers, or
-
Information about the Magelis XBTN410 HMI
All level 2 menu structure pages are accessible from the Home page.
Controller Currents Page
Use the Controller Currents page to monitor the Average Current Ratio for all connected LTMR controllers, and to navigate to other pages as described in the following table:
|
Level 2 |
Description |
|
|---|---|---|
|
Controller Currents |
– |
|
|
Opens the Controller page for the selected LTMR controller (1-8). |
||
|
Controller status |
Opens the Controller Status page. |
|
|
Remote reset |
Opens the Remote Reset page. |
|
|
Home |
Returns to the Home page. |
|
Controller Status Page
Use the Controller Status page to monitor the System On and System Trip status of all connected LTMR controllers, and to navigate to other pages as described in the following table:
Trips Display
The Magelis XBTN410 HMI displays active trips in a series of pages-1 trip to a page-when:
-
A trip occurs, and the display of active trips automatically opens
-
You select Trips in the Home page and manually open the display of active trips.
For information about trip management, including the trips display pages, refer to Trip Management (1-to-many).
Remote Reset Page
Use the Remote Reset page to remotely execute a Trip Reset Command for a tripped LTMR controller–for controller with Trip Reset Mode set to Remote, and to navigate to other pages:
|
Level 2 |
Description |
|
|---|---|---|
|
Remote Reset |
– |
|
|
Executes a Trip Reset Command for the selected LTMR controller (1-8) if remote trip reset is enabled for that controller. |
||
|
Controller currents |
Opens the Controller Currents page. |
|
|
Controller status |
Opens the Controller Status page. |
|
|
Home |
Returns to the Home page. |
|
Reset to Defaults Page
The Reset to Defaults page provides the Clear Statistics Command and the Clear Controller Settings Command for each LTMR controller, as displayed in the following table:
|
Level 2 |
Description |
|
|---|---|---|
|
Reset to defaults |
– |
|
|
Clears statistics (left arrows) or settings (right arrows) for the selected LTMR controller (1-8), and restores factory settings. |
||
XBTN Reference Page
The XBTN Reference page provides information about the HMI. The following is an example of information displayed in this page:
|
Level 2 |
Parameter Name/Description |
|---|---|
|
XBTN Reference |
– |
|
MB Speed= 19200 |
HMI Port Baud Rate Setting |
|
MB Parity= Even |
HMI Port Parity Setting |
|
LTM_1T8_E_Vx.xx.DOP |
File name for the HMI application program |
|
XX/XX/200X xx:xx:xx |
Date of the HMI application program file |
|
XBT-L1000= V 4.42 |
Version of the XBT 1000 software |
|
Firmware= V 3.1 |
Version of the HMI firmware |
Controller Page (1-to-many)
Overview
The Controller page presents information and commands for the LTMR controller that was selected in either the Controller Currents page or the Controller Status page. For more information, refer to Controller Currents Page.
The Controller page is the only page located in level 3 of the menu structure.
Use the Controller page to:
-
Monitor dynamically changing current, voltage, and power values for a single, selected LTMR controller
-
Navigate to editable parameter settings for an LTMR controller
-
Navigate to read-only statistics and product information for an LTMR controller
-
Execute the Self Test command for an LTMR controller
Controller Page
The Controller page displays dynamically changing parameter values, and contains the command lines, as follows:
|
Level 3 |
Parameter Name/Description |
|
|---|---|---|
|
Page header indicating LTMR controller address (1-8). |
||
|
Avg Current= xxxx%FLC |
Average Current Ratio |
|
|
L1 Current= xxxx%FLC |
L1 Current Ratio |
|
|
L2 Current= xxxx%FLC |
L2 Current Ratio |
|
|
L3 Current= xxxx%FLC |
L3 Current Ratio |
|
|
GRCurr= xxxx.x%FLCmin |
Ground Current Ratio |
|
|
Curr Ph Imb= xxx%Imb |
Current Phase Imbalance |
|
|
Th Capacity= xxxxx% |
Thermal Capacity Level |
|
|
Time To Trip= xxxxSec |
Time To Trip |
|
|
Avg Voltage= xxxx%FLCmin |
Average Voltage |
|
|
L1-L2 Volts= xxxxxV |
L1-L2 Voltage |
|
|
L2-L3 Volts= xxxxxV |
L2-L3 Voltage |
|
|
L3-L1 Volts= xxxxxV |
L3-L1 Voltage |
|
|
Volt Ph Imb= xxx%Imb |
Voltage Phase Imbalance |
|
|
Power Factor= xx.xx |
Power Factor |
|
|
Active Pwr= xxxx.xkW |
Active Power |
|
|
React Pwr= xxxx.xkVAR |
Reactive Power |
|
|
Temp Sensor= xxxx.xΩ |
Motor Temp Sensor |
|
|
Settings |
Links to editable settings for the LTMR controller. |
|
|
Statistics |
Links to read-only statistics for the LTMR controller. |
|
|
Self Test v |
Executes the Self Test command. |
|
|
Product ID |
Links to product reference numbers and firmware versions for the LTMR controller and expansion module. |
|
|
Home |
Returns to the Home page. |
|
Settings (1-to-many)
Overview
The Magelis XBTN410 HMI provides several pages of editable parameter settings, nested in levels 4, 5, and 6 of the menu structure. The settings page is your starting place for locating and editing settings, including:
-
Motor
-
Local control
-
Transfer mode
-
Reset (trip)
-
Current
-
Voltage
-
Power
-
Load shed
-
Rapid cycle lockouts
-
Communication loss
The settings page is located in level 4 of the menu structure. To navigate to the settings page, use one of the following paths:
|
Level |
From this Page... |
Select... |
|---|---|---|
|
1 |
Home page |
Controller currents, or Controller status |
|
2 |
Controller Currents page, or Controller Status page |
LTMR controller number |
|
3 |
Controller page |
Settings |
Motor, Control, and Transfer Settings
Use the settings page to navigate to and edit the following motor, local control and transfer mode settings:
|
Level 4 |
Level 5 |
Parameter Name |
|---|---|---|
|
Settings Addr. 1-8 |
– |
|
|
Motor |
Nom Voltage |
Motor Nominal Voltage |
|
Nom Power (kW) |
Motor Nominal Power (expressed in kW) |
|
|
Nom Power (hp) |
Motor Nominal Power (expressed in hp) |
|
|
DirTrans |
Control Direct Transition |
|
|
TransTime |
Motor Transition Timeout |
|
|
2-step Level |
Motor Step 1 to 2 Threshold |
|
|
2-step Time |
Motor Step 1 to 2 Timeout |
|
|
Aux Fan |
Motor Auxiliary Fan Cooled |
|
|
TEMP SENSOR |
– |
|
|
Trip |
Motor Temp Sensor Trip Enable |
|
|
Trip Level |
Motor Temp Sensor Trip Threshold |
|
|
Warn |
Motor Temp Sensor Alarm Enable |
|
|
Warn Level |
Motor Temp Sensor Alarm Threshold |
|
|
Local Control |
Control Local Channel Setting |
|
|
Transfer Mode |
Control Transfer Mode |
|
Trip Reset Settings
Use the settings page to navigate to and edit the following trip reset settings:
|
Level 4 |
Level 5 |
Parameter Name |
|---|---|---|
|
Settings Addr.1-8 |
– |
|
|
Reset |
Manual |
Trip Reset Mode |
|
Remote |
||
|
Automatic |
||
|
Net Port |
Network Port Endian Setting |
|
|
AUTO GROUP 1 |
– |
|
|
Attempts |
Auto-Reset Attempts Group 1 Setting |
|
|
Reset Time |
Auto-Reset Group 1 Timeout |
|
|
AUTO GROUP 2 |
– |
|
|
Attempts |
Auto-Reset Attempts Group 2 Setting |
|
|
Reset Time |
Auto-Reset Group 2 Timeout |
|
|
AUTO GROUP 3 |
– |
|
|
Attempts |
Auto-Reset Attempts Group 3 Setting |
|
|
Reset Time |
Auto-Reset Group 3 Timeout |
|
Current Settings
From the settings page, you can navigate to and edit the following current settings:
|
Level 4 |
Level 5 |
Level 6 |
Parameter Name |
|---|---|---|---|
|
Settings Addr.1-8 |
– |
||
|
Current |
Th Overload |
Trip |
Thermal Overload Trip Enable |
|
FLC1-OC1 |
Motor Full Load Current Ratio |
||
|
FLC2-OC2 |
Motor High-Speed Full Load Current Ratio |
||
|
Trip Class |
Motor Trip Class |
||
|
Reset Level |
Thermal Overload Trip Reset Threshold |
||
|
Def O-Time |
Thermal Overload Trip Definite Timeout (O-Time) |
||
|
Def D-Time |
Long Start Trip Timeout (D-Time) |
||
|
Warn |
Thermal Overload Alarm Enable |
||
|
Warn Level |
Thermal Overload Alarm Threshold |
||
|
Phase Imb/Loss/Rev |
CURR PH IMB |
– |
|
|
Trip |
Current Phase Imbalance Trip Enable |
||
|
Trip Level |
Current Phase Imbalance Trip Threshold |
||
|
FltTimeStrt |
Current Phase Imbalance Trip Timeout Starting |
||
|
FltTimeRun |
Current Phase Imbalance Trip Timeout Running |
||
|
Warn |
Current Phase Imbalance Alarm Enable |
||
|
Warn Level |
Current Phase Imbalance Alarm Threshold |
||
|
CURR PH LOSS |
– |
||
|
Trip |
Current Phase Loss Trip Enable |
||
|
Trip Time |
Current Phase Loss Timeout |
||
|
Warn |
Current Phase Loss Alarm Enable |
||
|
CURR PH REV |
– |
||
|
Trip |
Current Phase Reversal Trip Enable |
||
|
Long Start |
Trip |
Long Start Trip Enable |
|
|
Trip Level |
Long Start Trip Threshold |
||
|
Trip Time |
Long Start Trip Timeout |
||
|
Jam |
Trip |
Jam Trip Enable |
|
|
Trip Level |
Jam Trip Threshold |
||
|
Trip Time |
Jam Trip Timeout |
||
|
Warn |
Jam Alarm Enable |
||
|
Warn Level |
Jam Alarm Threshold |
||
|
Current (continued) |
Under/Over Curr |
UNDER CURR |
– |
|
Trip |
Undercurrent Trip Enable |
||
|
Trip Level |
Undercurrent Trip Threshold |
||
|
Trip Time |
Undercurrent Trip Timeout |
||
|
Warn |
Undercurrent Alarm Enable |
||
|
Warn Level |
Undercurrent Alarm Threshold |
||
|
OVER CURR |
– |
||
|
Trip |
Overcurrent Trip Enable |
||
|
Trip Level |
Overcurrent Trip Threshold |
||
|
Trip Time |
Overcurrent Trip Timeout |
||
|
Warn |
Overcurrent Alarm Enable |
||
|
Warn Level |
Overcurrent Alarm Threshold |
||
|
Ground Current |
Trip |
Ground Current Mode |
|
|
IntFltLvl |
Internal Ground Current Trip Threshold |
||
|
IntFltTime |
Internal Ground Current Trip Timeout |
||
|
ExtFltLvl |
External Ground Current Trip Threshold |
||
|
ExtFltTime |
External Ground Current Trip Timeout |
||
|
Warn |
Ground Current Alarm Enable |
||
|
IntWarnLvl |
Internal Ground Current Alarm Threshold |
||
|
ExtWarnLvl |
External Ground Current Alarm Threshold |
||
Voltage Settings
From the settings page, you can navigate to and edit the following voltage settings:
|
Level 4 |
Level 5 |
Level 6 |
Parameter Name |
|---|---|---|---|
|
Settings Addr.1-8 |
– |
||
|
Voltage |
Phase Imb/Loss/Rev |
VOLT PH IMB |
– |
|
Trip |
Voltage Phase Imbalance Trip Enable |
||
|
Trip Level |
Voltage Phase Imbalance Trip Threshold |
||
|
FltTimeStart |
Voltage Phase Imbalance Trip Timeout Starting |
||
|
FltTimeRun |
Voltage Phase Imbalance Trip Timeout Running |
||
|
Warn |
Voltage Phase Imbalance Alarm Enable |
||
|
Warn Level |
Voltage Phase Imbalance Alarm Threshold |
||
|
VOLT PH LOSS |
– |
||
|
Trip |
Voltage Phase Loss Trip Enable |
||
|
Trip Time |
Voltage Phase Loss Trip Timeout |
||
|
Warn |
Voltage Phase Loss Alarm Enable |
||
|
VOLT PH REV |
– |
||
|
Trip |
Voltage Phase Reversal Trip Enable |
||
|
Under/Over Voltage |
UNDER VOLT |
– |
|
|
Trip |
Undervoltage Trip Enable |
||
|
Trip Level |
Undervoltage Trip Threshold |
||
|
Trip Time |
Undervoltage Trip Timeout |
||
|
Warn |
Undervoltage Alarm Enable |
||
|
Warn Level |
Undervoltage Alarm Threshold |
||
|
OVER VOLT |
– |
||
|
Trip |
Overvoltage Trip Enable |
||
|
Trip Level |
Overvoltage Trip Threshold |
||
|
Trip Time |
Overvoltage Trip Timeout |
||
|
Warn |
Overvoltage Alarm Enable |
||
|
Warn Level |
Overvoltage Alarm Threshold |
||
Power Settings
From the settings page, you can navigate to and edit the following power settings:
|
Level 4 |
Level 5 |
Level 6 |
Parameter Name |
|---|---|---|---|
|
Settings Addr.1-8 |
– |
||
|
Power |
Under/Over Power |
UNDER POWER |
– |
|
Trip |
Underpower Trip Enable |
||
|
Trip Level |
Underpower Trip Threshold |
||
|
Trip Time |
Underpower Trip Timeout Starting |
||
|
Warn |
Underpower Alarm Enable |
||
|
Warn Level |
Underpower Alarm Threshold |
||
|
OVER POWER |
– |
||
|
Trip |
Overpower Trip Enable |
||
|
Trip Level |
Overpower Trip Threshold |
||
|
Trip Time |
Overpower Trip Timeout |
||
|
Warn |
Overpower Alarm Enable |
||
|
Warn Level |
Overpower Trip Enable |
||
|
Under/Over PowFact |
UNDER POW FACTOR |
– |
|
|
Trip |
Under Power Factor Trip Enable |
||
|
Trip Level |
Under Power Factor Trip Threshold |
||
|
Trip Time |
Under Power Factor Trip Timeout |
||
|
Warn |
Under Power Factor Alarm Enable |
||
|
Warn Level |
Under Power Factor Alarm Threshold |
||
|
OVER POW FACTOR |
– |
||
|
Trip |
Over Power Factor Trip Enable |
||
|
Trip Level |
Over Power Factor Trip Threshold |
||
|
Trip Time |
Over Power Factor Trip Timeout |
||
|
Warn |
Over Power Factor Alarm Enable |
||
|
Warn Level |
Over Power Factor Alarm Threshold |
||
Load Shed, Diagnostic, Rapid Cycle Lockouts, Communication Ports Settings
From the settings page, you can navigate to and edit the following load shed, diagnostic, rapid cycle lockout, and communication ports settings:
|
Level 4 |
Level 5 |
Parameter Name |
|---|---|---|
|
Settings Addr.1-8 |
– |
|
|
Load Shed |
Trip |
Load Shedding |
|
Trip Level |
Voltage Dip Threshold |
|
|
Trip Time |
Load Shedding Timeout |
|
|
RestartLvl |
Voltage Dip Restart Threshold |
|
|
RestartTime |
Voltage Dip Restart Timeout |
|
|
Diagnostic |
DIAG TRIP |
|
|
Trip |
Diagnostic Trip Enable |
|
|
Warn |
Diagnostic Alarm Enable |
|
|
WIRING CT REVERSAL |
||
|
Trip |
Wiring trip enable |
|
|
Rapid Cycle Lockout Time |
Rapid Cycle Lockout Timeout |
|
|
Comm Ports |
Net Port |
Network Port Endian Setting |
|
HMI Port |
HMI Port Endian Setting |
|
|
NET PORT COMM LOSS |
– |
|
|
Trip |
Network Port Trip Enable |
|
|
Trip Time |
Network Port Comm Loss Timeout |
|
|
Warn |
Network Port Alarm Enable |
|
|
HMI PORT COMM LOSS |
– |
|
|
Trip |
HMI Port Trip Enable |
|
|
Warn |
HMI Port Alarm Enable |
|
Statistics (1-to-many)
Overview
The Magelis XBTN410 HMI provides read-only statistics pages–nested in levels 4 and 5 of the menu structure–for a selected LTMR controller.
To navigate to the statistics page, use one of the following paths:
|
Level |
From this Page... |
Select... |
|---|---|---|
|
1 |
Home page |
Controller currents, or Controller status |
|
2 |
Controller Currents page, or Controller Status page |
LTMR controller number |
|
3 |
Controller page |
Statistics |
Statistics
From the settings page, you can navigate to and read the following statistics:
|
Level 4 |
Level 5 |
Parameter Name |
|---|---|---|
|
Statistics Addr. 1-8 |
– |
|
|
CntrlTempMax |
Controller Internal Temperature Max |
|
|
OperTime |
Operating Time |
|
|
MtrStarts |
Motor Starts Count |
|
|
LastStartDur |
Motor Last Start Duration |
|
|
LastStart |
Motor Last Start Current |
|
|
All Trips |
Trips Count |
|
|
Th Ovld Flt |
Thermal Overload Trips Count |
|
|
Th Ovld Warn |
Thermal Overload Alarms Count |
|
|
Curr Imb Flt |
Current Phase Imbalance Trips Count |
|
|
LongStart Flt |
Long Start Trips Count |
|
|
UnderCurr Flt |
Undercurrent Trips Count |
|
|
Ground Current Trips |
Ground Current Trips Count |
|
|
VoltPhImb Flt |
Voltage Phase Imbalance Trips Count |
|
|
Under Volt Flt |
Undervoltage Trips Count |
|
|
Over Volt Flt |
Overvoltage Trips Count |
|
|
HMI Loss Flt |
HMI Port Trips Count |
|
|
Ntwk Int Flt |
Network Port Internal Trips Count |
|
|
Ntwk Cnfg Flt |
Network Port Config Trips Count |
|
|
Ntwk Port Flt |
Network Port Trips Count |
|
|
Cntrl Int Flt |
Controller Internal Trips Count |
|
|
InterPort Flt |
Internal Port Trips Count |
|
|
Trip n-0 |
Trip Code |
Trip Code n-0 |
|
Date (MMDDYYYY) |
Date And Time n-0 |
|
|
Time (HHMMSS) |
Date And Time n-0 |
|
|
FLC Ratio |
Motor Full Load Current Ratio n-0 |
|
|
FLC Max |
Motor Full Load Current Max n-0 |
|
|
Avg Current |
Average Current n-0 |
|
|
L1 Current |
L1 Current Ratio n-0 |
|
|
L2 Current |
L2 Current Ratio n-0 |
|
|
L3 Current |
L3 Current Ratio n-0 |
|
|
GRCurr |
Ground Current Ratio n-0 |
|
|
Curr Ph Imb |
Current Phase Imbalance n-0 |
|
|
Th Capacity |
Thermal Capacity Level n-0 |
|
|
Avg Volts |
Average Voltage n-0 |
|
|
L1-L2 Volts |
L1-L2 Voltage n-0 |
|
|
L2-L3 Volts |
L2-L3 Voltage n-0 |
|
|
L3-L1 Volts |
L3-L1 Voltage n-0 |
|
|
Volt Ph Imb |
Voltage Phase Imbalance n-0 |
|
|
Frequency |
Frequency n-0 |
|
|
Active Pwr |
Active Power n-0 |
|
|
Power Factor |
Power Factor n-0 |
|
|
Temp Sensor |
Motor Temp Sensor n-0 |
|
|
Trip n-1 |
Trip Code |
Trip Code n-1 |
|
Date (MMDDYYYY) |
Date And Time n-1 |
|
|
Time (HHMMSS) |
Date And Time n-1 |
|
|
FLC Ratio |
Motor Full Load Current Ratio n-1 |
|
|
FLC Max |
Motor Full Load Current Max n-1 |
|
|
Avg Current |
Average Current n-1 |
|
|
L1 Current |
L1 Current Ratio n-1 |
|
|
L2 Current |
L2 Current Ratio n-1 |
|
|
L3 Current |
L3 Current Ratio n-1 |
|
|
GRCurr |
Ground Current Ratio n-1 |
|
|
Curr Ph Imb |
Current Phase Imbalance n-1 |
|
|
Th Capacity |
Thermal Capacity Level n-1 |
|
|
Avg Volts |
Average Voltage n-1 |
|
|
L1-L2 Volts |
L1-L2 Voltage n-1 |
|
|
L2-L3 Volts |
L2-L3 Voltage n-1 |
|
|
L3-L1 Volts |
L3-L1 Voltage n-1 |
|
|
Volt Ph Imb |
Voltage Phase Imbalance n-1 |
|
|
Frequency |
Frequency n-1 |
|
|
Active Pwr |
Active Power n-1 |
|
|
Power Factor |
Power Factor n-1 |
|
|
Temp Sensor |
Motor Temp Sensor n-1 |
|
Product ID (1-to-many)
Overview
The Magelis XBTN410 HMI provides a description of the product number and firmware for both the LTMR controller and LTME expansion module.
To navigate to the Product ID page, use one of the following paths:
|
Level |
From this Page... |
Select... |
|---|---|---|
|
1 |
Home page |
Controller currents, or Controller status |
|
2 |
Controller Currents page, or Controller Status page |
LTMR controller number |
|
3 |
Controller page |
Product ID |
Product ID
In the Product ID page, you can read the following information about the LTMR controller and LTME expansion module:
|
Level 4 |
Parameter Name/Description |
|---|---|
|
Product ID Addr. 1-8 |
– |
|
Controller Catalog Ref |
Controller Commercial Reference (product number) |
|
Controller Firmware |
Controller Firmware Version |
|
Exp Module Catalog Ref |
Expansion Commercial Reference (product number) |
|
Exp Module Firmware |
Expansion Firmware Version |
|
Network Type |
Network Port ID Code |
|
Network Firmware |
Network Port Firmware Version |
Monitoring (1-to-many)
Overview
Use the Magelis XBTN410 HMI, in a 1-to-many configuration, to monitor:
-
Operating status and average current for multiple LTMR controllers, or
-
Current, voltage, and power parameters for a selected LTMR controller.
Monitoring Multiple LTMR Controllers
Navigate to the following pages to simultaneously monitor these dynamically changing values for all LTMR controllers:
|
Page |
Value |
|---|---|
|
Controller currents page |
Average current ratio |
|
Controller status page |
Operating status (On, Off, Trip) |
For more information on both pages, refer to Controller Currents Page.
Monitoring a Single LTMR Controller
Navigate to the Controller page for a selected LTMR controller to monitor the dynamically changing values of the following parameters:
-
Current:
-
Average Current Ratio
-
L1 Current Ratio
-
L2 Current Ratio
-
L3 Current Ratio
-
Ground Current Ratio
-
Current Phase Imbalance
-
-
Thermal
-
Thermal Capacity Level
-
Time To Trip
-
Motor Temp Sensor
-
-
Voltage
-
Average Voltage
-
L1-L2 Voltage
-
L2-L3 Voltage
-
L3-L1 Voltage
-
Voltage Phase Imbalance
-
-
Power
-
Power Factor
-
Active Power
-
Reactive Power
-
For more information on the Controller page, refer to Controller Page (1-to-many).
Trip Management (1-to-many)
Overview
When a trip occurs, the Magelis XBTN410 HMI automatically opens a trip display, consisting of one page for each active trip. Each page contains the:
-
Trip name
-
Address of the LTMR controller experiencing the trip
-
Total number of unresolved trips
Trip Display Pages
If more than one trip is active, use the
and
keypad buttons to move back
and forth through the trip display pages.
Because some trip
messages contain more than four lines of text, you may need to use
the
and
keypad buttons to scroll
up and down within a trip display page and display the entire trip
message.
Opening/Closing the Trip Display
The 1-to-many HMI automatically opens the trip display whenever a trip occurs. When you remove the cause of a specific trip and execute a trip reset command, that trips no longer appears in the trip display.
You can also close the trip display by clicking the
keypad button. This does
not fix the underlying cause of any trip, nor it does not clear any
trip. You can reopen the trip display at any time by navigating to
the Home page, scrolling to the Trips command line, then clicking
the
keypad button.
If you open the trip display when no trips are active, the HMI displays the message "".
Magelis XBT Communication Loss
If a key is pressed while the Magelis XBT HMI device loses communication, the keypad update will not be complete. When the communication with the LTMR is back, the following message displays: "". Press any key or power cycle the device.
Service Commands (1-to-many)
Overview
The Magelis XBTN410, in 1-to-many configuration, provides the following service commands:
|
Command |
Description |
Location/Reference |
|---|---|---|
|
Self Test |
Performs an internal check of the LTMR controller and LTME expansion module. |
Level 3, Controller page. Refer to Controller Page. |
|
Reset to Defaults: Statistics |
Executes the Clear Statistics Command for a selected LTMR controller. |
Level 2, Reset to Defaults page. Refer to Reset to Defaults Page. |
|
Reset to Defaults: Settings |
Executes the Clear Controller Settings Command for a selected LTMR controller. |
Level 2, Reset to Defaults page. Refer to Reset to Defaults Page. |
|
Remote Reset |
Performs remote trip reset for a selected LTMR controller |
Level 2, Remote Reset page. Refer to Remote Reset Page |
Using SoMove with the TeSys T DTM
Overview
The following topics show you how to use the LTMR controller when it is connected to a PC running SoMove with the TeSys T DTM.
Presentation of SoMove with the TeSys T DTM
Aim of the Software
SoMove software is a Microsoft Windows-based application, using the open FDT/DTM technology.
SoMove contains DTMs for different devices. The TeSys T DTM is a specific DTM that enables the configuration, monitoring, control, and customization of the control functions of the LTMR controller, as part of the TeSys T motor management system.
Functions
The TeSys T DTM can be used to:
-
Configure parameters for the LTMR controller,
-
Display information about the LTMR controller configuration and operation,
-
Display the status of trips and alarms in the LTMR controller,
-
Control the motor,
-
Customize operating modes.
For More Information
Refer to the TeSys T DTM for SoMove FDT Container Online Help embedded in the DTM software.
Installing SoMove and the TeSys DTM Library
Overview
The installation of SoMove includes some DTMs such as the TeSys DTM library.
The TeSys DTM library includes:
-
TeSys T DTM
-
TeSys U DTM
These DTM are automatically installed during the SoMove installation process.
Downloading SoMove
SoMove can be downloaded
from the Schneider Electric website (www.se.com) by entering SoMove Lite in the field.
Installing SoMove
|
Step |
Action |
|---|---|
|
1 |
Unzip the downloaded file: the SoMove file is unzipped in a folder named SoMove_Lite - V.X.X.X.X (where X.X.X.X is the version number). Open this folder and double-click . |
|
2 |
In the dialog box, select the installation language. |
|
3 |
Click . |
|
4 |
In the dialog box, click the button. |
|
5 |
If an dialog box appears and informs you that you must install Modbus driver, click the button. Result: Modbus driver is installed automatically. |
|
6 |
In the dialog box, click the button. |
|
7 |
In the dialog box, click the button. |
|
8 |
In the dialog box:
|
|
9 |
In the dialog box:
|
|
10 |
In the dialog box:
|
|
11 |
In the dialog box:
|
|
12 |
In the dialog box, click the button. Result: The SoMove Lite components are installed automatically:
|
|
13 |
In the dialog box, click the button. Result: SoMove Lite is installed on your computer. |