DOCA0127EN-03

Introducing the TeSys T Motor Management System

Overview

This chapter introduces the TeSys T motor management system and its companion devices.

Presentation of the TeSys T Motor Management System

Aim of the Product

The TeSys T motor management system offers protection, control, and monitoring capabilities for single-phase and three-phase AC induction motors.

The system is flexible, modular, and can be configured to meet the requirements of applications in industry. The system is designed to meet the needs for integrated protection systems with open communications and a global architecture.

Highly accurate sensors and solid-state full motor protection provide better utilization of the motor. Complete monitoring functions enable analysis of motor operating conditions and faster responses to prevent system downtime.

The system offers diagnostic and statistics functions and configurable alarms and trips, allowing better prediction of component maintenance, and provides data to continuously improve the entire system.

Examples of Supported Machine Segments

The motor management system supports the following machine segments:

Machine Segment

Examples

Process and special machine segments

Water and waste water treatment

  • Water treatment (pump, blowers, and agitators)

Metal, Minerals, and Mining

  • Cement

  • Glass

  • Steel

  • Ore extraction

Oil and gas

  • Oil and gas processing

    • Petrochemical

    • Refinery, Offshore platform

Microelectronic

Pharmaceutical

Chemical industry

  • Cosmetics

  • Detergents

  • Fertilizers

  • Paint

Transportation industry

  • Automotive transfer lines

  • Airports

  • Subway

Other industry

  • Tunnel machines

Complex machine segments

Includes highly automated or coordinated machines used in:

  • Pumping systems

  • Paper conversion

  • Printing lines

  • HVAC

Supported Industries

The motor management system supports the following industries and associated business sectors:

Industry

Sectors

Application

Building

  • Office buildings

  • Shopping centers

  • Industrial buildings

  • Ships

  • Hospitals

  • Cultural facilities

  • Airports

Control and manage the building facilities:

  • Critical HVAC systems

  • Water

  • Air

  • Gas

  • Electricity

  • Steam

Industry

  • Metal, mineral, and mining: cement, glass, steel, ore-extraction

  • Microelectronic

  • Petrochemical

  • Ethanol

  • Chemical: pulp and paper industry

  • Pharmaceutical

  • Food and beverage

  • Control and monitor pump motors

  • Control ventilation

  • Control load traction and movements

  • View status and communicate with machines

  • Process and communicate the data captured

  • Remotely manage data for one or several sites via the Internet

Energy and Infrastructure

  • Water treatment and transportation

  • Transportation infrastructure for people and freight: airports, road tunnels, subways, and tramways

  • Power generation and transport

  • Control and monitor pump motors

  • Control ventilation

  • Remotely control wind turbine

  • Remotely manage data for one or several sites via the Internet

TeSys T Motor Management System

The two main hardware components of the system are the LTMR controller and the LTME expansion module.

The microprocessor-based LTMR controller is the central component in the system that manages the control, protection, and monitoring functions of single-phase or three‑phase AC induction motors.

The LTMR controller is designed to work over the following networks:

  • An Ethernet network either through Modbus/TCP communication protocol or through EtherNet/IP communication

  • The Modbus network

  • The PROFIBUS DP network

  • The CANopen network

  • The DeviceNet network

The system can be configured and controlled:

  • Using an HMI (Human Machine Interface) device: Magelis XBT or TeSys T LTMCU.

  • Using a PC running SoMove with the TeSys T DTM.

  • Using a PLC connected to the system via the communication network.

  • Using the Ethernet Web server (for LTMR Ethernet controller only.)

Components such as external motor load current transformers and ground current sensors add additional range to the system.

LTMR Controller

The following table introduces the functions of the LTMR controllers:

LTMR Controller

Functional Description

  • Current sensing 0.4...100 A

  • Single-phase or three-phase current inputs

  • Six discrete logic inputs

  • Four relay outputs: three SPST, one DPST

  • Connections for a ground current sensor

  • Connection for a motor temperature sensor

  • Connection for a communication network

  • Connection for HMI device or expansion module

  • Current protection, metering, and monitoring functions

  • Motor control functions

  • Power indicator and communication protocol selection indicator

  • Trip and alarm LED indicators

  • Network communication and alarm indicators

  • HMI communication LED indicator

  • Test and reset function

NOTE: LTMR Ethernet controllers communicating over an Ethernet network can communicate either using the Modbus/TCP communication protocol or using the Ethernet/IP communication protocol.

Both protocols are loaded in the controller. The controller is pre-configured to communicate through Modbus/TCP protocol. Changing its configuration allows to switch to Ethernet/IP protocol.

LTMR Controller Reference Number Description

The following tables describe the LTMR controller’s reference number: LTMRxxyzz

xx

Rating

08

0.4...8 A

27

1.36...27 A

100

5...100 A

y

Communication Protocol

E

Ethernet (Modbus/TCP and Ethernet/IP)

M

Modbus SL

P

PROFIBUS DP

C

CANopen

D

DeviceNet

zz

Control Voltage

BD

24 Vdc

FM

100...240 Vac

LTME Expansion Module

There are two models of LTME expansion modules that provide voltage monitoring functionality and four additional logic inputs. The LTME expansion modules are powered by the LTMR controller via a connector cable.

LTME Expansion Module

Functional Description

Reference Number

  • Voltage sensing 110...690 Vac, 47...63 Hz

  • Three-phase voltage inputs

  • Four additional discrete logic inputs

  • Additional voltage protection, metering, and monitoring functions

  • Power LED indicator

  • Logic input status LED indicators

Additional components required for an optional expansion module:

  • LTMR controller to LTME connection cable

LTMEV40BD (24 Vdc logic inputs)

LTMEV40FM (100...240 Vac logic inputs)

HMI Device: Magelis XBTN410 (Discontinued)

The system uses the Magelis XBTN410 HMI device with a liquid crystal display.

Magelis XBTN410

Functional Description

Reference Number

  • Configures the system through menu entries

  • Displays parameters, alarms, and trips

Additional components required for an optional HMI device:

  • Separate power source

  • LTMR/LTME to HMI communication cable

  • Magelis XBTL1000 programming software

XBTN410 (HMI)

XBTZ938 (cable)

XBTL1000 (software)

HMI Device: LTMCU Control Operator Unit

The system uses the TeSys T LTMCU Control Operator Unit HMI device with a liquid crystal display and contextual navigation keys. The LTMCU is internally powered by the LTMR. Refer to the TeSys T LTMCU Control Operator Unit User Manual for more information.

LTMCU Control Operator Unit

Functional Description

Reference Number

  • Configures the system through menu entries

  • Displays parameters, alarms, and trips

  • Controls the motor

  • Provides the FDR (Fast Device Replacement) service (only with LTMCUF with embedded memory)

Additional components required for an optional HMI device:

  • LTMR/LTME to HMI communication cable

LTMCU (HMI device)

LTMCUF (HMI device with FDR service)

LTM9CU•0

(HMI communication cable)

TCSMCNAM3M002P

(cable kit)

LTM9KCU

(Kit for portable LTMCU)

SoMove with the TeSys T DTM

SoMove software is a Microsoft Windows® based application, using the open FDT/DTM technology.

SoMove contains many DTMs. A specific DTM exists for the TeSys T motor management system.

SoMove with the TeSys T DTM

Functional Description

Reference Number

  • configure the system through menu entries

  • Display parameters, alarms, and trips

  • Control the motor

  • Enable customization of operating modes

Additional components required for the SoMove FDT container:

  • A PC

  • separate power source

  • LTMR / LTME / LTMCU to PC communication cables

SoMove with the TeSys T DTM

TCSMCNAM3M002P

(cable kit)

Load Current Transformers

External load current transformers expand the current range for use with motors greater than 100 full load Amperes.

Schneider Electric Load Current Transformers

Primary

Secondary

Inside Diameter

Reference Number

mm

In.

100

1

35

1.38

LT6CT1001

200

1

35

1.38

LT6CT2001

400

1

35

1.38

LT6CT4001

Note: The following current transformers are also available: Schneider Electric LUTC0301, LUTC0501, LUTC1001, LUTC2001, LUTC4001, and LUTC8001.

Ground Current Sensors

External ground current sensors measure ground current trip conditions.

Schneider Electric Vigirex Ground Current Transformers

Type

Maximum Current

Inside Diameter

Transformation Ratio

Reference Number

mm

In.

TA30

65 A

30

1.18

1000:1

50437

PA50

85 A

50

1.97

50438

IA80

160 A

80

3.15

50439

MA120

250 A

120

4.72

50440

SA200

400 A

200

7.87

50441

PA300

630 A

300

11.81

50442

POA

85 A

46

1.81

50485

GOA

250 A

110

4.33

50486

Cables

System components require cables to connect to other components and communicate with the network.

Connection to....

Cable

Description

Reference Number

LTME expansion module

Connecting jumper 0.04 m (1.57 in.) length, for side by side connection of the LTMR and LTME

LTMCC004

LTMR to LTME RJ45 connector cable 1.0 m (3.28 ft) length

LTM9CEXP10

Ethernet network

Category 5 shielded/unshielded twisted-pair network connection cables with two RJ45 connectors

490 NTW 000 •••

Modbus network

Modbus network communication cable 0.3 m (11.81 in.) length

VW3A8306R03

Modbus network communication cable 1.0 m (3.28 ft) length

VW3A8306R10

Modbus network communication cable 3.0 m (9.84 ft) length

VW3A8306R30

PROFIBUS DP network

PROFIBUS DP network communication cable 100 m (328.08 ft) length

TSXPBSCA100

PROFIBUS DP network communication cable 400 m (1,312.33 ft) length

TSXPBSCA400

CANopen network

LZSH CANopen network communication cable 0.3 m (11.81 in) length

TSXCANCADD03

UL/IEC332-2 CANopen network communication cable 0.3 m (11.81 in) length

TSXCANCBDD03

LZSH CANopen network communication cable 1.0 m (3.28 ft) length

TSXCANCADD1

UL/IEC332-2 CANopen network communication cable 1.0 m (3.28 ft) length

TSXCANCBDD1

LZSH CANopen network communication cable 3.0 m (9.84 ft) length

TSXCANCADD3

UL/IEC332-2 CANopen network communication cable 3.0 m (9.84 ft) length

TSXCANCBDD3

LZSH CANopen network communication cable 5.0 m (16.40 ft) length

TSXCANCADD5

UL/IEC332-2 CANopen network communication cable 5.0 m (16.40 ft) length

TSXCANCBDD5

LTMCU HMI

LTMR/LTME to LTMCU HMI device connection cable 1.0 m (3.28 ft) length

LTM9CU10

LTMR/LTME to LTMCU HMI device connection cable 3.0 m (9.84 ft) length

LTM9CU30

PC

Cable kit, includes LTME / LTMR / LTMCU to PC communication cable 2.5 m (8.2 ft) length

TCSMCNAM3M002P

System Selection Guide

Overview

This section describes the LTMR controller with and without the optional LTME expansion module for metering and monitoring, protection, and control functions.

  • Metering and Monitoring functions

    • Measurement

    • Trip and alarm counters

    • System and device monitoring trips

    • Motor history

    • System operating status

  • Protection functions

    • Thermal motor protection

    • Current motor protection

    • Voltage and power motor protection

  • Control functions

    • Control channels (local/remote control source selection)

    • Operating modes

    • Trip management

Metering Functions

The following table lists the equipment required to support the metering functions of the motor management system:

Function

LTMR Controller

LTMR with LTME

Measurement

Line currents

X

X

Ground current

X

X

Average current

X

X

Current phase imbalance

X

X

Thermal capacity level

X

X

Motor temperature sensor

X

X

Frequency

X

Line-to-line voltage

X

Line voltage imbalance

X

Average voltage

X

Power factor

X

Active power

X

Reactive power

X

Active power consumption

X

Reactive power consumption

X

System and Device Monitoring Trips

Controller internal trips

X

X

Controller internal temperature

X

X

Control command trip diagnostic

X

X

Wiring trip - Temperature sensor connections

X

X

Wiring trip - Current connections

X

X

Wiring trip - Voltage connections

X

Configuration checksum

X

X

Communication loss

X

X

Time to trip

X

X

Trip and alarm counters

Protection trip counts

X

X

Protection alarm counts

X

X

Diagnostic trip counts

X

X

Motor control function counts

X

X

Trip history

X

X

Motor History

Motor starts / O1 starts / O2 starts

X

X

Operating time

X

X

Motor starts per hour

X

X

Motor last start current ratio

X

X

Motor last start duration

X

X

System Operating Status

Motor running

X

X

Motor ready

X

X

Motor starting

X

X

Minimum wait time

X

X

X The function is available

The function is not available

Protection Functions

The following table lists the equipment required to support the protection functions of the motor management system:

Functions

LTMR Controller

LTMR with LTME

Thermal overload

X

X

Current phase imbalance

X

X

Current phase loss

X

X

Current phase reversal

X

X

Long start

X

X

Jam

X

X

Undercurrent

X

X

Overcurrent

X

X

Ground current

X

X

Motor temperature sensor

X

X

Rapid cycle lockout

X

X

Voltage phase imbalance

X

Voltage phase loss

X

Voltage phase reversal

X

Undervoltage

X

Overvoltage

X

Load shedding

X

Underpower

X

Overpower

X

Under power factor

X

Over power factor

X

X The function is available

The function is not available

Control Functions

The following table lists the equipment required to support the control functions of the motor management system:

Control functions

LTMR Controller

LTMR with LTME

Motor control channels

Terminal strip

X

X

HMI

X

X

Remote

X

X

Operating mode

Overload

X

X

Independent

X

X

Reverser

X

X

Two-step

X

X

Two-speed

X

X

Custom

X

X

Trip Management

Manual reset

X

X

Automatic reset

X

X

Remote reset

X

X

X The function is available

The function is not available

Firmware Update Policy

Firmware update is recommended to benefit from the latest features and potential bug fixes. Update the firmware to the latest version when the latest features and bug fixes are required for your application. Use the firmware release notes to confirm if an update to the latest version of the firmware is relevant for your application. The latest firmware and release notes can be found together by searching for "TeSys T Firmware" at www.se.com.

Firmware Update with TeSys Programmer

Use the latest version of TeSys Programmer software to update the TeSys T range of devices with the latest firmware version available. The latest version of TeSys Programmer software is available at www.se.com. For more information on the use of TeSys Programmer software, refer to TeSys Programmer Help document that is provided with the software.

Physical Description of the LTMR Ethernet Controller

Phase Current Inputs

The LTMR controller includes internal current transformers for measuring the motor load phase current directly from the motor load power cables or from secondaries of external current transformers.

1 Windows for phase current measurement

Front Face

The LTMR controller front face includes the following features:

1 Test / Reset button

2 LTME / HMI port with RJ45 connector connecting the LTMR controller to an HMI, PC, or LTME expansion module

3 Ethernet port number 1 with RJ45 connector connecting the LTMR controller to a Modbus/TCP network

4 Ethernet port number 2 with RJ45 connector connecting the LTMR controller to a Modbus/TCP network

5 LTMR status-indicating LEDs

6 Plug-in terminal: control power, logic inputs, and commons

7 Plug-in terminal: double pole/single throw (DPST) output relay

8 Plug-in terminal output relay

9 Plug-in terminal: ground current trip input and temperature sensor input

10 Rotary switches (Tens and Ones) for IP addressing

11 Ethernet port link and activity LEDs

12 MAC address

Test / Reset Button

The Test / Reset button performs a reset, self-test, or places the LTMR controller in an internal trip state.

HMI Device/Expansion Module/PC Port

This port connects the LTMR controller to the following devices over the HMI port using an RJ45 connector:

  • An expansion module

  • A LTMCU/LTMCUF

  • A PC running SoMove with the TeSys T DTM

  • A Magelis XBTN410 HMI

LTMR Status Indicating LEDs

LED Name

Description

HMI Comm

Communication between LTMR controller and HMI device, PC, or LTME expansion module

Power

LTMR controller power or internal trip condition, motor status, and configured communication protocol

Alarm/MS

Protection alarm or trip, or internal trip indicator

Fallback

Indicates communication loss between the LTMR controller and network or HMI control source

STS/NS

Network status indicator

Ethernet Port Link and Activity LEDs

LED Name

Description

LK/ACT

Ethernet link status

Ethernet communication activity status

Physical Description of the LTMR Modbus Controller

Phase Current Inputs

The LTMR controller includes internal current transformers for measuring the motor load phase current directly from the motor load power cables or from secondaries of external current transformers.

1 Windows for phase current measurement

Front Face

The LTMR controller front face includes the following features:

1 Test / Reset button

2 HMI port with RJ45 connector connecting the LTMR controller to an HMI, PC, or LTME expansion module

3 Network port with RJ45 connector connecting the LTMR controller to Modbus network

4 LTMR status-indicating LEDs

5 Plug-in terminal: control power, logic inputs, and commons

6 Plug-in terminal: double pole/single throw (DPST) output relay

7 Plug-in terminal output relay

8 Plug-in terminal: ground current trip input and temperature sensor input

9 Plug-in terminal: Modbus network

Test / Reset Button

The Test / Reset button performs a reset, self-test, or places the LTMR controller in an internal trip state.

HMI Device/Expansion Module/PC Port

This port connects the LTMR controller to the following devices over the HMI port using an RJ45 connector:

  • An expansion module

  • A LTMCU/LTMCUF

  • A PC running SoMove with the TeSys T DTM

  • A Magelis XBTN410 HMI

LTMR Status Indicating LEDs

LED Name

Description

HMI Comm

Communication between LTMR controller and HMI device, PC, or LTME expansion module

Power

LTMR controller power or internal trip condition

Alarm

Protection alarm or trip, or internal trip

Fallback

Communication loss between the LTMR controller and network or HMI control source

PLC Comm

Network activity

Physical Description of the LTMR PROFIBUS DP Controller

Phase Current Inputs

The LTMR controller includes internal current transformers for measuring the motor load phase current directly from the motor load power cables or from secondaries of external current transformers.

1 Windows for phase current measurement

Front Face

The LTMR controller front face includes the following features:

1 Test / Reset button

2 HMI port with RJ45 connector connecting the LTMR controller to an HMI, PC, or LTME expansion module

3 Network port with nine-pin sub-D connector connecting the LTMR controller to a PROFIBUS DP PLC

4 LTMR status-indicating LEDs

5 Plug-in terminal: control power, logic Input, and common

6 Plug-in terminal: double pole/single throw (DPST) relay output

7 Plug-in terminal relay output

8 Plug-in terminal: ground current trip input and temperature sensor input

9 Plug-in terminal: PLC network

Test / Reset Button

The Test / Reset button performs a reset, self-test, or places the LTMR controller in an internal trip state.

HMI Device/Expansion Module/PC Port

This port connects the LTMR controller to the following devices over the HMI port using an RJ45 connector:

  • An expansion module

  • A LTMCU/LTMCUF

  • A PC running SoMove with the TeSys T DTM

  • A Magelis XBTN410 HMI

Network Port

This port provides communication between the LTMR controller and a network PLC via a 9-pin sub-D socket connector.

LTMR Status Indicating LEDs

LED Name

Describes

Appearance

Status

HMI Comm

Communication between LTMR controller and HMI device, PC, or LTME expansion module

Flashing yellow

Communication

OFF

No communication

Power

LTMR controller power or internal trip condition

Solid green

Power ON, motor OFF, no internal trips

Flashing green

Power ON, motor ON, no internal trips

OFF

Power OFF or internal trips exist

Alarm

Protection alarm or trip, or internal trip

Solid red

Internal or protection trip

Flashing red – 2 X per second

Alarm

Flashing red – 5 X per second

Load shed or rapid cycle

OFF

No trips, alarms, load shed, or rapid cycle (when power is ON)

Fallback

Indicates communications loss between the LTMR controller and network or HMI control source

Solid red

Fallback

OFF

No power (not in fallback)

BF

Indicates network status

OFF

Communication

Red

No communication

Physical Description of the LTMR CANopen Controller

Phase Current Inputs

The LTMR controller includes internal current transformers for measuring the motor load phase current directly from the motor load power cables or from secondaries of external current transformers.

1 Windows for phase current measurement

Front Face

The LTMR controller front face includes the following features:

1 Test / Reset button

2 HMI port with RJ45 connector connecting the LTMR controller to an HMI, PC, or LTME expansion module

3 LTMR status-indicating LEDs

4 Network port with nine-pin sub-D connector connecting the LTMR controller to a CANopen PLC

5 Plug-in terminal: control power, logic Input, and common

6 Plug-in terminal: double pole/single throw (DPST) relay output

7 Plug-in terminal relay output

8 Plug-in terminal: ground current trip input and temperature sensor input

9 Plug-in terminal: PLC network

Test / Reset Button

The Test / Reset button performs a reset, self-test, or places the LTMR controller in an internal trip state.

HMI Device/Expansion Module/PC Port

This port connects the LTMR controller to the following devices over the HMI port using an RJ45 connector:

  • An expansion module

  • A LTMCU/LTMCUF

  • A PC running SoMove with the TeSys T DTM

  • A Magelis XBTN410 HMI

Network Port

This port provides communication between the LTMR controller and a network PLC via a 9-pin sub-D plug connector.

LTMR Status Indicating LEDs

LED Name

Describes

Appearance

Status

HMI Comm

Communication between LTMR controller and HMI device, PC, or expansion module

Flashing yellow

Communication

OFF

No communication

Power

LTMR controller power or internal trip condition

Solid green

Power ON, motor OFF, no internal trips

Flashing green

Power ON, motor ON, no internal trips

OFF

Power OFF or internal trips exist

Alarm

Protection alarm or trip, or internal trip

Solid red

Internal or protection trip

Flashing red – 2 X per second

Alarm

Flashing red – 5 X per second

Load shed or rapid cycle

OFF

No trips, alarms, load shed, or rapid cycle (when power is ON)

Fallback

Indicates communications loss between the LTMR controller and network or HMI control source

Solid red

Fallback

OFF

No power (not in fallback)

Status

Indicates network status

Green

Communication

Red

No communication

Physical Description of the LTMR DeviceNet Controller

Phase Current Inputs

The LTMR controller includes internal current transformers for measuring the motor load phase current directly from the motor load power cables or from secondaries of external current transformers.

1 Windows for phase current measurement

Front Face

The LTMR controller front face includes the following features:

1 Test/Reset button

2 HMI port with RJ45 connector connecting the LTMR controller to an HMI, PC, or LTME expansion module

3 LTMR status-indicating LEDs

4 Plug-in terminal: control power, logic Input, and common

5 Plug-in terminal: double pole/single throw (DPST) relay output

6 Plug-in terminal relay output

7 Plug-in terminal: ground current trip input and temperature sensor input

8 Plug-in terminal: PLC network

Test / Reset Button

The Test / Reset button performs a reset, self-test, or places the LTMR controller in an internal trip state.

HMI Device/Expansion Module/PC Port

This port connects the LTMR controller to the following devices over the HMI port using an RJ45 connector:

  • An expansion module

  • A LTMCU/LTMCUF

  • A PC running SoMove with the TeSys T DTM

  • A Magelis XBTN410 HMI

Network Port

This port provides communication between the LTMR controller and a network PLC via terminal wiring.

LTMR Status Indicating LEDs

LED Name

Describes

Appearance

Status

HMI Comm

Communication between LTMR controller and HMI device, PC, or expansion module

Flashing yellow

Communication

OFF

No communication

Power

LTMR controller power or internal trip condition

Solid green

Power ON, motor OFF, no internal trips

Flashing green

Power ON, motor ON, no internal trips

OFF

Power OFF or internal trips exist

Alarm

Protection alarm or trip, or internal trip

Solid red

Internal or protection trip

Flashing red – 2 X per second

Alarm

Flashing red – 5 X per second

Load shed or rapid cycle

OFF

No trips, alarms, load shed, or rapid cycle (when power is ON)

Fallback

Indicates communications loss between the LTMR controller and network or HMI control source

Solid red

Fallback

OFF

No power (not in fallback)

MNS

Indicates network status

Green/red alternating

Startup self-test

Green flashing

Communication starting

Green solid

Communication established

Red flashing

Communication loss/timeout

Red solid

Unable to start network due to addressing / baud rate issue

Physical Description of the LTME Expansion Module

Overview

The LTME expansion module extends the monitoring and control functions of the LTMR controller by providing voltage measurement and additional logic inputs:

  • Three-phase voltage inputs

  • Four additional discrete logic inputs

LTME Expansion Module

LTME Expansion Module Connected to an LTMR Ethernet Controller

Front Face

The LTME expansion module front face includes the following features:

1 Port with RJ45 connector to HMI or PC

2 Port with RJ45 connector to LTMR controller

3 Status indicating LEDs

4 Plug-in terminal: voltage inputs

5 Plug-in terminal: logic inputs and common

NOTE: Logic inputs are externally powered according to input voltage ratings.

Status Indicating LEDs

LED Name

Description

Appearance

Status

Power

Power/Trip status

Green

Power ON, no trips

Red

Power ON, trips

OFF

Not powered

I.7

Logic Input I.7 status

Yellow

Activated

OFF

Not activated

I.8

Logic Input I.8 status

Yellow

Activated

OFF

Not activated

I.9

Logic Input I.9 status

Yellow

Activated

OFF

Not activated

I.10

Logic Input I.10 status

Yellow

Activated

OFF

Not activated

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.