DUG_Micro Module Shades Control_LK-00

Example of an automation

This demonstration shows you how to create an automation to open the Micro Module Shutter at the scheduled time.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Save.
    TIP: You can choose the cover image that best represents your automation by tapping .
  3. Tap Add Condition > Schedule.
    • Tap Repeat (A), select the days you want to set the schedule and tap Save.

    • Set the time (B) at which the automation must start and tap Next.

  4. Tap Add task > Run the device > Micro Module Shutter.
  5. Tap Control > Shutter Open (C) and tap Save.
  6. Tap Percentage (D) to update the percentage of shutter opening and tap Save.

  7. Tap Next.
  8. On the Automation Settings page, tap Save.

    Automation is now available on the Automation tab. Use toggle switch to enable/disable automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?