DUG_Micro Module Shades Control_LK-00

Pairing Wiser Wireless switch with shutter control (puck)

  1. If you do not need the lower rocker of the Wiser Wireless switch, you can replace it with a blind plate.
  2. Short press the left side of the rocker 5 times in quick succession on the Wiser Wireless switch.
    The status LED blinks green.
  3. Follow either of the options to pair the Puck:
    • Short press the Setup/Reset button 5 times in quick succession on the Puck.
    • Short press the mechanical double push button 1 for 5 times in quick succession.
    The status LED blinks green on the Puck.
    NOTE: If the Puck is located away from the mechanical push button, the status LED might not be visible.

    The shutter will move up and down a few times. The status LED stops blinking green on the Wiser Wireless switch and the Puck. The Puck can now be controlled by the Wiser Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?