DUG_Micro Module Shades Control_LK-00

Resetting the device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:

When reset is done successfully. The Wiser Wireless switch and device returns to factory default.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?