DUG_Micro Module Shades Control_LK-00

Pairing device manually

To pair the device manually:
  1. On Home page, tap + .
  2. Tap and select the Wiser Hub
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is recommended to add the device with install code.
  4. To pair the device with an install code, tap Add Device with Install Code to display the slide-up menu, then select one of the following options (B):
    • Scan Install Code: Scan the device for the install code.
      TIP: You can find the QR code on the back of the device.
    • Enter Install Code Manually: Manually enter the install code from the device.
      TIP: You can find the install code on the back of the device.
    After scanning or entering the install code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. Select one of the following options to add the device:
    • Short press the Setup/Reset button 3 times (< 0,5 s) on the Puck with a screwdriver.
    • Short press the push button 3 times.

    The LED blinks orange.
    NOTE: If the Puck is located away from the push button, the status LED might not be visible.
  7. In the app, select Confirm LED is flashing orange and tap Start Configuration (C).

  8. After a few seconds, a solid green LED indicates that the device is successfully paired to the Hub.

  9. After the device is added in the app, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?