DUG_Micro Module Shades Control_LK-00

Troubleshooting

Symptom

Solution

No shutter movement or uncontrolled shutter movement.

  • Check power supply.

  • Check the wiring between and push-button switch.

  • Check the load.

The device is not ready to pair after the device is removed from the app.

Reset to factory default settings, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?