DUG_Micro Module Shades Control_LK-00

About Quick Home Connect

Quick Home Connect is a wireless connectivity solution for Zigbee devices without the need for a Hub or smartphone application. Quick Home Connect is your starting point for wireless home automation. It performs functions like switching, dimming and shutter control using the LK FUGA® Wiser wireless battery 4 button switch (hereinafter referred to as Wiser Wireless switch) via a Zigbee network.

The Wiser Wireless switch is a battery-powered wireless push-button switch that is used to control Zigbee devices (such as dimmer, shutter, and relay) within the same Zigbee network.

Limitations

  • Quick Home Connect serves only as a room control solution.

  • In a 1-gang Wiser Wireless switch, you cannot combine lighting and shutter control. However, with a 2-gang Wiser Wireless switch, you can use one gang for dimming/switching and the other for shutter control, or vice versa.

  • This solution does not support remote control, smartphone app usage, or scheduling features.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?