DUG_Micro Module Shades Control_LK-00

Testing the device

Before using the Puck, manually test the Puck and make sure that it works when connected to the shutter.

To test the Puck:

  1. Short press the test button once.
    The shutter opens/closes gradually.

  2. Press and hold the test button.
    The shutter opens/closes fully.

  3. Record the time for the shutter to fully open/close.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?