Pairing the device with the Wiser Hub
- On the Home screen, tap
.
- Tap Shutters > . >
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.OBS: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.
-
(B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.
-
- Once the device is validated, tap Next, short-press the push button on the blind control switch 3 times and make sure that the LED blinks amber.
- Tap
, enter a name of the device.
- Tap Next and assign the device to a new room or an existing room and tap Submit.
- Tap Device Type: and select a
- Shutter: Proceed to step 8.
- Shutter with tilting slats: Proceed to step 9 to 11.
- Tap Setting default run time. and enter the open/close duration of shutter. Refer to
- Tap Set: , select a slat type
and tap
- Horizontal
- Tilted
- Vertical
- Tap Next and enter the following
durations:
- Open duration: Time taken to open the shutter.
- Close duration: Time taken to close the shutter.
- Tilt duration: Time taken to rotate the slats
completely from closed to open position.Refer to Setting default run time.
- Tap Submit.Once the pairing process is completed, the device name is listed on the Control tab under the All and Room tabs.