DUG_Exxact – Persiennstyrningsbrytare_WH-00

Setting up a schedule

The shutter can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time. The devices can be fully controlled by schedule. Once the schedule is set, the devices operates at a given time.
To create a schedule:
  1. On the Home screen, tap > Schedules > .
  2. Enter a name of the schedule (A).
  3. Select a device type (B).
  4. Select the list of devices (C) to which the schedule must apply.
  5. Tap Create.
  6. Tap to add an event.
  7. Select a state (Open/Closed/percentage) (D), time period (E) and tap Set.
    FÖRSLAG:
    • You can add multiple schedules based on your requirement. Select days, tap , set on/off state and time.

    • You can copy the existing schedule to another schedule or to the days of your choice. Tap .

      • Tap Schedule and select an existing schedule and tap Copy.

      • Tap Day and select the days you want to assign and tap Copy.

      • When the schedule begins, you can see the until time on the Control tab under the device name.

    • On the top-right screen, tap and select Follow Schedule toggle switch to turn On/Off the schedule.

    • When the schedule begins, you can see the until time in the following screens:

      • Device Control Screen.

      • Control tab under the device name.

      • Favourite devices section on the home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Var det här till hjälp?