DUG_Exxact – Persiennstyrningsbrytare_WH-00

Troubleshooting

Symptom

Solution

Connected shutter cannot be controlled.

  • Check power supply.

  • Remove power to the blind control switch and then re-connect power again.

  • Check the load.

  • In the case of an external push button, check the wiring.

  • Re-couple devices.

Shutter is not driving to the desired position.

Reset to factory default settings, refer to Resetting the device

Shutter is not moving in set time.

Calibrate again.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Var det här till hjälp?