DUG_Odace - Thermostat 2 A_WH-06

For your safety

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Safe electrical installation must be carried out only by skilled professionals. Skilled professionals must prove profound knowledge in the following areas:
  • Connecting to installation networks.
  • Connecting several electrical devices.
  • Laying electric cables.
  • Safety standards, local wiring rules and regulations.
Failure to follow these instructions will result in death or serious injury.
NOTICE
The device is not fitted with an internal fuse.
  • The device must be protected by a 2 A circuit breaker.
Failure to follow these instructions can result in equipment damage.
NOTICE
HAZARD OF EQUIPMENT DAMAGE
  • Ensure that the device is disconnected from its circuit during the insulation resistance test.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?