DUG_Smoke alarm DC_WH-01

Checking the device history

Using the Wiser Home app, you can monitor the smoke detection by accessing the device history.
NOTE: All device history is stored in the cloud. When the cloud connection is lost, the device history cannot be viewed.
To view the device history:
  1. On the Home page, tap All devices > Smoke Alarm.
  2. On the device control panel page, tap History.
    In the History page, you can see the date, time, and type of alarm detected.
    NOTE: For a maximum period of 90 days, device history can be recorded.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?