Pairing the device with the Wiser Hub
- On the Home screen, tap
.
- Tap .
- Tap Scan QR code and allow the Wiser
Home app to access your camera.NOTE: If the dimmer doesn't have the QR code or MAC Address and Install Code, you can manually pair it by tapping I can't find the correct QR code.
However, it is highly recommended to use a QR code or MAC Address and Install Code for pairing. - If the QR code is incorrect, a message Incorrect QR
code scanned will appear. Tap I can’t scan
the QR code, enter the MAC Address and Install Code, and then tap Connect.The Wiser Home app verifies as Confirmed if the MAC Address and Install Code are valid.NOTE: If the MAC Address and Install Code are not visible, you can manually pair it by tapping Skip and setup manually.
- Once the device is validated, Follow any one of the options
to pair the module based on your installation:
- Short press the Setup/Reset button of the module 3 times.
- Short press the mechanical push-button 3 times.
The LED first blinks amber.
- Wait for a few seconds until the LED turns green.The device is joined.
- Tap and select a device type:
- Tap ,
to enter the name of the device.
- Tap Next and assign the device to
a new room or an existing room and tap Submit.IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.
- Tap
and enter a Nominal power value.
IMPORTANT:-
The maximum power consumed by the appliance controlled by the module is known as Nominal power. It is the maximum power the module can manage.
-
By default, the value is 2000 W. The nominal power must be between 0 and 3000 W.
NOTE: The Nominal power value will only be used for the future updates in the Wiser Home app. -
- Tap Next and assign the device to a new room or an existing room.
- Tap Submit.Once the pairing process is complete, the device name (example, Water Heater) is listed under All devices in Home screen.