DUG_Multiwire Puck Dimmer_WH–01

Push button moment control

Assign a moment or create a new moment for both the short press and long press of the push-button switch.
  1. Select Moment from the slide up menu, and then tap Short Press (A).
  2. Select if there is an existing moment, then tap Select Moment or tap Create a Moment to create a new moment.
    Click the following link for a detailed procedure on creating a new moment, Creating a moment.
  3. Upon selecting the moment, tap the back icon (B) to return to the moment configuration page.
    You will now see that the Short Press function is configured with a moment. Follow the same procedure for the Long Press function.

Changing and Unbinding a moment

  1. On the moment control page, tap either Short Press or Long Press.
  2. Choose the following options to change or unbind the moment.
    • Changing: Tap the moment you want to configure for Short Press or Long Press function, then tap Select Moment.
      TIP: The moment with a green tick is the currently selected moment, tap a different moment to make changes.
    • Unbinding: Tap the moment you want to unbind for Short Press or Long Press function, then tap Select Moment.
      TIP: The moment with a green tick is the currently selected moment; tap the moment with the green tick to unbind it.
  3. Tap Yes, I’m sure to confirm and apply the changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?