Selecting the floor sensor
DANGER |
|---|
|
RISK OF FATAL INJURY FROM ELECTRIC SHOCK
The device is not a Safety Extra Low Voltage (SELV) device.
The sensors lines are on mains (230 VAC) line.
Failure to follow these instructions will result in death or serious injury.
|
To select the floor Sensor:
- On the Home screen, tap
.
- Tap (A) and select the sensor from the
list.
-
NTC 10K
-
NTC 12K
-
NTC 15K
-
NTC 33K
-
NTC 47K
NOTE: Not fitted is selected by default. -
- Tap OK.
Once the floor sensor is selected, new options (B) appear in the app.
-
Floor Temperature - It shows the temperature of the floor measured by the floor sensor.
-
Floor Sensor Offset - Allows you to calibrate the floor sensor to match the actual temperature of the floor.
-
Floor Sensor Upper Limit - The upper limit is set to maintain the floor temperature below the set limit.
-
Floor Sensor Lower Limit - The lower limit is set to maintain the floor temperature above the set limit.
-
DANGER