DUG_Wiser 16A Relay for Temperature Control_WH-07

Offsetting the floor sensor

Using Wiser Home app, the Floor Sensor Offset option allows you to calibrate the floor sensor to match the actual temperature measured by an external device.
To offset the floor sensor:
  1. On the Home screen, tap .
  2. Tap Devices > Climate > 16A Relay > Floor Sensor Offset (A) and select the temperature that is required for offsetting, to match the actual temperature.
  3. Tap OK.
    NOTE:
    • The allowed temperature range to offset the floor sensor is
      9 °C to -9 °C.

    • The floor temperature shows the final temperature of the floor including any offset that is applied.

    TIP: Offsetting the floor sensor is not required, if the floor temperature measured by the floor sensor and an external device are same. You can set it to 0 °C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?