DUG_Wiser 16A Relay for Temperature Control_WH-07

Setting the floor sensor Upper/Lower limit

Using the Wiser Home app, you can switch on/off the electrical underfloor heater by setting lower/upper temperature limit. This allows you to maintain the floor temperature within the set limits.
To set the floor sensor temperature limit:
  1. On the Home screen, tap .
  2. Tap Devices > Climate > 16A Relay .
  3. Tap Floor Sensor Upper Limit/ Floor Sensor Lower Limit (A) and set the upper/lower temperature limit.
    NOTE:
    • Upper limit range is 5 °C to 40 °C.

    • Lower limit range is 4 °C to 39 °C.

  4. Tap OK.
    TIP: You can select Disabled, if setting the floor sensor limit is not required.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?