0612CT0101

Section 3—Electronic Trip Systems

M-frame circuit breakers are available with the type ET 1.0 electronic trip system. P-frame and R-frame circuit breakers are available with either the ET1.0I basic electronic trip system or the MicroLogic electronic trip system. The NS630b–NS3200 circuit breakers are available with the MicroLogic electronic trip system. The sensing system responds to the flow of current through the circuit breaker.

Thermal Imaging

The thermal imaging function protects the cables or bus bars from overheating in case of low amplitude repetitive faults. Such overheating can be due to repetitive motor starting, fluctuating load, intermittent ground faults, or subsequent closing after a fault. Traditional electronic protection does not protect against repetitive faults because the duration of each overload above the pickup setting is too short to achieve effective tripping. Nevertheless, each overload involves a temperature rise in the installation, the cumulative effect of which could lead to overheating of the system.

The thermal imaging function remembers and integrates the thermal heating caused by each pickup setting overrun. Before tripping, the integrated heating value will reduce the associated time delay and, therefore, the reaction of the trip unit will be closer to the real heating of the power network system. After tripping, the function will also reduce the time delay when closing the circuit breaker on an overload.

True RMS Current Sensing

The sensing system responds to the flow of current through the circuit breaker. The trip unit samples the current waveform to provide true RMS protection through the fifteenth harmonic. This true RMS sensing gives accurate values for the magnitude of a non-sinusoidal waveform. Therefore, the heating effects of harmonically distorted waveforms are accurately evaluated.

The MicroLogic H trip unit provides additional sampling of the waveforms to measure and provide waveform capture of harmonic distortion to the thirty-first harmonic.

Type ET Electronic Trip System

Type ET trip units are available with M-frame, P-frame and R-frame UL/IEC circuit breakers. Circuit breakers with type ET trip units have a fixed ampere rating. The trip units are not field-interchangeable and will not accept any communications or other trip unit accessories. The trip system uses a set of current transformers (called CTs or sensors) to sense current, a trip unit to evaluate the current, and a tripping solenoid to trip the circuit breaker.

ET1.0 (M-Frame only)

The ET1.0 trip system is available on M-frame circuit breakers with both fixed and adjustable long-time (lr) setting and adjustable instantaneous (li) tripping. The long-time pickup is adjustable from 300 to 800 A. For fixed long-time circuit breakers, there are two circuit breaker amperage ratings. The instantaneous trip is a multiple of this setting from 2–10 x with no intentional time delay. There is additionally an automatic molded case switch available in 600 and 800 A.

ET1.0I (P-Frame and R-Frame only)

The ET1.0I trip system is available on both P-frame and R-frame circuit breakers and is equipped with fixed long-time and adjustable instantaneous tripping functions only. The long-time pickup is fixed at 1.0 x sensor rating (In), while the instantaneous pickup is adjustable (dial settings from 1.5–12 x In) with no intentional time delay.

ET1.0M (P-Frame only)

The ET1.0M trip system is only available on P-frame motor circuit protectors and provides protection for short circuit conditions only. The trip unit has a single adjustment for instantaneous pickup that, if exceeded, will trip the circuit breaker with no intentional delay. Instantaneous trip dial settings are 2–16 x In for 600 A circuit breakers and 1.5–12 x In for 800–1200 A circuit breakers.

MicroLogic Electronic Trip Systems

The P-frame, R-frame and NS630b–NS3200 electronic trip circuit breakers can be equipped with the optional MicroLogic trip systems listed below:

MicroLogic Trip Systems

Model

(LS0)
Long-time + Short-time + Zero delay (IEC Rated Only)

(LI)
Long-time + Instantaneous Protection (UL Listed, IEC Rated)

(LSI)
Long-time + Short-time + Instantaneous Protection (UL LIsted, IEC Rated)

(LSIG)
Long-time + Short-time + Instantaneous Protection + Equipment Ground-fault Protection (UL LIsted, IEC Rated)

MicroLogic Basic Trip Unit

2.0

3.0

5.0

MicroLogic A Trip Unit

2.0A

3.0A

5.0A

6.0A

MicroLogic P Trip Unit

5.0P

6.0P

MicroLogic H Trip Unit

5.0H

6.0H

MicroLogic 3.0 and 5.0 Basic Trip Units

MicroLogic 3.0A, 5.0A and 6.0A Trip Units

MicroLogic 5.0P and 6.0P Trip Units

MicroLogic 5.0H and 6.0H Trip Units

Trip units are designed to protect power circuits and loads. MicroLogic trip systems use a set of current transformers (called CTs or sensors) to sense current, a trip unit to evaluate the current, and a tripping solenoid to trip the circuit breaker. Adjustable rotary switches on the trip unit allow the user to set the proper overcurrent or equipment ground-fault current protection required in the electrical system. If current exceeds a set value for longer than its set time delay, the trip system opens the circuit breaker. Alarms may be programmed for remote indications. Measurements of current, voltage, frequency, power, and power quality optimize continuity of service and energy management.

Integration of protection functions in the Application Specific Integrated Circuit (ASIC) electronic component used in all MicroLogic trip units yields a high degree of reliability and immunity to conducted or radiated disturbances. On MicroLogic P and H trip units, advanced functions are managed by an independent microprocessor.

Circuit breakers are shipped with the trip unit long-time pickup switch set at 1.0 and all other trip unit adjustments set at their lowest settings. Actual settings required for a specific application must be determined by a qualified consultant or plant engineer. A coordination study is recommended to provide coordination between all circuit breakers in the distribution system.

MicroLogic Electronic Trip Unit Features

MicroLogic Trip Unit Features

Feature

MicroLogic Trip Unit (X = Standard Feature O = Available Option)

Standard

Ammeter

Power

Harmonics

2.0

3.0

5.0

2.0A

3.0A

5.0A

6.0A

5.0P

6.0P

5.0H

6.0H

Field-Installable

X

X

X

X

X

X

X

X

X

X

X

LI

X

X

LS0

X

X

LSI

X

X

X

X

LSIG/Ground-Fault Trip*

X

X

X

Ground-Fault Alarm/No Trip*

X

X

Ground-Fault Alarm and Trip*

X

X

Adjustable Rating Plugs

X

X

X

X

X

X

X

X

X

X

X

True RMS Sensing

X

X

X

X

X

X

X

X

X

X

X

UL Listed

X

X

X

X

X

X

X

X

X

Thermal Imaging

X

X

X

X

X

X

X

X

X

X

X

Phase-Loading Bar Graph

X

X

X

X

X

X

X

X

LED for Long-Time Pick-Up

X

X

X

X

X

X

X

X

X

X

X

LED for Trip Indication

X

X

X

X

X

X

X

X

Digital Ammeter

X

X

X

X

X

X

X

X

Zone-Selective Interlocking*

X

X

X

X

X

X

X

Communications

O

O

O

O

X

X

X

X

LCD Dot Matrix Display

X

X

X

X

Advanced User Interface

X

X

X

X

Protective Relay Functions

X

X

X

X

Neutral Protection*

X

X

X

X

Contact Wear Indication

X

X

X

X

Incremental Fine Tuning of Settings

X

X

X

X

Selectable Long-Time Delay Bands

X

X

X

X

Power Measurement

X

X

X

X

Power Quality Measurements

X

X

Waveform Capture

X

X

MicroLogic 2.0, 3.0 and 5.0 Basic Trip Units

1—Long-time current setting and tripping delay

2—Short-time pickup and tripping delay

3—Overload signal (LED)

4—Long-time rating plug screw

5—Instantaneous pickup

6—Test connector

The MicroLogic 2.0, 3.0, and 5.0 basic trip units protect power circuits.

Protection Settings

Protection thresholds and delays are set using the rotary switches. A full-range of long-time settings are available via field-installable adjustable rating plugs.

  • Overload protection

    • True RMS long-time protection

    • Thermal imaging: Active thermal imaging before and after tripping

  • Short-circuit protection

    • Short-time RMS

    • Selection of I2t type (ON or OFF) for short-time delay

  • Instantaneous protection

  • Neutral protection on four-pole circuit breakers

MicroLogic 2.0 and 3.0 Basic Trip Unit Settings

MicroLogic 2.0 and 3.0 Basic Trip Unit Settings

Long-Time Protection

Current Setting (A)
Tripping between 1.05 and 1.20 x Ir

Ir = ln x ...

2.0:

0.40

0.50

0.60

0.70

0.80

0.90

0.95

0.98

1.00

3.0:

0.40

0.45

0.50

0.60

0.63

0.70

0.80

0.90

1.00

Other ranges are available by changing rating plug

Maximum Time Delay (s)
Accuracy: 0 to –20%

tr at 1.5 x Ir

12.5

25

50

100

200

300

400

500

600

tr at 6 x Ir

0.5

1

2

4

8

12

16

20

24

tr at 7.2 x Ir

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Thermal Imaging

20 minutes before or after tripping

Short-Time Protection

Current Setting (A)
Accuracy: ±10%
No delay

Isd = Ir x ...

2.0:

1.5

2

2.5

3

4

5

6

8

10

Instantaneous Protection

Current Setting (A)
Accuracy: ±10%

Ii = In x ...

3.0:

1.5

2

3

4

5

6

8

10

12

MicroLogic 5.0 Basic Trip Unit Settings

MicroLogic 5.0 Basic Trip Unit Settings

Long-Time Protection

Current Setting (A)
Tripping Between 1.05 and 1.20 x Ir

Ir = ln x ...

IEC:

0.40

0.50

0.60

0.70

0.80

0.90

0.95

0.98

1.00

UL:

0.40

0.45

0.50

0.60

0.63

0.70

0.80

0.90

1.00

Other Ranges are Available by Changing Rating Plug

Maximum Time Delay (s)
Accuracy: 0 to –20%

tr at 1.5 x Ir

12.5

25

50

100

200

300

400

500

600

tr at 6 x Ir

0.5

1

2

4

8

12

16

20

24

tr at 7.2 x Ir

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Thermal Imaging

20 Minutes Before or After Tripping

Short-Time Protection

Current Setting (A)
Accuracy: ±10%

lsd = Ir x ...

1.5

2

2.5

3

4

5

6

8

10

Maximum Time Delay (s) at 10 x Ir

Settings

I2t OFF

0

0.1

0.2

0.3

0.4

 

I2t ON

0.1

0.2

0.3

0.4

 

tsd

Min. Trip Time (ms)

20

80

140

230

350

 

Max. Trip Time (ms)

80

140

200

320

500

 

Instantaneous Protection

Current Setting (A) Accuracy: ±10%

Ii = ln x ...

2

3

4

6

8

10

12

15

off

MicroLogic 2.0A, 3.0A, 5.0A and 6.0A Trip Units with Ammeter

A—Indication of tripping cause

B—Navigation buttons

C—Long-time current setting and tripping delay

D—Short-time pickup and tripping delay

E—Ground-fault pickup and tripping delay

F—Test lamp and reset

G—Digital display

H—Three-phase bar graph and ammeter

I—Overload signal (LED)

J—Long-time rating plug screw

L—Instantaneous pickup

L—Electronic push-to-trip

M—Test connector

MicroLogic A trip units protect power circuits and provide current measurements, overload protection, and short-circuit protection. In addition, the 6.0A trip units also provide ground-fault protection for equipment.

Protection Settings

Protection thresholds and delays are set using the rotary switches. The selected values are momentarily displayed in amperes and in seconds. A full-range of long-time settings are available via the field-installable rating plug:

  • Overload protection (true RMS long-time protection)

  • Thermal imaging (active thermal imaging before and after tripping)

  • Short-circuit protection:

    • Short-time RMS

    • I2t ON or OFF for short-time delay

  • Instantaneous protection

  • Ground-fault protection for equipment:

    • Residual ground-fault protection for equipment

    • Source ground-return ground-fault protection for equipment

    • Modified differential ground-fault protection (MDGF) for equipment

  • Neutral protection on four-pole circuit breakers

  • ZSI: Zone-selective interlocking:

    • ZSI terminal block may be used to interconnect a number of trip units to provide total discrimination for short-time and equipment ground-fault protection, without delay for tripping).

    • Not available for 3.0A trip units or for 2.0A trip units installed as upstream devices.

Ammeter Measurements

MicroLogic A trip units measure the true RMS value of currents. They provide continuous current measurement from 0.2 to 20 x In with an accuracy of 1.5% (including sensors). No auxiliary source is needed where I > 0.2 x In. The optional external power supply (24 Vdc) makes it possible to display currents where I < 0.2 x In and to store values of the interrupted current.

A digital LCD screen continuously displays the most heavily loaded phase (Imax) or displays the IA, IB, IC, Ig, and (on 4P circuit breakers only) IN stored current and setting values by successively pressing the navigation button.

Communication Network

In conjunction with an optional communication network, the trip unit transmits the following parameters:

  • Setting values

  • All ammeter measurements

  • Tripping causes

MicroLogic 2.0A and 3.0A Trip Unit Settings

MicroLogic 2.0A and 3.0A Trip Unit Settings

Long-Time Protection

Current Setting (A)
Tripping Between 1.05 and 1.20 x Ir

Ir = ln x...

2.0A:

0.40

0.50

0.60

0.70

0.80

0.90

0.95

0.98

1.00

3.0A:

0.40

0.45

0.50

0.60

0.63

0.70

0.80

0.90

1.00

Other Ranges are Available by Changing Rating Plug

Maximum Time Delay (s)
Accuracy: 0–20%

tr at 1.5 x Ir

12.5

25

50

100

200

300

400

500

600

tr at 6 x Ir

0.5

1

2

4

8

12

16

20

24

tr at 7.2 x Ir

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Thermal Imaging

20 Minutes Before or After Tripping

Short-Time Protection

Current Setting (A)
Accuracy: ±10%, No delay

Isd = Ir x...

2.0A:

1.5

2

2.5

3

4

5

6

8

10

Instantaneous Protection

Current Setting (A)
Accuracy: ±10%

II = In x...

3.0A:

1.5

2

3

4

5

6

8

10

12

MicroLogic 5.0A and 6.0A Trip Unit Settings

MicroLogic 5.0A and 6.0A Trip Unit Settings

Long-Time Protection

Current Setting (A)
Tripping Between 1.05 and 1.20 x Ir

Ir = ln x...

IEC:

0.40

0.50

0.60

0.70

0.80

0.90

0.95

0.98

1.00

UL:

0.40

0.45

0.50

0.60

0.63

0.70

0.80

0.90

1.00

Other ranges are available by changing rating plug

Maximum Time Delay (s)
Accuracy: 0–20%

tr at 1.5 x Ir

12.5

25

50

100

200

300

400

500

600

tr at 6 x Ir

0.5

1

2

4

8

12

16

20

24

tr at 7.2 x Ir

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Thermal Imaging

20 minutes before or after tripping

Short-Time Protection

Current Setting (A) Accuracy: ±10%

lsd = Ir x...

1.5

2

2.5

3

4

5

6

8

10

Maximum Time Delay (s) at 10 x Ir

Settings

I2t OFF

0

0.1

0.2

0.3

0.4

 

I2t ON

0.1

0.2

0.3

0.4

 

tsd

Min. trip time (ms)

20

80

140

230

350

 

Max. trip time (ms)

80

140

200

320

500

 

Instantaneous Protection

Current Setting (A)
Accuracy: ±10%

Ii = In x...

2

3

4

6

8

10

12

15

off

MicroLogic 6.0A Trip Unit with Ground-Fault Settings

MicroLogic 6.0A Trip Unit Ground-Fault Settings

Ground-Fault Pickup (A) Accuracy: ±10%

Ig = In x...

A

B

C

D

E

F

G

H

J

In ≤ 400 A

0.3

0.3

0.4

0.5

0.6

0.7

0.8

0.9

1.0

400 A < In ≤ 1200 A

0.2

0.3

0.4

0.5

0.6

0.7

0.8

0.9

1.0

In > 1200 A

500

640

720

800

880

960

1040

1120

1200

Maximum Time Delay (s) at 1 x Ig

Settings

I2t OFF

0

0.1

0.2

0.3

0.4

   

I2t ON

0.1

0.2

0.3

0.4

   

tg

Minimum Trip Time (ms)

20

80

140

230

350

   

Maximum Trip Time (ms)

80

140

200

320

500

   

External Power Supplies for MicroLogic Trip Units

Current-based protection functions require no auxiliary power source.

MicroLogic A Use of External 24 Vdc Power Supply

Function

Without 24 Vdc Power Supply at F1 and F2

With 24 Vdc Power Supply at F1 and F2

Fault Protection for LSIG Functions

Yes

Yes

LED Trip Indication

Yes

Yes

Ammeter and bar graph displays

Yes

Yes

Trip Setting and Max. Current Readings Can Be Accessed on the Display by Using Navigation Buttons.

Yes, If Current Flow on One Phase is Equal To or Greater Than:

Yes

 

Sensor Plug Value (In)

Minimum Ground-fault Pickup

 

100–250 A

30% of sensor rating

Ground-Fault Push-to-Trip Button Works for Testing Ground Fault*

 

400–1200 A

20% of sensor rating

 

1600–6300 A

500 A

Modbus Communications (Optional)

No

Yes, with separate 24 Vdc power supply for the circuit breaker communication module

Back-lit Display

No

Yes

MicroLogic 5.0P and 6.0P Trip Units with Power Metering

A—Indication of tripping cause

B—High resolution screen

C—Measurement display

D—Navigation buttons

E—Long-time current setting and tripping delay

F—Short-time pickup and tripping delay

G—Hole for settings lockout pin

H—Ground-fault pickup and tripping delay

I—Test lamp and indication reset

J—Maintenance indicators

K—Protection settings

L—Overload signal (LED)

M—Long-time rating plug screw

N—Instantaneous pickup

O—Electronic push-to-trip

P—Test connector

MicroLogic P trip units provide power metering and extended protection in addition to the adjustable protection functions of the MicroLogic A trip unit.

Protection Settings

The adjustable protection functions of the 5.0P and 6.0P trip units are identical to those of the MicroLogic A trip unit (overloads, short circuits, equipment ground-fault protection; see MicroLogic 2.0A, 3.0A, 5.0A and 6.0A Trip Units with Ammeter). These units also feature:

  • Fine adjustment
    Within the range below the rotary switch setting, fine adjustments of pickups/delays in steps of 1 A/s (except for short-time and ground-fault) are possible on the keypad or remotely by the communication network.

  • Inverse definite minimum time lag (IDMTL) setting.
    Coordination with fuse-type or medium-voltage protection systems is optimized by adjusting the long-time delay curve around 6 x Ir axis. This setting ensures better coordination with certain loads.

  • Neutral protection
    On three-pole circuit breakers, neutral protection may be set using the keypad or remotely using the communication network to one of four positions: OFF, 1/2N (1/2 x In), 1N (1 x In), or 1.6N (2 x In).
    NOTE: Neutral protection is disabled if long-time curve is set to one of the IDMTL protection settings.

  • Configuring Alarms and Other Protection Functions
    When the cover is closed, the keypad may no longer be used to change the protection settings, but it still provides access to the displays for measurements, histories, indicators, etc. Depending on the thresholds and time delays set, the MicroLogic P trip unit monitors current, voltage, power, frequency, and phase sequence. Each threshold overrun may be signalled remotely via the communication network.

Each threshold overrun may be combined with tripping (protection) or an indication carried out by an alarm programmed accessible with the optional IO module, or both (protection and alarm).

Maintenance Record

The maintenance record can be consulted using the service interface kit or the full-function test kit, or remotely via the communication network. It can be used as an aid in troubleshooting and to assist scheduling for device maintenance operations. Recorded indications include:

  • Highest current measured

  • Operation counter (cumulative total and total since last reset)

  • Number of test kit connections

  • Number of trips in operating mode

Load Shedding and Reconnection Parameters

Load shedding and reconnection parameters can be set according to the power or the current flowing through the circuit breaker. Load shedding is carried out by a remote computer via the communication network.

Indication Option Via Programmable Contacts

Alarms may be used to signal threshold overruns or status changes. It can be programmed using the keypad on the MicroLogic P trip unit or remotely using the communication network. The contact is required to obtain data from the protective relay functions on Type P and Type H trip units.

MicroLogic 5.0P and 6.0P Trip Unit Settings

MicroLogic 5.0P and 6.0P Trip Unit Settings

Long-Time (RMS) Protection

Current Setting (A)
Tripping Between 1.05 and 1.20 x Ir

Ir = ln x...

IEC

0.40

0.50

0.60

0.70

0.80

0.90

0.95

0.98

1.00

Ir = ln x...

UL

0.40

0.45

0.50

0.60

0.63

0.70

0.80

0.9

1.00

Other Ranges are Available by Changing Rating Plug

Maximum Time Delay (s) Accuracy: 0 to –20%

tr at 1.5 x Ir

12.5

25

50

100

200

300

400

500

600

tr at 6 x Ir

0.5

1

2

4

8

12

16

20

24

tr at 7.2 x Ir

0.34

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

IDMTL Setting

Curve slope

SIT

VIT

EIT

HV Fuse

DT

Thermal Imaging

20 Minutes Before or After Tripping

Short-Time (RMS) Protection

Current Setting (A)
Accuracy: ±10%

lsd = Ir x...

1.5

2

2.5

3

4

5

6

8

10

Maximum Time Delay (s)
at 10 x Ir

Settings

I2t OFF

0

0.1

0.2

0.3

0.4

I2t ON

0.1

0.2

0.3

0.4

tsd

Min. Trip Time (ms)

20

80

140

230

350

Max. Trip Time (ms)

80

140

200

320

500

Instantaneous Protection

Current Setting (A)
Accuracy: ±10%

II = IN x...

2

3

4

6

8

10

12

15

off

MicroLogic 6.0P Trip Unit with Ground-Fault Settings

MicroLogic 6.0P Trip Unit Ground-Fault Settings

Ground-Fault Pickup (A) Accuracy: ±10%

Ig = In x...

A

B

C

D

E

F

G

H

J

In ≤ 400 A

0.3

0.3

0.4

0.5

0.6

0.7

0.8

0.9

1.0

400 A < In ≤ 1200 A

0.2

0.3

0.4

0.5

0.6

0.7

0.8

0.9

1.0

In > 1200 A

500

640

720

800

880

960

1040

1120

1200

Time Delay (s) at 1 x In

Settings

I2t OFF

0

0.1

0.2

0.3

0.4

       

I2t ON

0.1

0.2

0.3

0.4

       

tg

Min. Trip Time (ms)

20

80

140

230

350

       

Max. Trip Time (ms)

80

140

200

320

500

       

MicroLogic 5.0P and 6.0P Trip Unit Settings with Protection Functions

MicroLogic 5.0P and 6.0P Trip Unit Settings for Protection Functions

 

Threshold

Time Delay

Current

Current Imbalance

0.05 to 0.6 x Imax

1 to 40 s

Maximum Current

Imax: IA, IB, IC, IN, Ig

0.2 to 1.0 x In

15 to 1500 s

Voltage

Voltage Imbalance

0.02 to 0.3 x Vn

1 to 40 s

Minimum Voltage

Vmin

100 to 725 V (Phase Total)

0.25 to 0.5 s

Maximum Voltage

Vmax

100 to 1200 V (Between Phases)

0.20 to 5.0 s

Power

Maximum Power

Pmax

5 to 500 kW

0.2 to 20 s

Reverse Power

Pr

0.02 to 0.2 x Pn

0.5 to 20 s

Frequency

Minimum Frequency

Fmin

45 to 65 Hz

0.2 to 5 s

Maximum Frequency

Fmax

45 to 540 Hz

0.2 to 5 s

Phase

Sequence

ΔØ

ØA-ØB-ØC or ØA-ØC-ØB

Instantaneous

MicroLogic 5.0P and 6.0P Trip Unit Settings for Current and Power Load-Shedding

MicroLogic 5.0P and 6.0P Trip Unit Settings for Current and Power Load-Shedding

Pickup

Drop-out

Threshold

Time Delay

Threshold

Time Delay

Current

I

0.5 to 1.0 x Ir Per Phase

20% to 80% x tr

0.3 to 1.0 x Ir per phase

10 to 600 s

Power

P

200 kW to 10 MW

10 to 3600 s

100 kW to 10 MW

10 to 3600 s

MicroLogic P Trip Units and 24 Vdc Power Supply

MicroLogic P trip units are designed to be used with an external 24 Vdc power supply. Current-based protection functions require no auxiliary power source.

MicroLogic P Trip Units and 24 Vdc Power Supply

Function

Without 24 Vdc Power Supply at F1 and F2

With 24 Vdc Power Supply at F1 and F2

Fault Protection for LSIG Functions

Yes

Yes

LED Trip Indication

Yes

Yes

LCD Display and Backlight are Functional

Yes*

Yes

Ground-Fault Push-to-Trip Button Works for Testing Ground Fault*

Yes*

Yes

Metering, Monitoring, and History Logs are Functional

Yes*

Yes

Communications Between Trip Unit and M2C contacts

No

Yes

Modbus Communications

No

Yes, with separate 24 Vdc power supply for the circuit breaker communication module

MicroLogic Trip Units Tripping and Alarm Histories

The last ten trips and ten alarms are recorded in two separate history files that can be displayed on the screen (sample displays are shown).

The following information is contained in these files:

Trip History

Alarm History

• Type of fault

• Type of alarm

• Date and time of fault

• Date and time of alarm

• Interrupted current

• Values measured at time of alarm

MicroLogic Trip Unit Metering

The MicroLogic P trip unit calculates in real time the electrical values V, A, W, VAR, VA, Wh, VARh, VAh, Hz, power factor and crest factor. It also calculates demand current and power over an adjustable time period.

Current Metering

Maximum Current

Voltage Metering

Power Metering

Frequency

Power Demand

Real-Time Metering

The value displayed on the screen is refreshed every second. Minimum and maximum measurement values are stored in memory.

Type of Measurement

Unit of Measurement

Measurement Source

Current

IRMS
IAVERAGE
IPEAK/√ 2

A
A
A

ØA, ØB, ØC or N
(ØA + ØB + ØC) / 3
ØA, ØB, ØC or N

Voltage

VRMS
VRMS
∆VIMBALANCE

V
V
%

(ØA–ØB), ( ØB–ØC) and (ØC–ØA)
(ØA–N), (ØB–N) and ( ØC–N)
VRMS

Power

P, Q and S
EP, EQ and ES
Power factor

W, VAR, VA
Wh, VARh, VAh

Total
Total
Total

Frequency

F

Hz

50/60

Demand Metering

The demand is calculated over a fixed or sliding time window that can be programmed from five to sixty minutes. Depending on the contract signed with the power supplier, specific programming makes it possible to avoid or minimize the cost of overrunning the subscribed power. Maximum demand values are systematically stored and time stamped.

Type of Measurement

Unit of Measurement

Measurement Source

Current

IDEMAND

A

ØA, ØB, ØC or N

Power

P, Q and SDEMAND

W, VAR, VA

Total

MicroLogic Communication Network

The communication network may be used to:

  • Remotely read parameters for the protection functions.

  • Transmit all the measurements and calculated values.

  • Signal the causes of tripping and alarms.

  • Consult the history files and the maintenance indicator record.

In addition, an event log of the last 100 events and a maintenance record, which is stored in the trip unit memory but not available locally, may be accessed via the communication network.

This Modbus communication system is compatible with the PowerLogic™ System Manager software (SMS).

MicroLogic Event Log

The event log may be accessed by a remote computer via the communication network. All events are time stamped and include:

  • Trips

  • Beginning and end of alarms

  • Modifications to settings and parameters

  • Loss of time

  • Test kit connections

  • Counter resets

  • System faults (thermal self-protection, major fault and minor fault alarms)

MicroLogic 5.0H and 6.0H Trip Units with Harmonic Metering

In addition to the P functions, the MicroLogic H trip units offer:

  • In-depth analysis of power quality including calculation of harmonics and the fundamentals.

  • Diagnostics aid and event analysis through waveform capture.

  • Customized alarm programming to analyze and track down a disturbance on the ac power system.

  • Systematic time stamping of all events and creation of logs.

Metering

The MicroLogic H trip unit offers all the measurements carried out by the MicroLogic P trip unit, with the addition of phase-by-phase measurements of power and energy as well as calculation of:

  • Current and voltage total harmonic distortion (THD)

  • Current, voltage and power fundamentals (50/60 Hz)

  • Harmonic components (amplitude and phase) up to the 31st current and voltage harmonic

  • Real-time metering: The value displayed on the screen is refreshed every second. The table below shows what is measured in real-time metering.

Measurements

Type of Measurement

Unit of Measurement

Measurement Source

Current

IRMS
IAVERAGE
IPEAK/√2
∆IIMBALANCE

A
A
A
%

ØA, ØB, ØC or N
(ØA + ØB + ØC) / 3
ØA, ØB, ØC or N
ØA, ØB, ØC or N

Voltage

VRMS
VRMS
∆VIMBALANCE

V
V
%

(ØA–ØB), ( ØB–ØC) and (ØC–ØA)
(ØA–N), (ØB–N) and ( ØC–N)
VRMS

Power

P, Q and S
EP, EQ and ES
Power factor

W, VAR, VA
Wh, VARh, VAh

Total
Total
Total

Frequency

F

Hz

ØA, ØB, or ØC

Power Quality Indicators

Fundamentals
THD
V and I harmonics

50/60 Hz component
%
Amplitude to phase

V, I, P, Q, and S
V/I
1, 2, 3, 4...50

Demand Metering: Similar to the MicroLogic P trip unit, demand values are calculated over a fixed or sliding time window that can be set from five to sixty minutes.

Type of Measurement

Unit of Measurement

Measurement Source

Current

IDEMAND

A

ØA, ØB, ØC or N

Power

P, Q and SDEMAND

W, VAR, VA

Total

Waveform Capture

The MicroLogic H trip units can capture and store current and voltage waveforms using digital sampling techniques similar to those used in oscilloscopes. Using the information available in the captured waveform, it is possible to determine the level of harmonics as well as the direction and amplitude of the flow of harmonic power.

The MicroLogic H trip unit can record manually via the keypad the following waveforms:

  • Currents IA, IB, IC and IN

  • Phase-to-phase voltages VAB, VBC, and VCA

Waveforms may be displayed on the graphic screen of the control unit or communicated over a networked system. The recording takes place over one cycle with a measurement range of 1 to 1.5 In for current and 0 to 690 volts for voltage. Resolution is 64 points per cycle.

Customized Alarm Programming

The instantaneous value of each measurement can be compared to user-set high and low thresholds. Overrun of a threshold generates an alarm. Programmable action can be linked to each alarm, including circuit breaker opening, recording of measurements in a log, etc.

Event Logs

Each event is recorded with:

  • The date, time, and name of the event

  • The event characteristics

MicroLogic H trip units are designed to be used with an external 24 Vdc power supply. Current-based protection functions require no auxiliary power source.

MicroLogic H Use of External 24 Vdc Power Supply

Function

Without 24 Vdc Power Supply at F1 and F2

With 24 Vdc Power Supply at F1 and F2

Fault Protection for LSIG Functions

Yes

Yes

LED Trip Indication

Yes

Yes

LCD Display and Backlight are Functional

Yes*

Yes

Ground-Fault Push-to-Trip Button Works for Testing Ground Fault*

Yes*

Yes

Metering, Monitoring, and History Logs are Functional

Yes*

Yes

Communications Between Trip Unit and M2C Programmable Contacts

No

Yes

Modbus Communications

No

Yes, with Separate 24 Vdc Power Supply for the Circuit Breaker Communication Module

Additional Characteristics for Type P and H Trip Units

  • Setting the display language: System messages can be displayed in six different languages (English - US, English - UK, French, German, Spanish, and Italian). The desired language is selected via the keypad.

  • Protection functions: All current-based protection functions require no auxiliary source. Voltage-based protection functions are connected to ac power via a voltage measurement input built into the circuit breaker on the bottom side. An optional external voltage measurement is available as a factory-installed option.

  • Accuracy of measurements (including sensors):

    • Voltage (V) 1%

    • Current (A) 1.5% (higher accuracy [1%] may be achieved with special calibration on the current transformer [CT characterization option])

    • Frequency (Hz) 0.1 Hz

    • Power (W) and energy (Wh) 2.5%

      The MicroLogic H trip unit uses a dedicated metering data chain separate from the protection data chain so that a greater number of data samples can be used for metering. This increases the number of samples taken per time period, which in turn gives the H trip unit a higher degree of metering accuracy.

  • Stored information: The fine setting adjustments, the last 100 events and the maintenance record remain in the trip unit memory even when power is lost.

  • Reset: An individual reset, via the keypad or remotely, will reset alarms, minimum and maximum data, peak values, counters and indicators.

MicroLogic Trip Unit Functions

Long-Time Trip Functions

Long-Time Trip Functions

The long-time pickup switch sets the maximum current level the circuit breaker will carry continuously. The maximum current level (Ir) is the long-time pickup setting multiplied by the sensor plug amperage (In). If the current exceeds this value for longer than the long-time delay time, the circuit breaker will trip.

The long-time delay switch sets the length of time that the circuit breaker will carry a sustained overload before tripping. Delay bands are labeled in seconds of overcurrent at six times the ampere rating. For maximum coordination, there are eight delay bands. Long-time delay is an “inverse time” characteristic in that the delay time decreases as the current increases.

The trip unit includes an alarm indicator that will be lit continuously when the current is above 100% of the pickup setting.

Short-Time Trip Functions

Short-Time Trip Functions

The short-time pickup switch sets the short-circuit current level at which the circuit breaker will trip after the set short-time delay. The short-time current (Isd) equals the short-time pickup setting multiplied by the long-time pickup (Ir).

The short-time delay switch sets the length of time the circuit breaker will carry a short circuit within the short-time pickup range. The delay (based on 10 times the ampere rating Ir) can be adjusted to four positions of I2t ramp operation (I2t ON) or five positions of fixed time delays (I2t OFF). I2t ON delay is an “inverse time” characteristic in that the delay time decreases as the current increases. Short-time delay for the 2.0 trip unit is fixed at a delay band of 20 to 80 ms.

Instantaneous Trip Function

The instantaneous pickup switch sets the short-circuit current level at which the circuit breaker will trip with no intentional time delay. The instantaneous current (Ii) is equal to the instantaneous pickup setting multiplied by the sensor plug amperage (In).

The instantaneous function will override the short-time function if the instantaneous pickup is adjusted at the same or lower setting than the short-time pickup. In trip units with both adjustable short-time and instantaneous trip functions, the adjustable instantaneous trip can be disabled by setting Instantaneous pickup to OFF.

Ground-Fault Trip Functions

Ground-Fault Trip Functions

The ground-fault pickup switch sets the current level at which the circuit breaker will trip after the set ground-fault delay. Ground-fault pickup values (Ig) are based on circuit breaker sensor plug (In) only, not on the rating plug multiplier (Ir). Changing the rating plug multiplier has no effect on ground-fault pickup values.

The ground-fault delay switch sets the length of time the circuit breaker will carry ground-fault current which exceeds the ground-fault pickup level before tripping. The delay, based on the sensor plug amperage (In), can be adjusted to four positions of I2t ramp operation (I2t ON) or five positions of fixed time delays (I2t OFF). I2t ON delay is an “inverse time” characteristic in that the delay time decreases as the current increases.

Smart System Communication Wiring System

Wiring System ULP

The wiring system is designed for low-voltage power switchboards. Installation does not require special tools or training. The prefabricated wiring simplifies both data transmission (Modbus protocol) and 24 Vdc power distribution for the communications modules on the MicroLogic trip units.

A. FDM128 display for 8 LV devices

B. IFE Ethernet interface for LV circuit breaker and gateway

C. IFM Modbus-SL interface for LV circuit breaker

D. FDM121 display for LV circuit breaker

E. IO input/output interface module for LV circuit breaker

F. MasterPacT NT/NW circuit breaker

G. PowerPacT H-, J-, or L-frame circuit breaker

H. ULP line terminator

I. ULP cable

J. Breaker ULP cord

K. NSX cord

L. PowerPacT P/R or ComPacT NS

Smart System Four Functional Levels

A: MicroLogic trip unit with ammeter

P: MicroLogic trip unit “Power”

H: MicroLogic trip unit “Harmonics”

See the section on the MicroLogic trip units for details about the trip units.

The PowerPacT and ComPacT devices can be integrated into Ethernet and Modbus communication environment.

There are four possible functional levels that can be combined.

Functional Level

Switch

Circuit Breaker

Status Indications

ON/OFF (O/F)
Spring charged
Ready to close
Fault-trip SDE
Connected / disconnected / test position CE/CD/CT (CCM only)

X
X
X
X

A
A
A
A
A

P
P
P
P
P

H
H
H
H
H

Controls

MX1 shunt trip
XF shunt close

X
X

A
A

P
P

H
H

Measurements

Instantaneous measurement information
Averaged measurement information
Maximum / minimum Ammeter
Energy metering
Demand for current and power
Power quality






A

A


P

P
P
P

H
H
H
H
H
H

Operating Assistance

Protection and alarm settings
Histories
Time stamped event tables
Maintenance indicators







A

P
P
P
P

H
H
H
H

Smart System Modbus Principle

The Modbus RS 485 (RTU protocol) system is an open bus on which communicating Modbus devices (MasterPacT NW with Modbus COM, Power Meter PM700, PM800, PowerPacT P/R-frame, etc.) are installed. All types of PLCs and microcomputers may be connected to the bus.

Addresses

The Modbus communication parameters (address, baud rate, parity) are entered using the keypad on the MicroLogic A, P, or H trip unit. For a switch, it is necessary to use the Electrical Asset Manager or RSU (Remote Setting Utility) MicroLogic utility.

Number of Devices

The maximum number of devices that may be connected to the Modbus bus depends on the type of device (PowerPacT circuit breaker with Modbus COM, PM700, PM800, MasterPacT circuit breaker, etc.), the baud rate (19200 is recommended), the volume of data exchanged and the desired response time. The RS 485 physical layer offers up to thirty-two connection points on the bus (one client, thirty-one servers).

Length of Bus

The maximum recommended length for the Modbus bus is 3940 feet (1200 meters).

Bus Power Source

A 24 Vdc power supply is required (less than 20% ripple, insulation class II).

Smart System Ethernet Principle

Ethernet is a data link and physical layer protocol defined by IEEE 802 10 and 100 Mbps specifications that connects computer or other Ethernet devices. Ethernet is an asynchronous Carrier Sense Multiple Access with Collision detection (referred as CSMA/CD) protocol. Carrier Sense means that the hosts can detect whether the medium (coaxial cable) is idle or busy.

Multiple Access means that multiple hosts can be connected to the common medium. Collision Detection means a host detects whether its transmission has collided with the transmission of another host (or hosts).

IFE Ethernet interface can be connected to a PC or a laptop over Ethernet. The maximum length of Ethernet cable is 325 feet (100 meters). IFE Ethernet interface + gateway provides a Modbus TCP/IP gateway over Ethernet to enable Modbus TCP communication from a Modbus TCP client to any Modbus server devices connected to it. The maximum active Modbus TCP client connection is twelve.

IFE Ethernet interface has an embedded web server (web page).

COM Option in PowerPacT and ComPacT Circuit Breakers

All PowerPacT and ComPacT devices can be fitted with the communication function thanks to the COM option. PowerPacT and ComPacT uses the Ethernet or Modbus communications protocol for full compatibility with the supervision management systems.

For fixed and drawout devices, the common communication option is made up of:

BCM ULP Module

  • A BCM ULP module, installed behind the MicroLogic trip unit and supplied with a set of switches (OF, SDE, PF and CH switches), a kit for connection to shunt close (XF) and shunt trip (MX1) communicating voltage releases (for electrically operated devices), and a COM terminal block (inputs E1 to E6).
    This module is independent of the trip unit and receives and transmits information on the communication network. An infra-red link transmits data between the trip unit and the communication module.
    Consumption: 30 mA, 24 V.

and

  • The IFM module, the Modbus interface for connection to the network, contains the Modbus address (1 to 99) declared by the user using the two dials in front. It automatically adapts (baud rate, parity) to the Modbus network in which it is installed.

or

I/O Application Module

  • The IFE module, the Ethernet interface for low-voltage circuit breakers, enables an intelligent modular unit (IMU) such as a MasterPacT NT/NW or PowerPacT circuit breaker to be connected to an Ethernet network. Each circuit breaker has its own IFE and a corresponding IP address.

For drawout device the Cradle Management option must be added:

The I/O (Input/Output) application module for low-voltage circuit breakers is delivered with the drawout devices ordered with the COM option for cradle management. It must be installed on a steel DIN rail that is properly grounded near the device. The I/O module must be connected to the ULP system and to the cradle position contacts (CD, CT, CE) that transmit the position of the circuit breaker in the cradle.

For communicating remote control for electrically operated devices, shunt close (XF) and shunt trip (MX1) communicating voltage releases must be added:

The shunt close (XF) and shunt trip (MX1) communicating voltage releases are equipped for connection to the communication module.

The remote-tripping function shunt trip (MX2) and undervoltage release (MN) are independent of the communication option. They are not equipped for connection to the communication module.

A. BCM ULP

B. OF, SDE, SD, PF, CH (tripped, open/closed, overcurrent trip, ready to close, charged Switches

C. COM Terminal Block (E1 to E6)

D. Shunt Trip (MX1) and Shunt Close (XF)

E. CE, CD, and CT (connected, disconnected, test) contacts

F. Circuit Breaker ULP Cord

G. I/O Application Module

H. ULP Cable

I. IFE Module

J. IFM Module

Smart System IFE Ethernet Interface

IFE Interface, IFE Interface + Gateway Description

IFE Interface

IFE Interface + Gateway

Introduction

The IFE interface and IFE interface + gateway enable low-voltage circuit breakers such as MasterPacT NT/NW or PowerPacT P/R-frame to be connected to an Ethernet network.

IFE Interface

Provides Ethernet access to a single low-voltage circuit breaker.

Function: Interface - one circuit breaker is connected to the IFE interface using its ULP port.

IFE Interface + Gateway

Provides Ethernet access to one or several low-voltage circuit breakers.

Functions:

  • Interface - one circuit breaker is connected to the IFE interface using its ULP port.

  • Gateway: several circuit breakers on a Modbus network are connected using the IFE interface + gateway client Modbus port.

IFE Interface, IFE Interface + Gateway Features

  • Dual 10/100 Mbps Ethernet port for simple daisy chain connection.

  • Device profile web service for discovery of the IFE interface, IFE interface + gateway on the LAN.

  • Ethernet interface for MasterPacT and PowerPacT circuit breakers.

  • Gateway for Modbus-SL connected devices (IFE interface + gateway only).

  • Embedded set-up web pages.

  • Embedded monitoring web pages.

  • Embedded control web pages.

  • Built-in e-mail alarm notification.

IFE Interface, IFE Interface + Gateway Screen

IFE Interface Mounting

The IFE interface and IFE interface + gateway are DIN rail mounting devices. A stacking accessory enables the user to connect several IFMs (ULP to Modbus interfaces) to an IFE interface + gateway without additional wiring.

IFE Interface 24 Vdc Power Supply

The IFE interface and the IFE interface + gateway must always be supplied with 24 Vdc power.

The IFMs stacked to an IFE interface + gateway have power supplied by the IFE interface + gateway, thus it is not necessary to supply them separately. It is recommended to use a UL listed and recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.

IFE Interface Required Circuit Breaker Communication Modules

The connection to an IFE interface or IFE interface + gateway requires a communication module embedded into the circuit breaker:

  • PowerPacT and ComPacT circuit breakers: BCM ULP communication module

  • Drawout PowerPacT and ComPacT circuit breakers: BCM ULP and its respective I/O (Input/Output) application module.

All connection configurations for the circuit breakers require the circuit breaker ULP cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac. When the second ULP RJ45 connector is not used, it must be closed with a ULP terminator (TRV00880).

Characteristic

Value

Type of interface module

Modbus RTU, RS485 serial connection
Modbus TCP/IP Ethernet

Transmission

Modbus RS485

Transfer rate: 9,600–19,200 Baud Medium Double shielded twisted pair
Impedance 120 Ω

Ethernet

Transfer rate: 10/100 Mbps
Medium STP, Cat5e, straight cable

Structure

Type

Modbus, Ethernet

Method

Client/Server

Device type

Modbus

Client

Ethernet

Server

Turnaround time

Modbus

10 ms

Ethernet

1 ms

Maximum length of cable

Modbus

1000 m

Ethernet

100 m

Type of bus connector

Modbus

4-pin connector

Ethernet

RJ45 (Shielded)

IFE Web Page Description

Monitoring Web Page

Real time data

X

Device logging

X

Control Web Page

Single device control

X

Diagnostics Web Page

Statistics

X

Device information

X

IMU (circuit breaker) information

X

Read device registers

X

Communication check

X

Maintenance Web Page

Maintenance log

X

Maintenance counters

X

Setup Web Page

Device localization/name

X

Ethernet configuration (dual port)

X

IP configuration

X

Modbus TCP/IP filtering

X

Serial port

X

Date and time

X

E-mail server configuration

X

Alarms to be e-mailed

X

Device list

X

Device logging

X

Device log export

X

SNMP parameters

X

Documentation links

X

Preferences

X

Advanced services control

X

User accounts

X

General Characteristics

Environmental Characteristics

Conforming to standards

UL 508, UL 60950, IEC 60950, 60947-6-2

Certification

cUIUs, FCC, CE

Ambient temperature

Storage: -40 to +185°F (-40 to +85°C)
Operation: ˗13 to +158°F (-25 to +70°C)

Protective Treatment

ULVO, conforming to IEC 60068-2-30

Pollution

Level 3

Mechanical Characteristics

Shock resistance

Conforming to IEC 60068-2-27 15g/11ms, 1/2 sinusoidal

Resistance to sinusoidal vibrations

Conforming to IEC 60068-2-6

Electrical Characteristics

Power Supply

24 Vdc, -20%/+10% (19.2 to 26.4 Vdc)

Consumption

Typical: 4 Vdc, 120 mA at 68°F (20°C)
Maximum with gateway: 26.4 Vdc, 3 A at 140°F (60°C)

Physical Characteristics

Dimensions

2.83 x 4.13 x 2.79 in. (72 x 105 x 71 mm)

Mounting

Mounting DIN rail

Weight

182.5 g (0.41 lb)

Degree of protection of the installed module

On the front panel (wall mounted enclosure): IP4x
Connectors: IP2x
Other parts: IP3x

Connections

Screw type terminal blocks

Technical Characteristics - 24 Vdc Power Supply

Power supply type

Regulated switch type

Rated power

72 W

Input voltage

100–120 Vac for single phase

200–500 Vac phase-to-phase

PFC filter

With IEC 61000-3-2

Output voltage

24 Vdc

Power supply out current

3 A

NOTE: Use a UL Listed / UL Recognized limited voltage / limited current or a Class 2 power supply with a 24 Vdc, 3 A maximum.

A. Ethernet 1 and Ethernet 2 communication port

B. 24 Vdc power supply terminal block

C. Ethernet communication LEDs:

  • yellow: 10 Mb

  • green: 100 Mb

D. Module status LED:

  • steady off: no power

  • steady green: device operational

  • steady red: major fault

  • flashing green: standby

  • flashing red: minor fault

  • flashing green/red: self-test

E. Network status LED:

  • steady off: no power/no valid IP address 

  • steady green: connected, valid IP address

  • steady orange: default IP address

  • steady red: duplicated IP address

  • flashing green/red: self-test

F. Sealable transparent cover

G. ULP status LED

H. Test button (accessible closed cover)

I. Locking pad

J. Modbus traffic status LED (IFE Interface + Gateway only)

K. Device name label

L. ULP ports

Smart System IFM Modbus Communication Interface

IFM Interface Function

IFM Modbus Communication Interface TRV00210

An IFM Modbus communication interface is required for connection of a MasterPacT or PowerPacT circuit breaker to a Modbus network as long as this circuit breaker is provided with a ULP (Universal Logic Plug) port. The port is available on the BCM ULP.

Once connected, the circuit breaker is considered as a server by the Modbus client. Its electrical values, alarm status, open/close signals can be monitored or controlled by a Programmable Logic Controller or any other system.

IFM Interface Characteristics

ULP Port

Two RJ45 sockets, internal parallel wiring.

  • Connection of a single circuit breaker.

  • A ULP line terminator or an FDM121 display unit must be connected to the second RJ45 ULP socket.

  • The RJ45 sockets deliver a 24 Vdc supply fed from the Modbus socket.

  • Built-in test function, for checking the correct connection to the circuit breaker and FDM121 display unit.

Modbus Server Port

  • Top socket for screw-clamp connector, providing terminals for:

    • 24 Vdc input supply (0 V, +24 V)

    • Modbus line (D1, D2, Gnd) 2-wire Modbus system.

  • Lateral socket, for DIN-rail stackable connector. Both top and lateral sockets are internally parallel wired.

  • Multiple IFMs can be stacked, thus sharing a common power supply and Modbus line without individual wiring.

  • On the front face:

    • Modbus address setting (1 to 99): two coded rotary switches

    • Modbus locking pad: enables or disable the circuit breaker remote control and modification of IFM parameters.

  • Self-adjusting communication format (Baud rate, parity).

A. Modbus Screw Clamp Connector

B. Modbus Address Switches

C. Modbus Traffic LED

D. Modbus Locking Pad

E .ULP Activity LED

F .Test Button

G. Mechanical Lock

H. ULP RJ45 Connectors

I. Stacking Accessory Connection

IFM Interface Technical Characteristics

Dimensions

0.71 x 2.83 x 3.78 in. (18 x 72 x 96 mm)

Maximum number of stacked IFM

12

Degree of protection of the installed module

Part projecting beyond the escutcheon

IP4x

Other module parts

IP3x

Connectors

IP2x

Operating temperature

-25 to +70°C

Power supply voltage

24 Vdc -20%/+10% (19.2–26.4 Vdc)

Consumption

Typical

21 mA/24 Vdc at 68°F (20°C)

Maximum

30 mA/19.2 Vdc at 140°F (60°C)

Certification

CE

IEC/EN 60947-1

UL

UL 508 - Industrial Control Equipment

CSA

No. 142-M1987 - Process Control Equipment

  • CAN/CSA C22.2 No. 0-M91 - General requirements - Canadian Electrical Code Part

  • CAN/CSA C22.2 No. 14-05 - Industrial Control Equipment

Simplified IFM Interface Installation

Stacking an IFM

Stacking Accessories

Up to 12 Stacked IFMs

Stacking an IFE Interface + Gateway with IFMs

Smart System I/O Application Module

I/O Application Module Description

I/O Application Module

The I/O (Input/Output) application module for an low-voltage circuit breaker is part of an ULP system with built-in functions and applications to enhance the application needs. The ULP system architecture can be built without any restrictions using the wide range of circuit breakers.

The I/O application module is compliant with the ULP system specifications.

Two I/O application modules can be connected in the same ULP network.

The ranges of low-voltage circuit breakers enhanced by the I/O application module are:

  • MasterPacT NW

  • MasterPacT NT

  • PowerPacT R-Frame

  • PowerPacT P-Frame

  • ComPacT NS

I/O (Input/Output) Application Module for Low-Voltage Circuit Breaker Resources

The I/O application module resources are:

  • Six digital inputs that are self powered for either NO and NC dry contact or pulse counter

  • Three digital outputs that are a bistable relay (5 A maximum)

  • One analog input for PT100 temperature sensor

I/O Application Module Pre-Defined Application

The pre-defined application adds new functions to the I/O application module by:

  • Selection by the application rotary switch on the I/O application module, defining the application with pre-defined input/output assignment and wiring diagram.

  • No additional setting with the customer engineering tool required.

The resources not assigned to the pre-defined application are free for additional user-defined applications:

  • cradle management

  • circuit breaker operation

  • cradle management + ERMS (Energy Reduction Maintenance Setting)

    NOTE: Use only MicroLogic P or H trip units with the blue ERMS label for energy reduction maintenance setting systems. Review the I/O module user guide 0613IB1317 and ERMS installation instructions NHA67346 for details on installation, testing, and operation of the ERMS system.
  • light and load control

  • custom

I/O Application Module User-Defined Applications

User-defined applications are processed by the I/O application module in addition to the pre-defined application selected.

The user-defined applications are available depending on:

  • the pre-defined application selected

  • the I/O application module resources (inputs and outputs) not used by the application.

The resources required by user-defined applications are assigned using the customer engineering tool:

  • protection

  • control

  • energy management

  • monitoring

I/O Application Module Mounting

The I/O application module is a DIN rail mounted device. Install on a steel DIN rail that is properly grounded near the device.

I/O Module Application Rotary Switch

The application rotary switch enables the selection of the pre-defined application. It has nine positions and each position is assigned to a pre-defined application. The factory set position of the switch is pre-defined application one.

I/O Application Module Setting Locking Pad

The setting locking pad on the front panel of the I/O application module enables the setting of the I/O application module by the customer engineering tool.

I/O Application Module General Characteristics

A. 24 Vdc power supply terminal block

B. Digital input terminal block: 6 inputs, 3 commons and 1 shield

C. 6 input status LEDs

D. Analog input status LED

E. 3 output status LEDs

F. I/O application module identification labels

G. Sealable transparent cover

H. Analog input terminal block

I. Digital output terminal blocks

J. ULP status LED

K. Test/reset button (accessible with cover closed)

L. Setting locking pad

M. Application rotary switch: 1 to 9

N. Switch for I/O addressing (I/O 1 or I/O 2)

O. ULP connectors

   

General Characteristics

Environmental Characteristics

Conforming to standards

UL 508, UL 60950, IED 60950, 60947-6-2

Certification

cULus, EAC, FCC, CE

Ambient temperature

Storage: -40 to +185°F (-40 to +85°C)
Operation: -13 to +158°F (-25 to +70°C)

Protective Treatment

ULVO, conforming to IEC 60068-2-30

Pollution

Level 3

Mechanical Characteristics

Shock resistance

Conforming to IEC 60068-2-27 15g/11ms, 1/2 sinusoidal

Resistance to sinusoidal vibrations

Conforming to IEC 60068-2-6

Electrical Characteristics

Power Supply

24 Vdc, -20%/+10% (19.2 to 26.4 Vdc)

Consumption

Typical: 24 Vdc, 165 mA at 20°C
Maximum with gateway: 26.4 Vdc, 420 mA at 60°C

Physical Characteristics

Dimensions

2.83 x 4.52 X 2.79 in. (72 x 115 x 71 mm)

Mounting

DIN rail

Weight

0.51 lb. (229.5 g)

Degree of protection of the installed I/O application module

  • On the front panel (wall mounted enclosure): IP4x

  • I/O parts: IP3x

  • Connectors: IP2x

Connections

Screw type terminal blocks

Technical Characteristics
24 Vdc power supply

Power supply type

Regulated switch type

Rated power

72 W

Input voltage

  • 100–120 Vac for single phase

  • 200–500 Vac phase-to-phase maximum

 

PFC filter

With IEC 61000-3-2

Output voltage

24 Vdc

Power supply out current

3:00 AM

NOTE: It is recommended to use an UL listed/UL listed recognized limited voltage/limited current or a class 2 power supply with a 24 Vdc, 3 A maximum.

Digital Inputs

Digital input type

Self powered digital input with current limitations as per IEC 61131-2 type 2 standards (7 mA)

Input limit values at state 1 (close)

19.8–25.2 Vdc, 6.1–8.8 mA

Input limit values at state 0 (open

0–19.8 Vdc, 0 mA

Maximum cable length

33 ft (10 m)

NOTE: For a length greater than 10 m (33 ft) and up to 300 m (1,000 ft), it is mandatory to use a shielded twisted cable. The shield cable is connected to the I/O functional ground of the I/O application module.

Digital Outputs

Digital output type

Bistable relay

Rated load

5 A at 250 Vac

Rated carry current

5 A

Maximum switching voltage

380 Vac, 125 Vdc

Maximum switch current

5 A

Maximum switching power

1250 VA, 150 W

Minimum permissible load

10 mA at 5 Vdc

Contact resistance

30 mΩ

Maximum operating frequency

  • 18000 operations/hr (Mechanical)

  • 1800 operations/hr (Electrical)

 

Digital output relay protection by an external fuse

External fuse of 5 A or less

Maximum cable length

10 m (33 ft)

Analog Inputs

The I/O application module analog input can be connected to a Pt100 temperature sensor

Range

-22 to 392°F (-30 to 200°C)

Accuracy

-22 to 68°F (-30 to 20°C): ±3.6°F (2°C)

68 to 284°F (20 to 140°C): ±1.8°F (1°C)

284 to 392°F (140 to 200°C): ±3.6°F (2°C)

Refresh interval

5 s

EcoStruxure™ Power Commission Software

Introduction to EcoStruxure Power Commission Software

The EcoStruxure engineering tool is a software application that helps the user to manage a project as part of designing, testing, site commissioning, and maintenance of the project life cycle. It enables the user to prepare the settings of the devices offline (without connecting to the device) and configure them when connected with the devices. It also provides other value-added features for the user to manage the project such as: safe repository in cloud, attach artifacts to each device or at the project level, organize devices in switchboard, manage a hierarchical structure of the installation, etc.

Compatible Devices (Configuration and Device Management)

The EcoStruxure engineering tool is compatible with the following devices:

  • ComPacT NSX100-630 (IEC) circuit breakers

  • PowerPacT (UL) circuit breakers

  • ComPacT NS630b-3200 (IEC) circuit breakers

  • MasterPacT NT/NW (IEC and UL) circuit breakers

  • Compatible devices (Device Management in the project)

  • Switches (ComPacT NSX, MasterPacT and PowerPacT Family)

  • Third party devices

References:

The EcoStruxure software package can be downloaded from our website:

www.se.com

Features

The EcoStruxure engineering tool includes the Schneider Electric customer engineering tools such as the Remote Setting Utility (RSU) and Remote Control Utility (RCU) with additional features.

The EcoStruxure engineering tool supports the connection of Schneider Electric communicable devices to:

  • create projects by device discovery, selection of devices, and importing a Bill of Material (BOM)

  • monitor the status of protection and I/O status

  • read information (alarms, measurements, parameters)

  • check protection discrimination between two devices

  • upload and download of configuration or settings in batch mode to multiple devices.

  • carry out commands and tests

  • generate and print a device settings report and communication test report

  • manage multiple devices with an electrical and communication hierarchy model

  • manage artifacts (project documents)

  • check consistency in settings between devices on a communication network

  • compare configuration settings between PC and device (online)

  • download latest firmware

The EcoStruxure engineering tool enables the user to access the advanced features of the software once the project is saved in the Schneider Electric cloud.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.