6037CT9901

Power-Zone 4 Arc Resistant Switchgear with ArcBlok Technology

Power-Zone 4 Arc Resistant Low Voltage, Metal-Enclosed Drawout Switchgear with MasterPacT ArcBlok Low Voltage Power Circuit Breakers

As the Occupational Safety and Health Administration (OSHA) continues to impose more stringent worker safety practices through the National Fire and Protection Agency's NFPA 70E, the market has seen a major shift towards arc resistant solutions. Dangerous electrical events, such as an arc flash, can cause injury or even death to personnel in addition to tremendous equipment damage resulting in substantial financial consequences. Reducing the occurrence of these incidents, as well as containing the effects of an arc flash event once it occurs, is essential to reducing risk to personnel.

What is an arc flash?

An arc flash occurs when insulation or isolation between electrified conductors is breached or can no longer withstand the applied voltage. As employees work on or near energized conductors or circuits, movement near or contact with the equipment may cause a phase-to-ground and/or a phase-to-phase fault. Temperatures of more than 5,000 degrees Fahrenheit and a powerful explosion can be produced in an arc flash incident. OSHA has begun to enforce the NFPA 70E safety guidelines for arc flash safety. The guidelines:

  • provide analysis detailing arc flash incident energy, boundary distances, and the Personal Protective Equipment (PPE);

  • state that PPE must be provided;

  • mandate proper worker training;

  • provide procedures for safe work practices;

  • state that tools for a safe work environment must be provided; and

  • state that equipment be installed in accordance with the safety requirements of the National Electrical Code (NEC).

Protecting Your Personnel and Equipment from an Arc Flash

Power-Zone 4 arc resistant switchgear with MasterPacT MTZ2, 3 and NW ArcBlok technology offers patented, superior arc flash protection for operators and maintenance personnel. Power-Zone 4 arc resistant switchgear offers arc flash containment features unique to the industry in both the circuit breaker compartment and the structure.

This offer is engineered with an internal arc gas management system designed to channel dangerous arc flash energy through a pressure relief mechanism in the top of the equipment. This mechanism is comprised of either top mounted baffles (standard) or plenums (as option). The standard top mounted baffles contain roof flaps, which open to relieve pressure and allow for ejection of harmful gasses and plasma away from personnel and equipment. Optional plenums can be provided as an option to safely isolate and exhaust these gasses to a user specified location either internal or external to the facility.

MasterPacT with ArcBlok technology helps quench and transfer an arc before it propagates inside the circuit breaker compartment. This patented technology provides improved protection from the consequences of internal arcing faults and does not increase the footprint of the equipment. Arc flash energy containment occurs on the front, back, and sides, even when the instrument compartment door is open*, providing ANSI Type 2B rating. This simple, stand-alone circuit breaker solution features a space-saving design and offers an improved level of protection for personnel and equipment. Plus, Power-Zone 4 arc resistant switchgear features easy installation and reduced maintenance and inspection requirements.

MasterPacT Circuit Breakers with Arc Flash Technology

Breakthrough technology was used to design the MasterPacT circuit breakers to interrupt large amounts of fault current without being protected by fuses. The same technology and design that allows the MasterPacT circuit breakers to interrupt large fault currents without fuses also provides very good arc flash limitation. The decision to design the MasterPacT to eliminate the need for fuse protection was based on the following:

  • Requirements for smaller footprints and space-saving installations;

  • Avoidance of fuse installation, maintaining supplies, and the need to enter the equipment, in order to check and change fuses;

  • The need to be adjustable, to provide coordination with downstream products and better arc flash protection.

Advantages of using MasterPacT circuit breakers and Power-Zone 4 switchgear, when there are arc flash concerns:

  • Arc flash limiting feeder circuit breakers up to 2000 A can reduce arc incident energy on downstream equipment such as motor control centers (MCCs) and power distribution panels (PDPs).

  • Through-the-door circuit breaker operation allows unit to be operated/racked while door is closed; this reduces NFPA 70E PPE category by one level.

  • Optional rear hinged doors allow easy access to cables; this reduces NFPA 70E PPE category by one level.

  • MasterPacT arc flash circuit breaker equations are easily inserted into software packages such as SKM Analysis to get these testing results. For further information on applying MasterPacT circuit breakers for arc flash protection, refer to data bulletins 0613DB02XX and 0100DB04XX.

Helpful Definitions:

An Arc Flash is a through-air short circuit event that occurs as a result of a fault condition in an electrical distribution system.

Arc resistant refers to the equipment rating achieved by meeting the ANSI C37.20.7 Standard for arc resistant switchgear.

ArcBlok is a Schneider Electric patented technology applied inside of PZ-4 switchgear which is designed to rapidly quench and transfer an internal arcing fault before it propagates inside the circuit breaker compartment.

Codes and Standards

  • Power-Zone 4 Arc Resistant Switchgear with ArcBlok Technology: is certified to comply with ANSI C37.20.7 IEEE Guide for Testing Metal-Enclosed Switchgear Rated Up to 38 kV for Internal Arcing Faults, and third-party (UL) witnessed as arc resistant switchgear. Refer to Data Bulletin 6037DB1302 for complete UL Witness Certification Summary.

  • All arc resistant switchgear sections meet ANSI C37.20.1, C37.51, C37.20.7 standards, and CSA C22.2 No. 31 standards. UL/cUL third party certifications has been achieved to document successful arc flash tests per the criteria of these standards up to 500 milliseconds (30 cycles).

  • Rated Type 2B per ANSI C37.20.7 definitions—from 208 Vac to 635 Vac, 3-phase 3-wire or 3-phase 4-wire with 50% or 100% neutral. Type 2B is the accessibility rating of the equipment. Type 2 designates arc resistant protection on the front, sides, and rear of the equipment. The "B" suffix designates that the equipment maintains the arc resistant rating even with the instrument compartment door open.

  • MasterPacT ArcBlok circuit breakers: meet ANSI C37.13, C37.16, C37.17, and C37.50

  • Arc resistant switchgear can be applied as UL Service Entrance Equipment (option)

  • Option to meet the seismic requirements of the IBC, ICC Edition, ASCE7, and OSHPD (California Healthcare) Special Seismic Certifications.

Features and Benefits

Standard

  • MasterPacT MTZ2, 3 or NW circuit breakers with patented ArcBlok technology (up to 5000 A)

  • 60 in. (1524 mm) deep x 22 in. (559 mm) wide (smallest arc resistant footprint in the industry)

  • 22 in. (559 mm), 36 in. (914 mm) section widths (30 in./762 mm section width not available)

  • 60 in. (1524 mm), 72 in. (1829 mm), 80 in. (2032 mm) section depths

  • Internal arc gas management system for optimized cooling

  • ANSI C37.20.7 Type 2B Rating when racking into Disconnected, Test or Connected position with door closed.

  • NEMA 1 enclosures

  • Bus ratings up to 5000 A

  • MicroLogic trip units

  • Baffles (roof and floor)

  • Bottom plates

  • Floor dampers

  • Rodent barriers

  • Ground bus

  • Up to 100 kAIC, 635V short circuit ratings are available

  • 4 high per section breaker construction available. (Arc Resistant construction does not lower continuous current rating from standard Power-Zone 4 Switchgear ratings.)

Optional

  • Insulated copper bus

  • Zone selective interlocking

  • High-resistance grounding

  • Energy reduction maintenance switch

  • Section barriers (rear, cable, and side)

  • Overhead circuit breaker lifter

  • Circuit breaker remote racking

  • Rear covers, hinged doors

  • ANSI Type 2B rated arc plenum exhaust

  • Arc resistant prepared spaces

  • ANSI Type 2B rated instrument compartments

  • Front Door Gasketing (gasketing for side and rear covers or doors are standard)

  • Arc Resistant Power-Zone 4 Switchgear is not available in NEMA Type 3R Walk-In or Front Accessible Enclosures

Arc Resistant Structure

Power-Zone 4 arc resistant switchgear structures are tested to the ANSI/IEEE C37.20.7 Guide for Testing Metal-Enclosed Switchgear Rated up to 38 kV for Internal Arcing Faults and are third-party, UL witness tested. Built to withstand an internal arcing event up to 635 V and at interrupt ampacities of up to 100,000 A, Power-Zone 4 arc resistant switchgear offers the best-in-class protection and performance characteristics with the smallest footprint in the industry. Each vertical section can be configured with up to 4 cells which can contain all existing cell options including MasterPacT MTZ2,3 or NW low voltage power circuit breakers with ArcBlok technology, instrument compartments with ANSI/IEEE C37.20.7 Type 2B ratings, and prepared spaces for future expansion. As with standard Power-Zone 4 switchgear, vertical sections are divided into three compartments: the circuit breaker compartment, bus compartment, and rear cable compartment. Each section can be fitted with optional isolation barriers to further reduce the likelihood of an internal arcing event from propagating section to section or compartment to compartment. Structures are rear accessible, NEMA Type 1 with available widths of 22 in. (559 mm) and 36 in. (914 mm), and depths of 60 in. (1524 mm), 72 in. (1829 mm), 80 in. (2032 mm). ANSI #49 Grey is standard, but other color options are available.

Internal Arc Gas Management System

Power-Zone 4 arc resistant switchgear employs an innovative, internal arc gas management system utilizing newly designed structure, circuit breaker and cell components, which both quench arc faults and redirect dangerous energies and debris through the roof and away from personnel, while allowing for exceptional ventilation and cooling under normal operation. This system includes roof baffles with pressure-relief flaps, additional hardware and reinforced seams in equipment covers for added strength and support, and spring-loaded floor mechanisms in each bus compartment, which allow for ventilation and then closure in the event of an internal arcing fault. Finally, circuit breaker cells are modified to include control cable glands, as well as the patented ArcBlok technology to increase arc flash performance and protection.

Arc Resistant Roof Design

Power-Zone 4 arc resistant roof comprised of specific designed top covers with reinforced seams and additional hardware for additional strength and support. The roof comprises of three separate pieces: the cell roof, the bus compartment roof, which contains either a top-mounted baffle (standard) or plenum (optional), and the cable compartment roof.

Arc Resistant Baffles

Each arc resistant section comes standard with top-mounted baffles containing pressure-relief flaps, which prevent pressure build-up on front, back, and the sides of the enclosure and allow for venting of arc fault gasses out of the top of the equipment and away from personnel. The pressure relief flaps have perforated edges that are designed and calibrated to open within 5-15 milliseconds of the initiation of the arc fault and the exhausted plasma is directed up and towards the rear of the equipment. The perforated edges allow the pressure-relief flaps to remain open to prevent secondary pressure build-up. Baffles are also a critical component to the thermal ventilation system, which allow for continuous airflow and should not be obstructed. Rail-mounted, circuit breaker lifters are compatible with arc resistant baffles. Baffles ship separately and are to be installed on site. Conduit entry space is not sacrificed with arc resistant baffle assemblies.

Note for room layout: The switchgear requires a minimum switchgear base to ceiling height of 10 ft. (3 m) with no obstructions above the supplied equipment. The roof baffle must be inspected to assure it is in place and is free of damage. The temporary shipping cover must be removed to install the roof baffle before applying power to the equipment. Refer to Figure above for typical roof baffle construction. To maintain the Arc Resistant rating, the switchgear requires a minimum clearance of 3 inches from the front, rear or sides to the nearest wall or obstruction (see note below for Code required aisleways for equipment). Equipment directly coupled to the switchgear is allowed. A close coupled transformer, such as in a unit substation, is acceptable and all sections in the Power-Zone 4 Switchgear will retain their Type 2B arc resistant rating. The transformer equipment connected adjacent to the switchgear through a direct bus connection is not covered by the arc resistant rating of the switchgear. When installing the equipment, consider the aisle space required at the front and rear of the equipment, as well as space at the ends of the lineup.

NOTE: Required minimum clearances around switchgear are given in Article 110.26 of the National Electrical Code® (NEC®) or Rule 2-308 of the Canadian Electrical Code (CEC®). These clearances are only a minimum. Additional space may be required for insertion and withdrawal of circuit breakers and to transfer to other compartments with a hoist or floor crane.

Arc Resistant Plenums

As an option, UL witnessed, ANSI Type 2B rated plenums can be added to redirect and exhaust arc fault gasses and explosive energy to a secure, customer-specified location, away from equipment and personnel. Plenums can be configured to exit the top of the gear in rear or sides and modular extensions are available for custom routing up to and flush with any wall, but not through the wall. Because ventilated plenums require a complex, maintenance intensive design with dampers that can fail in the event of an arc fault, eliminating them provides users with clear benefits of reduced maintenance and increased safety. Power-Zone 4 Arc Resistant Plenums are the only non-ventilated plenums in the industry, minimizing arc fault debris, gasses, or soot from escaping into unwanted areas. Baffles are not available to be used in conjunction with plenums. Plenums are required to exit every other section to facilitate normal state heat exhaust and cannot contain bends (i.e. must be straight runs to exhaust to prevent back pressure).

Plenum Assembly Components

Plenum Elevation Drawing

NOTE: 10 ft./3 m minimum unobstructed ceiling height from base of switchgear required to install plenum and exhaust duct.

Arc Resistant Side Covers/Plates

Side covers are 14 gauge steel and are designed with interlocking flanges and seams around the perimeter and in the middle of the equipment to provide additional structural integrity and improved strength. Multiple L-brackets are installed to overlap the top and side covers for added support. Insulating barriers are installed on the inside of the end covers to protect against phase-to-ground faults within the bus compartments. These insulating barriers cover the entire bus compartment end cover preventing faults from propagating from section to section. Sealing plates placed between sections also improve protection from fault propagation.

Side Cover Assembly (R) with Sealing Bracket Assembly

Doors and Hinges

Due to the arc extinguishing capabilities of the patented MasterPacT circuit breakers with ArcBlok technology, front mounted arc resistant switchgear doors require no additional fasteners, hinges, or increased thickness and ultimately utilize the same doors as standard Power-Zone 4 switchgear*. This allows for reductions in weight and cost. Rear mounted arc resistant doors are reinforced with thicker steel (22 inches wide are 12 gauge and 36 inches wide are 10 gauge), and are structurally reinforced for additional strength.

Typical Front Door Construction

Typical Rear Door Construction

Bus Compartment Spring Loaded Floor Damper

The bus compartment of each arc resistant section contains a spring-loaded floor. The floor is comprised of several compression springs, steel covered with fire retardant polypropylene insulator barrier, and a perforated base plate that allows for thermal ventilation during normal operating conditions and closes under the event of an internal arcing fault, preventing dangerous energies from escaping the bottom of the equipment. Ventilation in the floor damper assembly, allows for fully rated bus.

NOTE: Due to the floor mounted damper system, bottom incoming busway is not available.

Internal Baffle Assembly and Vents

Arc resistant switchgear structures have been modified to include an internal baffle compartment and a repositioning of front and rear door vents to the base of the equipment for improved ventilation and convective cooling.

The internal baffle assembly employs a chamfered design which maximizes air velocity and optimizes the cooling capacity of incoming air. The baffle is designed with louvers that are covered with a chamfered bracket that also allows ground connections. All arc resistant switchgear sections contain louvered vents mounted near the base of the equipment on the rear.

Fans

Fan Mounting Plate

For sections with vertical riser bus rated above 4000 A:

To meet thermal requirements, AR/PZ-4 technology requires a standard roof baffle or an optional open top into a plenum. Fans located at the bottom rear of the equipment are also required. Refer to Fan Mounting Plate for fan location and construction.

Fan Dashboard

The fans are thermostatically controlled and only operate when needed. Each fan assembly is provided with a dashboard located on a dedicated instrument compartment door to indicate the status of the fan system. The fan dashboard includes a light for each fan to indicate ON or OFF as well as a light to indicate if the temperature has passed the threshold to turn the fan system ON. There is also a selector switch called FAN MODE which has two settings, AUTO and TEST. AUTO mode means that the thermostat is used to automatically control when the fans run. Switching to TEST mode makes all of the fans run, regardless of the thermostat setting. Test mode should be used when performing fan system maintenance.

The fan system is designed with one redundant fan per system. The redundant fan will only run if one of the other fans is inoperable and the thermostat indicates the fans need to be running. If the fans become inoperable and the temperature exceeds an acceptable level, the main circuit breaker will be tripped.

MasterPacT MTZ2, 3 or NW Circuit Breakers with ArcBlok Technology

MasterPacT circuit breakers with ArcBlok technology helps quench an arc before it propagates inside the circuit breaker compartment. This patented technology provides improved protection from the consequences of internal arcing faults without increasing the footprint of the circuit breaker cell or structure. This simple, stand-alone circuit breaker solution features performance and space-savings unmatched in the industry, all while allowing for easy installation and reduced maintenance and inspection requirements. ArcBlok technology is the first to reduce the arc flash incident energy, pressure blast, and equipment damage at the cell.

The MasterPacT with ArcBlok technology interfaces with the ArcBlok cradle to prevent arcing events by enclosing the phases at the primary connection of the cradle. If for any reason an arcing event happens, with the separation between phase to phase and phase to ground, the arc is extinguished in less than 12 ms to reduce arc flash energy. The MasterPacT NW with ArcBlok technology is tested as part of Arc Resistant Equipment to ANSI C37.20.7.

MasterPacT Circuit Breaker with ArcBlok (NW shown)

Cluster Shields

The ArcBlok system is comprised of 2 primary interworking components, cluster shields and cradle barriers. The cluster shields provide isolation and protection of circuit breaker stabs in the connected, test, and disconnected positions. These cluster shields are attached to the rear of the circuit breaker and work in concert with the cradle barriers to create a labyrinth effect. This purposely designed labyrinth system helps to prevent the opportunity for faults to occur at the stabs. In the event of an arc fault, the cluster shields and cradle barriers are engineered to extinguish the arc much faster than standard switchgear.

Cluster Shields

NOTE: Circuit breaker ratings up to 200 kAIC with ArcBlok are available in Arc Resistant Power-Zone 4 Switchgear; however, the switchgear has a maximum short circuit rating of 100 kAIC and will be stated as such on the lineup rating nameplate even though the CB nameplate will indicate a 200 kAIC rating.

Cradle Barriers

The cradle barriers are attached to the rear of the cradle and each of the phase isolation barriers interlock with the cluster shields on the rear of the circuit breaker to complete the ArcBlok system. The cradle barrier assembly is comprised of a thermo set body and a Formex® cover located on the top and back surfaces which make no direct contact with any grounded metal components. The Formex cover contains perforated venting slots which both allow for additional ventilation of the stab connections and transfer the arc fault away from the breaker and out the top of the gear. ArcBlok cradle barriers are provided on all circuit breakers and prepared spaces in Power-Zone 4 Arc Resistant Switchgear.

Cradle Barriers Front View

Cradle Barrier Rear View

MasterPacT Cradle with ArcBlok showing cradle barriers

NOTE: CTs must be located in bus/cable compartment for Arc Resistant Switchgear. Systems with Modified Differential Ground Fault Systems require CTs to be mounted in the bus compartment.

Spare Cassette for Prepared Space

Prepared spaces are available for future expansion in Power-Zone 4 arc resistant switchgear. Each prepared space requires a spare cassette. Spare cassettes are comprised of MasterPacT MTZ2, 3 or NW cradles and MasterPacT MTZ2, 3 or NW circuit breaker casings which do not contain any functional circuit breaker components (i.e. trip units, contacts, arc chutes, etc.). For future expansion, the MasterPacT MTZ2, 3 or NW circuit breaker cassette must be removed and replaced with a fully functional MasterPacT MTZ2, 3 or NW circuit breaker. Future expansion circuit breakers cannot be sized for loads greater than what the prepared space is designed and built to deliver from the factory. To maintain the arc resistant ratings of the gear, all cassettes must be racked in with the door closed. ArcBlok cradle barriers are provided on all circuit breakers and prepared spaces in Power-Zone 4 Arc Resistant Switchgear.

Room Clearance Requirements

10-ft. minimum ceiling height is required as measured from the base of the AR switchgear to the ceiling (i.e. 28.5-in. of clear space above the equipment) is required and includes arc blast, baffles or plenum needs. There is a minimum 3-in. space required around the equipment front, sides or rear according to the ANSI C37.20.7 test criteria, unless the equipment is direct coupled to other equipment. If the equipment is located against a Power-Zone house wall that opens up for rear access to the terminal cabinet, a clearance of 14-in. is required from the rear of the equipment for proper ventilation. Additional space may be required for insertion and withdrawal of circuit breakers and to transfer to other compartments with a hoist or crane. In addition, required minimum clearances around switchgear are given in Article 110.28 of the National Electric Code or Rule 2-308 of the Canadian Electrical Code.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.