6037CT9901

Weights

Refer to the shipping documents for the actual weights and dimensions. The weights given here are approximate values. Must add breaker weights for each breaker from Circuit Breaker Cell Weights (lbs/kg) to the section weights in Section Weights (lbs/kg).

Circuit Breaker Cell Weights (lbs/kg)

Breaker Frame Amps No. of Poles Filled Breaker Space Prepared Space only
800 Amp (MTZ1/NT) 3 Pole (single wide) 91/42 51/24
800 Amp (MTZ2/NW) 3 Pole (single wide) 290/132 181/83
 
1600 Amp
2000 Amp
3200 Amp 3 Pole (single wide) 351/160 224/102
3200 Amp 6 Pole (double wide) 673/305 446/203
4000 Amp
5000 Amp
1600 Amp 4 Pole (single wide) 367/167 225/103
2000 Amp
3200 Amp 4 Pole (single wide) 444/202 279/127
3200 Amp 8 Pole (double wide) 847/385 552/251
4000 Amp
5000 Amp

Section Weights (lbs/kg)

Section Contains only 3/6 Pole Circuit Breaker on No Circuit Breakers*
Bus Rating 22-in. Wide* 30-in. Wide 36-in. Wide*
1600-2000 Amp 1200/545 1250/567 1300/590
3200 Amp 1400/635 1450/658 1500/681
4000-5000 Amp 1700/772 1750/794 1800/817
Section Contains at least one 4/8 Pole Circuit Breaker
Bus Rating 30-in. Wide 48-in. Wide  
1600-2000 Amp 1750/794 3575/1622  
3200 Amp 2025/918 3575/1622  
4000-5000 Amp 2025/918 3575/1622  

Consult factory or quotation drawings for other section types.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.