6037CT9901

Trip Unit Comparison

The table below lists the standard (X) and optional (O) trip unit features for Trip Unit types Standard, Ammeter, Power, Harmonic and MicroLogic X/Xi for use in Power-Zone 4 Switchgear. If the feature is tagged in the table with the letters "DM" then that indicates that a separate MicroLogic X Digital Module must be selected in order to get that specific trip unit functionality (see Upgrade with Digital Modules).

Trip Unit Comparison

Features Standard Ammeter Power Harmonics X/Xi
2.0 3.0 5.0 2.0A 3.0A 5.0A 6.0A 5.0P 6.0P 5.0H 6.0H
LI   X     X             X
LS0 X     X               X
LSI     X     X   X   X   X
LSIG/Ground Fault Trip             X   X   X X
Ground Fault Alarm/No Trip               X   X   DM
Ground Fault Alarm and Trip                 X   X DM
Adjustable Rating Plugs X X X X X X X X X X X X
True RMS Sensing X X X X X X X X X X X X
UL listed   X X   X X X X X X X X
Thermal Imaging X X X X X X X X X X X X
Phase-Loading Bar Graph       X X X X X X X X X
LED for Long-Time Pick-Up X X X X X X X X X X X X
LED for Trip Indication       X X X X X X X X X
Digital Ammeter       X X X X X X X X X
ZSI       X   X X X X X X X
Communications       X X X X X
LCD               X X X X X
Advanced User Interface               X X X X X
Protective Relay Functions               X X X X DM
Neutral Protection               X X X X X
Contact Wear Indication               X X X X X
Incremental Fine Tuning of Settings               X X X X X
ERMS               X X X X DM
Power Measurement               X X X X X
Power Quality Measurements total                   X X X
Power Quality Measurements per phase                   X X DM
Waveform Capture                   X X DM
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.