Add Buttons

  1. To add buttons to the toolbar, right-click the gray area of the toolbar and select Customize.
  2. Select the Commands tab and click ArcFM Solution.
  3. Drag icons from Commands and drop on the toolbar.
  4. To remove buttons from the toolbar, right-click the gray area of the toolbar and select Customize.
  5. Drag the button from the toolbar and drop it anywhere off the toolbar.
  6. To reset a toolbar, click the Toolbars tab.
  7. Highlight the toolbar you want to reset.
  8. Click Reset to restore any removed default buttons. Added buttons that are not on the toolbar by default will be removed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?