Delete

When you're in an edit session, you can use Delete to remove a feature from the geodatabase. Designer removes a deleted feature from both the map and the geodatabase.

IMPORTANT: Deleting Conductors: When deleting multiple conductors, select them and use the Delete tool on the Attribute Editor (right-click and select Delete). The Esri delete tools (Delete key on the keyboard or Edit > Delete) do not interact well with Feeder Manager and may cause corrupted data when deleting multiple conductors on multiple feeders.
  1. Right-click a feature on the Selection tab of the Attribute Editor.
  2. Select Delete from the Utilities menu.

  3. You will have the option to confirm the deletion on the Delete Tool confirmation screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?