Number of Cables
In congested areas (such as a downtown network), some utilities use multiple cables per phase to spread the load. For example, a three-phase conductor might actually have multiple cables per phase (3 cables for A, 3 for B, and 3 for C). Conduit Manager allows you to represent multiple cables per phase with the “Number of Cables” field. To change the number of cables, follow these steps:
-
Ensure the conductor is associated to the conduit. See the help topic Associate Conductor to Duct.
-
If necessary, open the ArcFM Conduit Association Editor.
-
Select the conduit.
-
On the ArcFM Attribute Editor > Selection tab, right-click the conduit and choose Edit Conduit Associations.
-
-
Expand the Duct Position that contains the conductor with multiple cables. In the following example, a three-phase conductor is inside duct Position 1.
-
Click the conductor once to highlight it in blue.
-
Under Number of Cables, click the plus and minus signs to increase or decrease the number of cables. You can also type in the number.
IMPORTANT: Is your Number of Cables field grayed out and not becoming active? The most likely reason is a missing piece of configuration. The underlying relationships require a field called “Cables” to track the number. See the Configuration Guide topics Conduit Manager > Create Relationships > Conduit_Cable and Underground Facility Manager > Create Relationships > Conductor_Duct for more information. -
Notice the count appears by the conductor inside the duct.
-
If each phase occupies a different duct, click Break into Phases. Notice the cable counts now appear by the individual phases.
-
Click and drag each phase into its appropriate duct position.
-
Click OK to close the ArcFM Conduit Association Editor dialog.