Remove from Selection/Remove All from Selection

This tool allows you to remove features from the Selection Tab of the Attribute Editor. It does not delete features from the map.

  1. Right-click a feature listed on the Selection tab.
  2. Select Remove from Selection to remove only the selected features. Select Remove All from Selection to clear the Selection tab.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?