Perform Phase Swap
The Phase Swap tool gives users the ability to switch a branch of existing energized feeder from one phase to another. You may swap single- or multi-phase lines, but you may not change the number of phases on a line. How features are selected to participate in the phase swap depends on the Phase Swap Option settings. More information about phase swap tracing is available on the Interpreting Trace Results page.
Phase Swap performs two traces in order to successfully modify the phases. First, it does a trace to identify the tap point. Second, it traces downstream to identify the features to be modified. Both of these traces respect the "Respect Enabled field when tracing" setting in Feeder Manager (see Feeder Manager Settings in the Configuration Guide). If you have this setting selected (turned on) and the Enabled field set to False, then the feature will not be included in either trace used to determine the features to be phase swapped.
Ensure you have an Edit session started and the map display shows the feeder you want to swap. If you want to view the phase swap features as a selection set, you may want to clear any selected sets before the phase swap trace to ensure accurate results.
- Phase Swap does respect downstream edge and junction barriers when identifying features to participate in the phase swap operation. You may place these on the feeder before executing the Phase Swap tool.
-
Select the Phase Swap
button from the ArcFM Toolbar. If the Phase Swap tool is not available, select the correct geometric network from the Esri Utility Network Analyst toolbar.
-
Click a point on the conductor. In the example below, the
user clicked the conductor at the green box. The large red dot is
the tap point or the point at which the phase swap operation is initiated.
All features downstream of the tap point may be affected by the swap.
They are highlighted in red on the map.
When the user clicks a point on the conductor, Phase Swap traces upstream based on the Phase Swap option setting.
De-energized Edges: If you click a de-energized edge, Phase Swap performs a trace to find the downstream-most conductor that has at least one phase not found on the start edge (comparing the PhaseDesignation fields). If it finds such a conductor, the junction at its downstream end is designated as the tap point for Phase Swap. If no such conductor is found, you will receive a message indicating that no valid tap point could be found.
- In the ArcFM Phase Swap window, indicate how the phases should be swapped. Select from the pull down menus in the To: column. If the conductor is single-phase, you may select only one phase.
-
If you want to view the trace results (highlighted in red)
as a section, select the Results as Selection
button. The results are highlighted on the map and added to the Attribute Editor.
-
If you want to zoom to the trace results, click the Zoom
To Results
button. The display will zoom in or out to encompass the phase swap trace results.
- If you want to view detailed information about the features that will be swapped, click the Details button on the ArcFM Phase Swap window. Right-click any feature in the list to Zoom To, Pan To, Highlight, or open the Quick Attribute Viewer.
- Click Swap to update the phase of the selected features and their related objects. ArcFM updates the PhaseDesignation and NormalPosition fields.