Reassociate Separated Phases

As described in Break into Phases, the application can separate a multiple-phase conductor into individual ducts. To rejoin the phases of a conductor that have been broken apart, you must first disassociate the conductor from the conduit and then reassociate it without splitting the phases.

  1. On the map, select the conductor or cable and the conduit.
  2. On the Attribute Editor > Selection tab, right-click the conductor and select Disassociate from Conduit.

  3. Still on the Selection tab, use the Ctrl key to choose both the conduit and conductor so they are highlighted in blue.
  4. Right-click and choose Associate to a Conduit.
  5. In the ArcFM Conduit Association Editor, ensure the Place Phases checkbox is not checked, then place the conductor in a desired duct position.
  6. Notice all phases reside as a single feature in a single duct.

  7. Click OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?