Open Design

You may open a design that has already been created. When you have a design open, the Open Workflow Manager button on the Workflow Manager toolbar in Designer will be disabled. To open a design, you must access Workflow Manager through ArcMap.

  1. In ArcMap, ensure you are not currently editing.
  2. Click the Open Workflow Manager button on the Workflow Manager toolbar in ArcMap. This button will be disabled if you have a design open.
  3. Click the plus (+) symbol next to a Work Request (WR) to expand its contents and view the designs beneath.
  4. Select a design and click the Open Design button. You may also double-click the selected design to open it in ArcMap.

    Workflow Manager will open the selected design in ArcMap and ensure an edit session has been started. The design and its Compatible Units (CU) and Work Locations (WL) appear on the Design tab of the Attribute Editor.

    If you have populated the Facility ID field on the Location tab of the design's Work Request (see Work Request tabs), ArcMap will create a Work Request polygon around the feature and zoom to it. Every other time you open the design, the display will zoom to the last extent of the stored display associated with the design.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?