Page Templates in Designer

The Page Templates tool in Designer works the same as it does in ArcFM, with the exception of an additional category on the Page Templates window when a design is open. This category holds design page templates and is displayed when a design with an associated page template is open.

When a design is open, the design page template also appears in the Stored Items Manager dialog.

To create design page templates, open a design and create a page template. A design page template cannot be opened or managed unless the design is open.

More information about page templates is available in the ArcFM Stored Items section.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?