Field Model Names

The following field model names are added to the Designer Field Model Name domain.

IMPORTANT: CU_LIBRARY_IDAssigned to the ID field on the MM_CU_LIBRARY table. This field provides a unique ID for CUs.Deleting system tables results in some possibly unforeseen side effects. If you delete the MM_CU_LIBRARY table, then all filter relationship classes will be deleted as well. If you must delete MM_CU_LIBRARY, then delete the rest of the MM_CU_* system tables as well (those listed above).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?