Add a New Operational Map
Once you have a map service published to ArcGIS Server, you can configure it for XI series application use in the Mapping plugin.
You need the map’s URL before proceeding.
To add a new map, follow these steps:
- In Solution Center, click the Mapping plugin.
- Click the Operational Maps tab.
- Click the Add New
button.
- Type a Display Name. This name appears throughout the other XI series application plugins, so use a short but descriptive name readily identifiable by other administrators and users. These steps use “Service Area Parcel Lines” as an example.
- Paste the published map service URL into the URL field. The URL in the image is just an example and not a working map service.
- Use the toggles to determine which XI series applications are allowed to access the map.
- Under Machine-to-machine authentication, type the User
Name and Password for the ArcGIS Server/Portal user credential.IMPORTANT:
-
This is only required if your company is using the hosted Edge Service. If your company is using the on-site Edge Service, this credential is not required and you can leave these fields empty. If in the future your company moves to a hosted Edge Service, this credential can be satisfied at that time.
-
Create a Portal account for these machine-to-machine communications.
-
The Portal account can be the same for all three (Operational Maps, Sync Settings, and Markup Settings). Or, for more granular access control, use a separate Portal account for Sync Settings, Markup Settings, and each Operational Map.
-
For Operational Maps, the Portal account must have access to the map service linked to the operational map.
-
For Markup Settings, the Portal account must have access to all Markup feature services.
-
For Sync Settings, the Portal account must have access to all map services that require offline data.
-
-
- Click Save.