Cable Simulator Plugin
A cable simulator plugin is a part of a Conditioning Tap. It is commonly used to simulate signal loss in a cable in an overall strategy to compensate for tilt.
Cable Simulator Plugin Identification
Manufacturer
The manufacturer of the component.
Model Number (required)
The component's model number. The model number is required to be unique across all resources of the same type.
Company ID
The ID your company assigns to the component. It is recommended that you use unique company IDs. You will see a warning if you type a company ID that is not unique, but you are allowed to continue with a non-unique ID.
Description
A short description of the component.
Catalog Id
The GUID assigned to the component.
Is Deprecated (default: not selected)
Toggle to mark the component as deprecated.
Cable Simulator Plugin Properties
Equalizer Value in dB (required)
The auto-optimization engine uses this value in calculations for optimizing your network design in Designer HFC.
Forward Loss (required): The amount of forward signal loss at a particular frequency.
Return Loss (required): The amount of return signal loss at a particular frequency.