Multiple Tenant Drop-Down

If you work with multiple tenants, use the drop-down to quickly change to a different tenant. This is much faster than signing out and signing back in to a different tenant. For example, you might have production and development tenants, especially during the implementation phase, and this is a quick way to toggle between the two configurations.

NOTE: Production tenants are marked with the letter “P” as seen in the image above.

For this drop-down to appear, the following requirements must be met:

  • Your company has more than one tenant.

  • Your user is allowed to view multiple tenants.

  • The tenants have been mapped in Client Configuration.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?