Announcements

In Announcements you can find information about new releases, updates, or important notices about expiring licenses. By default, all announcements are sorted with the most recent listed first.

10–16–2024 added content per GD-4414, C. Walker

IMPORTANT: Announcements can also contain necessary actions that must be taken prior to the rollout of a new release.

Review specific announcements through the five tabs:

  • Products: Major and minor releases as well as hot fixes.

  • Upcoming: Planned updates.

  • Services: Updates for services.

  • Plugins: Solution Center plug-in updates.

  • Notifications: Any other announcements that do not fit in the previous tabs.

Use the filter tool to pare the announcement list to only those of interest. Each tab can have a different filter list which will persist until cleared or Solution Center is closed. Use the Search field to filter the list based on a keyword style search that queries the announcement title, text body, and type tag. Search results appear in a new Search tab. Clicking away from this new tab clears the search results.

Rectangle screen shot with filter tags of various colors. Check boxes for each tag as well as select all and deselect all are included.


To configure email notifications, click the Open Announcement Notification Settings quick link in the header of the Announcements page. You can also click the user icon in the upper, right-hand corner and select User Options > Settings > Email Settings > Announcements tab to navigate to the same settings location. Use the email notifications to filter by product or announcement type.


Screen shot of Announcements plug-in window. Showcases available tabs and sample announcements.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?