Testing a Circuit Breaker With Extended Rotary Handle
Push-to-Trip Procedure
![]() |
---|
HAZARD OF NUISANCE TRIPPING
Device tests must only be done by qualified electrical
personnel.
Failure to follow these instructions can result in injury or equipment damage.
|
When testing the trip mechanism take precautions against:
-
Disrupting operations
-
Activating inappropriate alarms
-
Triggering unwanted actions
For example, tripping the circuit breaker with the push-to-trip button can lead to inappropriate fault indications or corrective actions (such as switching to an alternate power source).
There is no push-to-trip button on the door of a circuit breaker with a front extended rotary handle. To check the trip mechanism, the door must first be opened.
Follow these steps to test the trip mechanism:
Step |
Action |
Position |
|
---|---|---|---|
1 |
Switch the circuit breaker to the open O (OFF) position. Open the door. |
O (OFF) |
|
2 |
Turn the circuit breaker from the O (OFF) position to the I (ON) position, using one of the following tools:
The circuit breaker is ready for the test. |
I (ON) |
|
3 |
Press the push-to-trip button. The circuit breaker trips. |
Trip |
|
4 |
Use a specific tool (refer to step 2) to turn the extension shaft counterclockwise and switch the circuit breaker from the Trip position to the O (OFF) position. The circuit breaker is in the open position. |
O (OFF) |
|
5 |
Close the door. |
– |