Protection Against Overcurrents in Electrical Distribution
ComPact NSX Circuit Breaker Overcurrent Trip Units
ComPact NSX circuit breaker trip units are designed to handle overcurrents (overload currents and short-circuit currents) and in certain cases, ground fault currents.
-
Pickup adjustments are calculated relative to the downstream circuit to be protected.
-
Time delay adjustments are calculated in relation to the protection management (coordination).
There are two types of trip unit:
-
Thermal-magnetic trip units for ComPact NSX100-250 circuit breakers
-
MicroLogic electronic trip units for ComPact NSX100-630 circuit breakers
Standard Settings for Overcurrent Protections
Standard IEC/EN 60947-2 states the trip characteristics at the circuit breaker limits.
The following table summarizes the recommendations of standard IEC/EN 60947-2 for the circuit breaker protection function:
Protection function |
Setting recommendations |
---|---|
Long-time protection |
Long-time protection of the inverse time type (with I 2t constant):
For a higher fault current, the trip time is inversely proportional to the fault current value. |
Short-time protection |
Short-time protection is definite time:
The trip time is:
|
Instantaneous protection |
Instantaneous protection is definite time:
The trip time is less than 0.2 s. |
The Neutral Conductor
The installation rules closely define the type of protection to be used having regard to:
-
Potential overcurrents (overloads and short-circuits).
-
Conductors to be protected.
-
Simultaneous cutoff of all conductors including the neutral conductor (multi-pole breaking).
Description of the Neutral Protection
The neutral must have specific protection if:
-
It is reduced in size compared to the phases.
-
Nonlinear loads generating third order harmonics and multiples thereof are installed.
It may be necessary to cut off the neutral for functional reasons (multiple source diagram) or safety reasons (working with power off).
To summarize, the neutral conductor can be:
-
Non-distributed (3P).
-
Distributed, not cut off and not protected (3P).
-
Distributed, not cut off but protected (3P with ENCT option). Refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide.
-
Distributed, cut off and protected (4P).
ComPact NSX trip units are suitable for all protection types.
ComPact NSX |
Possibilities |
Neutral protection |
---|---|---|
3P |
3P, 3D |
None |
3P + ENCT |
3P, 3D |
None |
3P, 3D + N/2 |
Half neutral |
|
3P, 3D + N |
Full neutral |
|
3P, 3D + OSN (1) |
Oversized neutral |
|
4P |
4P, 3D |
None |
4P, 3D + N/2 |
Half neutral |
|
4P, 4D |
Full neutral |
|
4P, 4D + OSN (1) |
Oversized neutral |
|
(1) OSN (OverSized Neutral) protection is used when high third harmonic (and multiples of the third harmonic) currents are present. OSN protection is installed on MicroLogic 5, 6, and 7 trip units. Refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide. P: Breaking pole, D: Pole protected by the trip unit, N: Neutral protection. |