DOCA0140EN-03

TM-G Thermal-Magnetic Trip Unit

Introduction

The TM-G thermal-magnetic trip unit has low thermal and magnetic pickups. It is designed to protect long conductors and/or distribution systems powered by generators.

There is one configuration of this trip unit: 3P, 3D.

Description

The adjustment dial is on the front of the trip unit:

A Setting range for the TM-G thermal-magnetic trip unit

B Adjustment dial for the thermal protection pickup Ir

Setting the Thermal Protection

The thermal protection pickup Ir is set by a 4-setting dial.

Turning the thermal protection adjustment dial (A) modifies the trip curve as shown (B).

The following table shows the values of the pickup Ir (in amperes) for thermal protection (values indicated on the dial) with respect to every trip unit rating, relative to the position of the dial Ir.

Trip unit rating In (A)

16

25

40

63

Pickup Ir (A)

11

18

28

44

13

20

32

50

14

23

36

57

16

25

40

63

Setting the Magnetic Protection

The magnetic protection pickup Ii cannot be adjusted and equals the value shown below:

Trip unit rating In (A)

16

25

40

63

Pickup Ii (A) +/- 20%

64

80

80

125

Example of Application

Protection of an incoming feed with the following characteristics:

  • Power supplied by a generator defined by:

    • Generator power 40 kVA - 400 V, giving an operating current of 58 A

    • Subtransient reactance: 30%

  • Generator protection. The loads mainly consist of heating and lighting (incandescent bulbs). The neutral is distributed.

The following illustration shows the installation diagram:

Calculations performed on the installation in accordance with the regulations have determined the characteristics of the appropriate ComPact NSX circuit breaker to install (calculations performed using the Ecostruxure Power Design – Ecodial software).

The following table presents the circuit breaker selection:

Installation

Chosen ComPact NSX

Comments

In = 57 A

ComPact NSX100

Determination of case size

Distributed neutral

4P, 3D

Full neutral and linear loads

Isc = 0.3 kA

B

Icu performance can be read from rating plate

Ikmin = 0.25 kA

TM-G

Generator protection circuit breaker

The following table presents the trip unit protections settings:

Installation

Chosen trip unit

Comments

In = 57 A

TM-G 63, Ir set to 57 A

Thermal protection Ir setting

Ikmin = 0.25 kA

Ii =125 A

Low pickup magnetic protection Ii cannot be adjusted

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?