Characteristics of MicroLogic Electronic Trip Units
Introduction
MicroLogic electronic trip units provide the following functions:
-
Protection of the electrical distribution or specific applications
-
Measurement of instantaneous values and measurement of average values (demand) for electrical quantities
-
Kilowatt hour metering
-
Operational assistance such as peak demand, customized alarms, and operation counters
-
Communication
Identification
Identify the trip unit installed on the circuit breaker by using the four characters on the front face:
Protection (X) |
Case (Y) |
Measurements (Z) |
Application (T) |
|||||
---|---|---|---|---|---|---|---|---|
1 |
SI |
2 |
ComPact NSX100/160/250 |
– |
No measurement |
– |
Distribution |
|
Examples |
||||||||
MicroLogic 1.3 |
SI |
400 or 630 A |
– |
Distribution |
||||
MicroLogic 2.2 G |
LS0I |
100, 160 or 250 A |
– |
Generator |
||||
MicroLogic 2.3 |
LS0I |
400 or 630 A |
– |
Distribution |
||||
MicroLogic 2.3 M |
LS0I |
400 or 630 A |
– |
Motor |
||||
MicroLogic 4.2 |
LS0IR |
100, 160 or 250 A |
– |
Distribution including trip on earth leakage |
||||
MicroLogic 4.3 AL |
LS0I |
400 or 570 A |
– |
Distribution including alarm on earth leakage |
||||
MicroLogic 5.3 E |
LSI |
400 or 630 A |
Energy |
Distribution |
||||
MicroLogic 6.3 E-M |
LSIG |
400 or 630 A |
Energy |
Motor |
||||
MicroLogic 7.2 E-AL |
LSI |
100, 160 or 250 A |
Energy |
Distribution including alarm on earth leakage |
||||
MicroLogic 7.3 E |
LSIR |
400 or 630 A |
Energy |
Distribution including trip on earth leakage |
||||
Type of protection: I Instantaneous L Long-time S0 Short-time (time delay cannot be adjusted) S Short-time G Ground-fault R Residual (earth-leakage) |
MicroLogic Trip Unit Families
The range of MicroLogic trip units is made up of several families:
-
MicroLogic 1, 2, and 4 without display screen
-
MicroLogic 5, 6, and 7 with display screen.
On MicroLogic 1, 2, and 4 trip units, the protection functions are set
using adjustment dials on the front face of the trip unit:
On MicroLogic 5, 6, and 7 trip units, the protection functions are set:
-
By using the adjustment dials
-
By additional settings on the keypad. Setting values are displayed on the screen
-
Through EcoStruxure Power Commission software.

For more information about the MicroLogic 5, 6, and 7 trip units, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide.
In Rating of MicroLogic Trip Units
The In rating (in amps) of a MicroLogic trip unit corresponds to the maximum value of the long-time protection (Ir) setting range for the trip unit. The setting range is indicated on the label on the front face of the trip unit (this label is visible on the front face of the ComPact NSX circuit breaker after the trip unit has been fitted).

Example: MicroLogic 5.2 E 250 trip unit:
-
Setting range: 100-250 A
-
In rating = 250 A
Distribution Trip Unit
The following figure and table define the protection functions for distribution-type MicroLogic trip units.
Item |
Parameter |
Description |
MicroLogic(1) |
|||||
---|---|---|---|---|---|---|---|---|
2 |
4 |
5 |
6 |
7 |
||||
A |
– |
Trip unit setting range: minimum setting/maximum setting. The trip unit rating In corresponds to the maximum value of the Ir setting range. |
O |
O |
O |
O |
O |
|
B |
Ir |
Long-time protection pickup |
L |
✓ |
✓ |
✓ |
✓ |
✓ |
C |
tr |
Long-time protection time delay |
O |
O |
✓ |
✓ |
✓ |
|
D |
Isd |
Short-time protection pickup |
S |
✓ |
✓ |
✓ |
✓ |
✓ |
E |
tsd |
Short-time protection time delay |
O |
O |
✓ |
✓ |
✓ |
|
F |
I2t ON/OFF |
Short-time protection I2t curve in ON or OFF position |
– |
– |
✓ |
✓ |
✓ |
|
G |
Ii |
Instantaneous protection pickup |
I |
O |
O |
✓ |
✓ |
✓ |
H |
Ig |
Ground-fault protection pickup |
G |
– |
– |
– |
✓ |
– |
I |
tg |
Ground-fault protection time delay |
– |
– |
– |
✓ |
– |
|
J |
I2t ON/OFF |
Ground-fault protection I2t curve in ON or OFF position |
– |
– |
– |
✓ |
– |
|
K |
IΔn |
Earth-leakage protection pickup |
R |
– |
✓ |
– |
– |
✓ |
L |
Δt |
Earth-leakage protection time delay |
– |
✓ |
– |
– |
✓ |
|
(1) Functions: ✓: Adjustable O: Fixed –: Not present |
Thermal Memory
The thermal memory is used to simulate temperature build-up and cooling in conductors caused by current variations, according to a time constant. In the event of an overload, the trip units with a thermal memory memorize the build-up temperature caused by the current. Memorizing the build-up temperature leads to a reduction in the trip time.
All MicroLogic trip units incorporate a thermal memory as standard:
-
For MicroLogic 2 and 4 trip units, the time constant is 15 minutes.
-
For MicroLogic 5, 6, and 7 trip units, the time constant is 20 minutes.
Motor Trip Units
Item |
Parameter |
Description |
MicroLogic type M |
|||
---|---|---|---|---|---|---|
1.3 |
2 |
6 E |
||||
A |
– |
Trip unit setting range: minimum setting/maximum setting. The trip unit rating In corresponds to the maximum value of the setting range. |
O |
O |
O |
|
B |
Ir |
Long-time protection pickup |
L |
– |
✓ |
✓ |
C |
Class |
Long-time protection trip class |
– |
✓ |
✓ |
|
D |
Isd |
Short-time protection pickup |
S |
✓ |
✓ |
✓ |
E |
tsd |
Short-time protection time delay |
O |
O |
O |
|
F |
Ii |
Instantaneous protection pickup |
I |
O |
O |
O |
G |
Ig |
Ground-fault protection pickup |
G |
– |
– |
✓ |
H |
tg |
Ground-fault protection time delay |
– |
– |
✓ |
|
– |
Iunbal |
Phase-unbalance protection pickup |
– |
O |
✓ |
|
– |
tunbal |
Phase-unbalance protection time delay |
– |
O |
✓ |
|
(1) Functions: ✓: Adjustable O: Fixed –: Not present |
Motor Trip Unit: Additional Protection
MicroLogic type M trip units (in particular MicroLogic 6 E-M) also incorporate additional protection for the motor application. For more information, refer to DOCA0141EN, ComPact NSXMicroLogic 5/6/7 Electronic Trip Units - User Guide..
Indication LEDs
Indication LEDs on the front of the trip unit indicate its operational state.
The LEDs and their meaning depend on the type of MicroLogic trip unit.
Type of MicroLogic trip unit |
Description |
---|---|
Distribution |
|
Motor |
The MicroLogic 1.3 M trip unit, which provides short-time protection only, displays the Ready LED (green). |
The indication LEDs function for circuit breaker load currents:
-
Above 15 A on a MicroLogic trip unit rated 40 A
-
Above 30 A on MicroLogic trip units rated > 40 A
The limit value is indicated on the front panel, above the Ready LED of the MicroLogic trip unit.
To activate the Ready LED when the load current is below the limit value, you can:
-
Install a 24 Vdc external power supply module which allows the trip unit to be monitored continuously, even when the circuit breaker is open. For more information, refer to LVPED217032EN, ComPact NSX & NSXm Catalogue.
-
Or, during maintenance visits, connect the pocket battery to monitor the trip unit.
Test Port
MicroLogic trip units feature a test port specifically for maintenance actions.

Use the test port to:
-
Connect a pocket battery for local testing of the MicroLogic trip unit
-
Connect the Service Interface for testing, setting the MicroLogic trip unit, updating the MicroLogic firmware, or for installation diagnostics with EcoStruxure Power Commission software
-
Connect the USB maintenance interface:
-
For push-to-trip test or installation diagnostics with the USB maintenance interface stand-alone
-
For testing and installation diagnostics, setting the MicroLogic trip unit, updating the MicroLogic firmware with the USB maintenance interface connected to a PC
-
![]() |
---|
hazard of REDUCED INSULation distances
On a ComPact NSX400K circuit breaker,
do not remove the cap on the MicroLogic test
port.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Interchangeability of MicroLogic Trip Units
Onsite replacement of trip units is simple:
-
No connections to make
-
No specific tools (for example, calibrated torque wrench)
-
Compatibility of trip units provided by mechanical cap
-
Torque limited screw provides correct torque
The simplicity of the replacement process means that it is easy to make the necessary adjustments as operation and maintenance processes evolve.