EIO0000005638.01

Clock

RTC accuracy

±65 seconds per month (deviation at room temperature of 25 °C [77 °F] and power is OFF).

Clock data backup

Lithium metal battery (primary battery, not replaceable)

Battery life: 3 years (approximate)

Variations in operating conditions and battery life can cause clock deviations from -380 to +90 seconds per month. If you use this product in a system where timing is critical, adjust the clock at regular intervals.

This product uses a primary battery for data backup of the internal clock. If the battery is depleted, the clock data will be lost.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?