EIO0000005638.01

How to Connect the DC Power Cord

DC Power Connector

+ 24 Vdc
- 0 Vdc
FG Functional ground (Connect the FG terminal properly to ground.)

Connection Procedure

  1. Confirm the power cord is not connected to the power supply.
  2. Check the rated voltage.
  3. Strip the membrane of the power cord, and twist the wire ends.
  4. Insert each power cord wire into its corresponding hole. Fasten the screws of the DC power connector to clamp the wire in place.
    NOTE:
    • The necessary torque is 0.56 N•m (5 lb-in).

    • Do not solder the cable connection.

    1. DC power connector

    2. Flat-blade screwdriver (size 0.6 x 3.5 mm)

  5. After inserting all three power cord wires, insert the DC power connector into the power connector on this product.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?