EIO0000005638.01

Panel Cut Dimensions

Based on the panel cutout dimensions, open a mounting hole on the panel.

A

B

C

HMIET5400

190 mm (+1/-0 mm)
(7.48 in [+0.04/-0 in])

135 mm (+1/-0 mm)
(5.31 in [+0.04/-0 in])

1.6...5 mm
(0.06...0.2 in)

HMIET5500

255 mm (+1/-0 mm)
(10.04 in [+0.04/-0 in])

185 mm (+1/-0 mm)
(7.28 in [+0.04/-0 in])

1.6...5 mm
(0.06...0.2 in)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?