Touch Panel
|
Touch panel type |
Resistive film (analog) |
|
Touch points |
Single touch |
|
Touch panel service life |
1 million times or more |
|
Touch panel resolution |
1,024 x 1,024 |
The touch panel does not support multi-touch (two-point touch/multi-point touch). If you touch multiple points on the touch panel, it will operate as if you touched the center-point of the multiple touches.
For example, if you touch two or more points on the touch panel and at the center of the touches is a switch for a drive system, even though you did not directly touch that switch, it may function as if you did.
WARNING |
|---|
|
UNINTENDED EQUIPMENT OPERATION
Do not touch two or more points on the touch
panel.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING