EIO0000005638.01

Grounding

Independent Grounding

Always ground the FG (functional ground) terminal. Be sure to separate this product from the FG of other devices as shown below.

  1. This product

  2. Other device

Precautions

  • Check that the grounding resistance is 100 Ω or less or your country's applicable standard.*1

  • The FG wire should have a cross sectional area 2 mm2 (AWG14) or greater*1. Create the connection point as close as possible to this product, and make the wire as short as possible. When using a long grounding wire, replace the thin wire with a thicker wire, and place it in a duct.

  • The SG and FG terminals are separated internally in this product. When connecting the FG and SG, be sure that no ground loop is formed.

*1 Observe local codes and standards.

Common Grounding

Electromagnetic Interference (EMI) can be created if devices are improperly grounded. EMI can cause loss of communication. If independent grounding is not possible, use a common grounding point as shown in the configuration below. Do not use any other configuration for common grounding.

Correct grounding

  1. This product

  2. Other device

Incorrect grounding

  1. This product

  2. Other device

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?